Design For A Cause 2021
  • Challenges & Projects
  • Design Challenges
  • Design For A Cause 2021
  • More
  • Cancel
Design For A Cause 2021
Blog VenTTracker #06 -  Window Sensor Prototype
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: javagoza
  • Date Created: 11 Apr 2021 12:44 PM Date Created
  • Views 2346 views
  • Likes 4 likes
  • Comments 2 comments
  • venttracker
  • arduino_nano_33_iot
  • covid-19
  • linear position sensors
  • reed switch
  • design_for_a_cause_2021
  • natural ventilation
Related
Recommended

VenTTracker #06 -  Window Sensor Prototype

javagoza
javagoza
11 Apr 2021

One of the main components of our ventilation routine monitoring project is the sensor for the status of doors, windows and blinds. During this week we have given a boost to the creation of that sensor. The blog describes the work of these days consolidating a simple design and the construction of a first prototype that will allow us to fine-tune our software and start taking data to develop a machine learning model. We have equipped the device with several sensors that will help us to automatically label the samples for the training of our machine learning models.

 

image

  Design for A Cause 2021 the VenTTracker project

  01 - Intro and motivation. | 02 - Analyzing Window Types (I) | 03 - Analyzing Window Types (II) | 04 - Playing with the IMU | 05-Sliding Window Mock-up | 06 -  Window Sensor Prototype | 07 - Adjusting the window sensor | 08 - Trying to make a measuring device with the accelerometer | 09 - Checking and updating WiFiNINA Firmware | 10 - Ventilation Monitor on Arduino IoT Cloud | 11 - Wireless Environmental Monitor on Arduino Nano 33 IoT | 12 - Window Anomaly Detection. Edge Impulse & Arduino Nano 33 IoT | 14 - Environmental Monitor Revisited - Version 2 | 13 - Project wrap-up and Lessons learned

 

Tracking System for Classroom Ventilation Routines

A STEM project for classrooms

 

image

 

the VenTTracker project - Blog #06 - Window Sensor Prototype

Our first window sensor protoype:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The Design

 

What are we building?

We are building a Wireless door and window opening sensor. This is an IOT device that can be placed on windows, shutters, blinds and doors to be able to keep track of whether they are open or not and in what position they are: Fully open, semi-open, closed ... Our ventilation routines monitor system will use several of these devices. The device uses an Arduino Nano 33 IoT. It can estimate the degree of opening of the window. To obtain an origin reference that marks the closed position and the full opened position, it uses reed switches. The device can be adapted to multiple types of windows, blinds, shutters and doors.

 

Changes from previous versions

 

This revision of our sensor:

  • Add two reed switches to detect open and close window events and acts as an absolute reference for the linear position encoder and the accelerometer.
  • Maintains the magnetic linear encoder made with another two reed switches.
  • All the switches are attached to ports that support interruptions to allow us to work with multithreading.
  • All the switches use Internal 20K pull-ups. The logic of the switches in our design is negative.
  • Add an OLED Display for debugging purposes.
  • Add a reset button.
  • It is built on a pad-board.

The schematic

 

image

 

 

Components

  • C1: 100nF
  • C2: 10uF
  • DC1: DC005-2.0MM
  • DP1: OLED DISPLAY 128x32 0.91" I2C SSD1306
  • H1: HDR-F-2.54_1x2
  • 2x16 Female Header
  • J2: HDR-M-2.54_1x4
  • LED1,LED2: LED-TH-3mm_G
  • R1,R2: 100 Ohm
  • S1,S2,S3,S4: Plastic Reed Switch Reed Contact Normally Open (N/O)
  • SW1 Push Button - 6x6mm - 2 pins

 

 

Bill of Materials

My apologies that the product descriptions are in Spanish. I am a Farnell Spain customer and they decide for me. I can't change the language or send the BOM list to Farnell UK image those are the problems of such smart websites image. As the news say "the descriptions are in Spanish due to a computer error" Software developers like me are always the problem!

 

Product NameManufacturerQuantityBuy KitBuy Kit
MPCC100V104KY5U-CAPACITOR, 0.1UF, 100V, 10%, Y5U, RADMULTICOMP PRO1Buy NowBuy Now
ECA2GHG100-Condensador Electrolítico, 10 µF, 400 V, Serie NHG, ± 20%, Con Conexión Radial, 1000 horas a 105°CPANASONIC1Buy NowBuy Now
MACD-14-15-20-REED SWITCH, SPST-NO, 0.5A, 200V, AXIALLITTELFUSE4Buy NowBuy Now
CES-116-01-T-S-Conector Hembra para PCB, Simple, Placa a Placa, 2.54 mm, 1 Filas, 16 ContactosSAMTEC2Buy NowBuy Now
CES-102-01-T-S-Conector Hembra para PCB, Simple, Placa a Placa, 2.54 mm, 1 Filas, 2 ContactosSAMTEC1Buy NowBuy Now
ABX00032-PLACA NANO 33 IOT, CONECTOR DE PINESARDUINO1Buy NowBuy Now
CES-104-01-T-S-Conector Hembra para PCB, Simple, Placa a Placa, 2.54 mm, 1 Filas, 4 ContactosSAMTEC1Buy NowBuy Now
HLMP-1401-LED, Amarillo, Agujero Pasante, T-1 (3mm), 10 mA, 2 V, 585 nmBROADCOM2Buy NowBuy Now
MCF 0.25W 100R-Resistencia de Agujero Pasante, 100 ohm, Serie MCF, 250 mW, ± 5%, Axial, 250 VMULTICOMP PRO2Buy NowBuy Now
LS-00003-Product Range:-OSEPP1Buy NowBuy Now
Pantalla OLED Gráfica, 128 x 32 Píxeles, Blanco sobre Negro, 3 V, I2C, 35,8mm x 12mm, -40 °CMIDAS1Buy NowBuy Now
Battery ClipKEYSTONE2Buy NowBuy Now
9V Battery Snap ConnectorMCM1Buy NowBuy Now

 

 

Additional Parts

 

 

Product NameManufacturerQuantity
PCB1

 

 

Software debounce

As we have seen in a previous blog we will need a low pass filter to avoid bouncing on the switches. See VenTTracker #03 - Analyzing window types II

Bouncing is due to mechanical vibration in the sliding motion of the window. This vibratory movement that can move the magnet towards and away from the switch reeds, producing unwanted transitions.

We are using a microcontroller so we are going to use "software debounce" technique for our switches.

The microcontroller we are using include internal pullups and a simple interrupt driven code can look for a stable change of state.

This is why it is very important that our sensors are connected to ports that do support the programming of interrupt services routines.

 

 

Pad-board prototype

Before going to PCB let's make a pad-board prototype. For this prototype we are using a 9v battery.

 

Connections

 

image

 

image

 

 

Assembling our first prototype

 

This are the minimum configuration for our sensor. Nothing else is necessary, the rest of the components are to facilitate debugging and sampling with automatic labeling.

image

 

Checking arduino headers

image

Checking the two encoder magnetic reed switches

image

 

Left and Right Open/Closed Detection Magnetic Reed Sensors and two headers for the display.

 

 

image

 

Bottom view

image

 

Checking Display and IMU/Display relative orientation. We use the developed for the 04 blog: VenTTracker #04 -  Playing with the IMU

image

Everything works!

 

Window Sensor Images

 

Let's add some standoffs and put a transparent protective cover

 

image

 

image

 

image

Right View: You can see the left magnetic reed switch used for detecting open/close events in windows where the magnet is on the right side of the sensor.

You can see the 12v battery under the Arduino Nano 33 IoT between the two headers.

image

 

Left View: You can see the left magnetic reed switch used for detecting open/close events in windows where the magnet is on the left side of the sensor.

image

A close view:

image

 

Placing the sensor in our Sliding Window Mockup

Our Venttracker Window Sensor Prototype Assembled On the Sliding Window Mock-up: VenTTracker #05 -  Sliding Window Mock-up

image

Adding a reset button and some LEDs

 

The reset button is not accessible image. Let's add a reset button and two indicator LEDs as in our old prototype: VenTTracker #03 -  Analyzing window types II

At the bottom right the reset button.

Between the reed switches the new indicator LEDs

 

image

 

Enough empty space for a 12v battery. We need clips for this kind of battery.

 

image

 

image

 

 

And finally a big thank you to the entire element14 community! image

 

image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

The demo code

 

See explanation about the ISR and interrupts in the past blog: VenTTracker #03 -  Analyzing window types II

 

/**************************************************************************
  This is an example for testting the VenTTracker Window Sensor
  Displays the element14 logo in a Monochrome OLEDs based on SSD1306 drivers


  This example is for a 128x32 pixel display using I2C to communicate
  3 pins are required to interface (two I2C and one reset).


  Lights LED according sensor events:
                       | LEFT LED  |  RIGHT LED  |
  WINDOW OPEN EVENT    |    OFF    |    OFF      |
  WINDOW CLOSED EVENT  |    ON     |    ON       |
  TO THE LEFT MOVEMENT |    ON     |    OFF      |
  TO THE RIGHT MOVEMENT|    ON     |    OFF      |


  Author: Enrique Albertos
  Date: 2021-04-10
 **************************************************************************/


#include <Wire.h>
#include <Adafruit_GFX.h>
#include <Adafruit_SSD1306.h>


#define SCREEN_WIDTH 128 // OLED display width, in pixels
#define SCREEN_HEIGHT 32 // OLED display height, in pixels


// Declaration for an SSD1306 display connected to I2C (SDA, SCL pins)
#define OLED_RESET     4 // Reset pin # (or -1 if sharing Arduino reset pin)
Adafruit_SSD1306 display(SCREEN_WIDTH, SCREEN_HEIGHT, &Wire, OLED_RESET);


// Port connections
int leftSwitchPort = 10; // switch to ground + internal pull-up resistor. Negative logic LOW when switch is closed
int rightSwitchPort = 9;  // switch to ground + internal pull-up resistor. Negative logic LOW when switch is closed
int leftLedPort = 8; // positive logic. HIGH turn on the LED
int rightLedPort = 7; // positive logic. HIGH turn on the LED
int openClosedSwitchPort = 2;  // switch to ground + internal pull-up resistor. Negative logic LOW when switch is closed


#define LOGO_HEIGHT   20
#define LOGO_WIDTH    128
// element14 logo 8 pixels per Byte Little Endian Horizontal
static const unsigned char PROGMEM logo_bmp[] = {
  0x00, 0x00, 0x40, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x60, 0x00, 0x00, 0x00,
  0x00, 0x00, 0xE0, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x60, 0x00, 0x00, 0x00,
  0x00, 0x00, 0xE0, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x60, 0x00, 0x00, 0x00,
  0x00, 0x00, 0xE0, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x60, 0x00, 0x00, 0x00,
  0x07, 0x00, 0xE0, 0x1C, 0x00, 0x0C, 0x03, 0x00, 0x07, 0x00, 0x01, 0x80, 0x70, 0x06, 0x18, 0x00,
  0x3F, 0xE0, 0xE0, 0xFF, 0x83, 0x3F, 0x9F, 0xE0, 0x3F, 0xE0, 0x6F, 0xF1, 0xFC, 0x06, 0x18, 0x00,
  0x70, 0x70, 0xE1, 0xC1, 0xC3, 0xE1, 0xF8, 0x70, 0x70, 0x70, 0x78, 0x78, 0x70, 0x06, 0x18, 0x00,
  0x60, 0x38, 0xE3, 0x80, 0xE3, 0xC0, 0xE0, 0x30, 0x60, 0x38, 0x70, 0x18, 0x60, 0x06, 0x18, 0x00,
  0xE0, 0x18, 0xE3, 0x00, 0x63, 0x80, 0xE0, 0x30, 0xE0, 0x18, 0x60, 0x18, 0x60, 0x06, 0x18, 0x18,
  0xC0, 0x18, 0xE3, 0x00, 0x63, 0x80, 0xE0, 0x30, 0xC0, 0x18, 0x60, 0x18, 0x60, 0x06, 0x18, 0x18,
  0xC0, 0x18, 0xE3, 0x00, 0x63, 0x80, 0xE0, 0x30, 0xC0, 0x18, 0x60, 0x18, 0x60, 0x06, 0x18, 0x18,
  0xFF, 0xF8, 0xE3, 0xFF, 0xE3, 0x80, 0xC0, 0x30, 0xFF, 0xF8, 0x60, 0x18, 0x60, 0x06, 0x18, 0x18,
  0xFF, 0xF8, 0xE3, 0xFF, 0xE3, 0x80, 0xC0, 0x30, 0xFF, 0xF8, 0x60, 0x18, 0x60, 0x06, 0x18, 0x18,
  0xC0, 0x00, 0xE3, 0x00, 0x03, 0x80, 0xC0, 0x30, 0xC0, 0x00, 0x60, 0x18, 0x60, 0x06, 0x18, 0x18,
  0xC0, 0x00, 0xE3, 0x00, 0x03, 0x80, 0xC0, 0x30, 0xC0, 0x00, 0x60, 0x18, 0x60, 0x06, 0x1C, 0x18,
  0xE0, 0x00, 0xE3, 0x00, 0x03, 0x80, 0xC0, 0x30, 0xC0, 0x00, 0x60, 0x18, 0x60, 0x06, 0x0F, 0xFF,
  0xE0, 0x00, 0xE3, 0x80, 0x03, 0x80, 0xC0, 0x30, 0xE0, 0x00, 0x60, 0x18, 0x60, 0x06, 0x03, 0xFE,
  0x60, 0x00, 0xE1, 0x80, 0x03, 0x80, 0xC0, 0x30, 0x60, 0x00, 0x60, 0x18, 0x70, 0x06, 0x00, 0x18,
  0x7F, 0xF0, 0xE1, 0xFF, 0xC3, 0x80, 0xC0, 0x30, 0x7F, 0xF0, 0x60, 0x18, 0x3E, 0x06, 0x00, 0x18,
  0x1F, 0xE0, 0x40, 0x7F, 0x83, 0x80, 0xC0, 0x30, 0x1F, 0xE0, 0x60, 0x18, 0x1E, 0x06, 0x00, 0x18
};


typedef enum direction_t  {RIGHT = 0x00, LEFT = 0xFF};
volatile direction_t lastWindowDirection = LEFT;


volatile int8_t encoderPosition = 0; // don't know where is our encoder, we'll need an absolute reference
// let's assume we are in closed position and window opens from left to right
volatile bool encoderChangePending = false;
unsigned long lastLeftSwitchDebounceTime = 0;  // the last time the input left encoder pin was toggled
unsigned long debounceDelay = 50;    // the debounce time


void isrFallingLeftSwitchPort(); // ISR for leftSwitchPort
void isrChangeOpenClosedSwitchPort(); // ISR for open/close switches


void setup() {
  Serial.begin(9600);


  // SSD1306_SWITCHCAPVCC = generate display voltage from 3.3V internally
  if (!display.begin(SSD1306_SWITCHCAPVCC, 0x3C)) { // Address 0x3C for 128x32
    Serial.println(F("SSD1306 allocation failed"));
    for (;;); // Don't proceed, loop forever
  }


  // set port switches with internal 20K pull up resistors
  pinMode (leftSwitchPort, INPUT_PULLUP);
  pinMode (rightSwitchPort, INPUT_PULLUP);
  pinMode (openClosedSwitchPort, INPUT_PULLUP);


  // set debugging LEDs ports
  pinMode (leftLedPort, OUTPUT);
  pinMode (rightLedPort, OUTPUT);


  // After reset blink the logo
  display.clearDisplay();
  drawLogo();
  // Invert and restore display, pausing in-between
  display.invertDisplay(true);
  delay(1000);
  display.invertDisplay(false);
  delay(1000);


  // detect falling edges the switch chages from open to closed. It is negative logic
  attachInterrupt(digitalPinToInterrupt(leftSwitchPort),
                  isrFallingLeftSwitchPort, FALLING);


  // detect switch chages from open to closed. It is negative logic
  attachInterrupt(digitalPinToInterrupt(openClosedSwitchPort),
                  isrChangeOpenClosedSwitchPort, CHANGE);


}


void loop() {
  // if there is a new event from the encoder acknowledge it and do pending actions
  if (encoderChangePending) {
    encoderChangePending = false;
    // turn on left led when window direction is LEFT
    digitalWrite(leftLedPort, lastWindowDirection == LEFT );
    // and turn on right led when window direction is RIGHT
    digitalWrite(rightLedPort, lastWindowDirection == RIGHT );
    // scroll the logo according direction
    if (lastWindowDirection == RIGHT) {
      display.startscrollright(0x00, 0x07);
    } else {
      display.startscrollleft(0x00, 0x07);
    }
    // log encoder position to serial port
    Serial.println(encoderPosition);
  }
}


/**
  Interrupt Service Routine for Falling Edge in Left Switch Port
*/
void isrFallingLeftSwitchPort() {
  if ((millis() - lastLeftSwitchDebounceTime) > debounceDelay) {
    if (digitalRead(rightSwitchPort) == HIGH) {
      encoderPosition++;
      lastWindowDirection = RIGHT;
    } else {
      encoderPosition--;
      lastWindowDirection = LEFT;
    }
    lastLeftSwitchDebounceTime = millis();
    encoderChangePending = true;
  }
}


/**
  Interrupt Service Routine for Changing Edge in Open Close Switches
  when the window is closed light the two LEDS
*/
void isrChangeOpenClosedSwitchPort() {
  int switchState = !digitalRead(openClosedSwitchPort);
  if ((millis() - lastLeftSwitchDebounceTime) > debounceDelay) {
    // Light LEDs when window closed
    digitalWrite(leftLedPort, switchState);
    digitalWrite(rightLedPort, switchState);
    if (switchState) {
      display.stopscroll();
    }
    lastLeftSwitchDebounceTime = millis();
  }
}


/**
  Send logo to the Display and center it and wait 1 second
*/
void drawLogo(void) {
  display.clearDisplay();
  display.drawBitmap(
    (display.width()  - LOGO_WIDTH ) / 2,
    (display.height() - LOGO_HEIGHT) / 2,
    logo_bmp, LOGO_WIDTH, LOGO_HEIGHT, 1);
  display.display();
  delay(1000);
}

Future improvements

For the next revision we will consider:

  • make a PCB and a case.

image

  • replace the reed switch sensor by Hall Digital Switches like A1120LUA-T

Next Steps

  • Start taking and labeling samples and design a ML model.
  • Continue with the design of our Indoor Air Quality Desktop Monitor.

 

VenTTracker Blogs
VenTTracker #01 - Intro and motivation.
VenTTracker #02 - Analyzing window types.
VenTTracker #03 - Analyzing window types II
VenTTracker #04 - Playing with the IMU
VenTTracker #05 - Sliding Window Mock-up
VenTTracker #06 - Window Sensor Prototype
VenTTracker #07 - Adjusting the window sensor
VenTTracker #08 - Trying to make a measuring device with the accelerometer
VenTTracker #09 - Checking and updating WiFiNINA Firmware
VenTTracker #10 - Ventilation Monitor on Arduino IoT Cloud
VenTTracker #11 - Wireless Environmental Monitor on Arduino Nano 33 IoT
VenTTracker #12 - Window Anomaly Detection. Edge Impulse & Arduino Nano 33 IoT
VenTTracker #14 (aka #11 bis) - Environmental Monitor Revisited - Version 2
VenTTracker #13 - Project wrap-up and Lessons learned

 

 

<< Previous VenTTracker BlogNext VenTTracker Blog  >>
VenTTracker #05 - Sliding Window Mock-upVenTTracker #07 - Adjusting the window sensor
  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +2
    Nice build. DAB
  • javagoza
    javagoza over 5 years ago in reply to DAB +1
    Thanks DAB!
  • javagoza
    javagoza over 5 years ago in reply to DAB

    Thanks DAB!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago

    Nice build.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down