Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog 1958 Turntable from the Black Forest - 20: Fast Fourier Transform on the SAMA5D4 - End of Chapter 3
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 19 May 2015 6:35 PM Date Created
  • Views 1533 views
  • Likes 3 likes
  • Comments 12 comments
  • sama5d4
  • enchanted_player
  • enchanted_objects
  • port
  • arduino
  • xplained_ultra
Related
Recommended

1958 Turntable from the Black Forest - 20: Fast Fourier Transform on the SAMA5D4 - End of Chapter 3

Jan Cumps
Jan Cumps
19 May 2015

image

 

I've mastered the SAMA5D4 just in time for chapter 3 closure. The end of a chapter is the right time to look back and reflect.

 

The world is unfair for people that don't know. I have this powerful board in my hands. And I can't get anything usable out of it. I struggle tremendously and blog (some may say whine) about that.

Then magic happens. The first program compiles. That first program runs. The board says 'hello'.

Having a working program speeds things up. Finally, you can check things out. Change something. Does it still work? No? Why not? Take a step back.

Having that reference point - a working example - is the stepping stone to all further endeavors.

 

Looking back, it's hard to understand why it took that long. In hindsight, it's all not that difficult.

Hindsight is 20/20.

That's why the world is unfair for people that don't know. I know now. The progress in the last few days may be a factor 100 more than what I was able to achieve the previous two months. The blog series tells the story.

 

image

 

 

Finish the Light Organ

 

At very start of the enchanted objects, I stole the Arduino Light Organ design from Daniel Herrera. Unchanged.

Why should I change it? It works perfectly.

But with the SAMA5D4 working, I needed something to practice my skills. And (repeating myself today) having a working example is an ideal starting position.

The Arduino example works. So I ported Daniel's code. I also ported the fft-fix Arduino library that he's using (by itself already a port originating from pre-1990 work of Tom Roberts).

 

In my port, I tried to stay as close as possible to the designs of the original code. I only made tactical changes to make it work on the Xplained board.

You can see that in the attached source code. I've spent 0% to do proper design. When porting something, my favorite way is to stay as close as I can to the original.

I focus on getting it working, not on proper design or reuse. The less confuscated the work, the easier to compare it with the original. Refactoring into proper classes, parameterising and clubbing into reusable parts is for later.

Go ahead and look at the code that I attached to this post. It's very visible that I did the port that way. It's still riddled with debug comments - something that helps me to see where I've done tests and result checking between the Arduino and SAMA5D4. And lots of actions are repeated where a generic function would be appropriate. I may do that later. Or someone else - trying to master the SAMA5D4 - may get their hands dirty and post a sanitized version.

 

 

image

 

Looking at the FFT Results

 

The Organ uses Fast Fourier Transforms to turn the sampled audio signal into buckets of audio frequency spectrum. In this design, 128 samples are turned into 64 buckets, from the low side to the high side.

Bright minds may be able to do the full calculation of the covered bandwidth based on my scope's screen capture.

The high part of the blue signal indicates how long one sample burst takes. And I take 128 samples each time. Post the calculations in the comments, please.

 

SAMA5D4  92ms / 129 samplesimage

 

ARDUINO 3.86ms / 128 samples

image

I made a mistake here and measured* the inner time between two samples instead of the time to take 128 samples. Below is the old capture that shows the wrong info.

 

This changes the picture a bit, because the sample time is now longer than on Arduino, and I'll have to optimize code instead of adding _nops.

 

image

 

I've recorded the FFT result of a 20Hz, 200Hz, 2kHz a,d 20 kHz signal. My program printed the resulting spectrum array on the linux console.

Here's a chart of the results. It's not yet a very good outcome. 20Hz and 20 kHZ give an outcome as expected, at the low and high side of the spectrum.

But I'm not yet satisfied with how the 200Hz and 2kHz signals are calculated. The 2kHz has peaks lower in spectrum than the 200Hz signal.

Since I used a clean sinus wave as input, this shouldn't happen.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The plot below, based upon the four tests, shows that the situation is rather fuzzy in the middle part. You can also see a huge peak of the 20kHz signal.

The skew in my results may be based (is very likely based) on the sample speed. In particular the 2kHz signal behaves badly.

I'll try to slow it down* speed it up and get to the same sample speed as the Arduino. That'll give better results.

 

image

 

These are the captures of the four input signals, taken while doing the exercise:

 

imageimageimageimage

 

 

 

Side story: Perpetuum Ebner

 

The small workshop that the brothers Steidinger ran was one of the first in Germany to build gramophone 'clockworks'. That isn't strange, because they were clock mechanism makers.

We're talking early 1900's here. The audio industry was still in its very early days. The brothers - both fine craftsmen - made clockworks that could compete with the best. At last their small company was making some money.


But they didn't escape the faith of many brother based companies: they didn't get along.  Both had a juxtaposed view on the business. They didn't get along. It got so bad that the situation couldn't last.

Their separation wasn't friendly. Josef left, and his share of the company was payed out in cogs and springs.

Christian's story is known to all. He created an electrical/spring powered gramophone motor combination (dual drive -> hence the name DUAL). The DUAL brand still brings a tear to the eye of many strong men.


For Josef, it was back to off. With no money and just a pile of spring motor parts a s capital, he rented the sawmill next to Sankt-Georgen station. He calls his humble business "Perpetuum Schwarzwälder Federmotoren und Automatenwerke".


And it's 1911. Another 3 years and it's wartime. Things are about to change for Josef and many other fine mechanics factories in Germany.

 

* I made a mistake in my time measurement for sampling. On the Arduino I measured the time to take 128 samples, on the SAMA5D I measured the time to take one sample.I've corrected the post, but left the original info in place for reference.

 

 

Table of Contents
Chapter 1: Fix the turntable
1: Perpetuum Ebner Musical 1
2: A Time to Kill and a Time to Heal
3: Preparation for Motor Drive
4: Motor control with Infineon Motor Shield and Arduino UNO
5: Turntable speed sample testbed with Arduino UNO
6: Turntable Speed Sensor design
7: Control Theory - End of Chapter 1
Chapter 2: First Enchantments
8: Digital Light Organ Enchantment
9: Autonomous Servo Lift
10: SMD Time - Solder the IR Speed Sensor PCB
11: Yelp - who can Help me to Compile and Run my First SAMA5D4 C Program
12: Son et Lumiere - End of Chapter 2
Chapter 3: Taming the Board
13: Breakthrough - Run my own C++ Program on the SAMA5D4
14: Digital Light Organ Input Buffer
15: SAMA5D4 Blinky
16: Scope Creep
17: Audio Sampling with 16-bit ADC ADS8343
18: Sending Files to SAMA5D4 over USB
19: Port my Light Organ from Arduino to SAMA5D4
20: Fast Fourier Transform on the SAMA5D4 - End of Chapter 3
Epilogue: Reaching for the Clouds
21: Right-Sizing my Plans
22: My Own C++ Buffered Sampler on the SAMA5D4
Interlude
23: Building In the Motorized Light Organ
24: Up to the Clouds with Yún
25: Publish or Perish
26: Turntable Finished
Stretch & Boni
Bonus 1a: Remote Light Organ with WiFI pt. 1
Bonus 1b: Remote Light Organ with WiFI pt. 2
Grande Finale: Paho MQTT Client on the SAMA5D4
Related blog
Vintage Turntable repair: Can I fix a Perpetuum Ebner from 1958
Review 1: Atmel SMART SAMA5D4 Xplained Ultra Unboxing and First Steps
Review 2: Atmel SMART SAMA5D4 Xplained Ultra - Building the Libraries from Source
Review 3: Digital Continuous Rotation (360°) Servo Part 1
Review 4: Digital Continuous Rotation (360°) Servo Part 2
Review 5: Atmel SMART SAMA5D4 Xplained Ultra - TCP/IP running
Review 6: Atmel SMART SAMA5D4 Xplained Ultra - LINUX Distro with SSH support
poem
Enchanted Objects: Let's work together to tame the ATMEL SMART SAMA5D4 Xplained Ultra kit
17 bis: Off South...
Review 7: Atmel SMART SAMA5D4 Xplained Ultra - C++ ADC Example on Linux
Review 8: Atmel SMART SAMA5D4 Xplained Ultra - Product Review
Review 9a: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 1
Review 9b: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 2
Review 10: Atmel SMART SAMA5D4 Xplained Ultra - New Content on AT91.com
1958 Turntable from the Black Forest - Summary of the Enchanted Player Story
Attachments:
Enchanted_Player_SAMA5D4.zip
https://community.element14.com/cfs-file/__key/communityserver-blogs-components-weblogfiles/00-00-00-01-17/fft_5F00_buckets.ods
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 10 years ago +1
    Finally got that video uploaded.
  • clem57
    clem57 over 10 years ago in reply to Jan Cumps +1
    git checkout -b dizzy -t remotes/origin/dizzy Should work
Parents
  • Jan Cumps
    Jan Cumps over 10 years ago

    Finally got that video uploaded.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to Jan Cumps

    Did my suggestion help?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to clem57

    I haven't retried to do a checkout with tag yet.

    My reason for checking out the source tree was because I was looking for an ADC buffer example.

    In stead of continuing the side track of checking out how to check out (sic) the code, I looked it up in a repo viewer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to clem57

    I'm retrying (still without a tag).

    It's not the build that fails for me but the fetch.

    I'm using the Yocto Project Development manual: http://www.yoctoproject.org/docs/1.8/dev-manual/dev-manual.html#local-yp-release

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to clem57

    For my own reference, commands used:

    git clone git://git.yoctoproject.org/poky
    cd poky

     

    git clone -b dizzy git://git.yoctoproject.org/poky.git

    (may be wrong, but the command on the AT91 site throws error. I may come back to this later

    C:\Atmel\yocto\poky>git checkout dizzy -b my_branch

    fatal: Cannot update paths and switch to branch 'my_branch' at the same time.

    Did you intend to checkout 'dizzy' which can not be resolved as commit?)

     

    git clone git://git.openembedded.org/meta-openembedded
    cd meta-openembedded
    git checkout origin/dizzy -b my_branch
    cd ..
    git clone git://github.com/meta-qt5/meta-qt5.git
    cd meta-qt5
    git checkout origin/master -b my_branch
    cd ..
    git clone git://github.com/linux4sam/meta-atmel.git meta-atmel
    cd meta-atmel
    git checkout origin/dizzy -b my_branch
    cd ..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to Jan Cumps

    git checkout -b dizzy -t remotes/origin/dizzy

    Should work

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 10 years ago in reply to Jan Cumps

    git checkout -b dizzy -t remotes/origin/dizzy

    Should work
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.