Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog 1958 Turntable from the Black Forest - 23: Building In the Motorized Light Organ
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 1 Jun 2015 12:26 PM Date Created
  • Views 877 views
  • Likes 3 likes
  • Comments 2 comments
  • enchanted_player
  • enchanted_objects
  • fft
  • adc
  • arduino
  • fast_fourier_transform
  • atmel
Related
Recommended

1958 Turntable from the Black Forest - 23: Building In the Motorized Light Organ

Jan Cumps
Jan Cumps
1 Jun 2015

image

 

In this episode, I'm combining the light organ and the servo control into one Arduino UNO..

It's also the first provisional attempt of mounting into the base of the turntable.

 

 

image

 

How the Light Organ and the Servo Lift Work Together

 

I want the light organ and the lift to just work together, without me having to worry about them.

In previous posts I have introduced the autonomous light organ and the autonomous lift.

They are now combined on a single Arduino, but still have a life of their own.

 

As soon as the music plays, the light organ will do its work and starts flashing its LEDs.

At the same time, it will tell the servo to move up and stay up for a while (its lifespan: 150 while loops).

Each time a LED is active, it renews the lifespan. But when there's no LED on, one point is taken from the lifespan.

If all the lifepoints are taken, the servo retreats and moves the LEDS back inside the case.

 

A video says more than 1000 words:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The code is simple. Search for the word decay to find out what's happening.

 

 

 

 

 

#include <Servo.h>
#include <fix_fft.h>


// servo declaration


Servo servo;


#define SERVO_PIN 9
#define SERVO_DELAY 25
#define SERVO_BASE 90
#define SERVO_TOP (SERVO_BASE + 61)


int servoPos = SERVO_BASE;
bool servoUp = false;






// light organ declaration


#define MUESTRAS 128           // Numero de muestras para el cálculo de la FFT
#define LOGM 7                 // Logaritmo en base 2 del número de muestras


#define BAJOS_MEDIOS 7         // Nº de banda para el corte entre Bajos y Medios
#define MEDIOS_AGUDOS 35       // Nº de banda para el corte entre Medios y Agudos


#define BPIN  13                // Pin de salida Bajos
#define MPIN  12               // Pin de salida Medios
#define APIN  11               // Pin de salida Agudos
#define TIMERPIN 8




#define MAX_PASADAS 10         // Nº de pasadas para el cálculo de los lÃmites


char data[MUESTRAS];           // Array con los valores muestreados (parte real)
char im[MUESTRAS];             // Array con los valores muestreados (parte imaginaria)


unsigned char salida[MUESTRAS/2];  // Valores obtenidos de la FFT (espectro de 64 bandas)
unsigned char bajos,medios,agudos; // Valores calculados para cada canal


byte  pasada,                            // nº de pasada para el cáculo de los lÃmites
      acumBajos,acumMedios,acumAgudos,   // acumuladores de veces que se supera el lÃmite
      limBajos,limMedios,limAgudos;      // lÃmites calculados para cada canal








// both:
// decay is a decreasing counter that tells how long the servo will stay up after the last led flashed.
// reset to DECAY each time a led lights up
// looses one live each time no leds are active
#define DECAY 150U
unsigned int uDecay = 0U;




// servo functionality


void servoInit() {
    servoUp = false;
    servo.attach(SERVO_PIN);
    servoPos = SERVO_BASE;
    servo.write(SERVO_BASE);
    delay(1000);
}


void servoGoUp() {

  if (servoPos < SERVO_BASE) {
    servoInit();
  }

  if (servoPos < SERVO_TOP) {
    servoPos++;
    servo.write(servoPos);
    delay(SERVO_DELAY);
  }
}


void servoGoDown() {

  if (servoPos < SERVO_BASE) {
    servoInit();
  }

  if (servoPos > SERVO_BASE) {
    servoPos--;
    servo.write(servoPos);
    delay(SERVO_DELAY);
  }
}


void servoGo() {
  if (servoUp) {
    servoGoUp();
  } else {
    servoGoDown();
  }
}




// light organ fuctions


/*
* Funcion que aplica una ventana de Hann a los datos muestreados para reducir el
* efecto de las discontinuidades en los extremos
*/
void aplicaVentana (char *vData) {
    double muestrasMenosUno = (double(MUESTRAS) - 1.0);
  // Como la ventana es simétrica , se calcula para la mitad y se aplica el factor por los dos extremos
    for (uint8_t i = 0; i < MUESTRAS/2 ; i++) {
        double indiceMenosUno = double(i);
        double ratio = (indiceMenosUno / muestrasMenosUno);
        double factorPeso = 0.5 * (1.0 - cos(6.28 * ratio));
  vData[i] *= factorPeso;
  vData[MUESTRAS - (i + 1)] *= factorPeso;
    }
}




void lightOrganSetup() {
    // Configuramos el prescaler a 32 -> 16Mhz/32 = 500 KHz
    // como cada conversion son 13 ciclos 500/13 ~ 38.4KHz
    // Es decir podemos medir en teoria hasta unos 19KHz,
    // que para este proyecto sobra.
    bitWrite(ADCSRA,ADPS2,1);
    bitWrite(ADCSRA,ADPS1,0);
    bitWrite(ADCSRA,ADPS0,1);


    // Como la señal es muy baja,utilizamos la referencia interna
    // de 1.1 V en vez de la de defecto de 5 V.
    analogReference(INTERNAL); 
  
    // Salidas para los canales de Bajos,Medios y Agudos
    pinMode(BPIN,OUTPUT);
    pinMode(MPIN,OUTPUT);
    pinMode(APIN,OUTPUT);
  
  
    // debug
    pinMode(TIMERPIN,OUTPUT);
    Serial.begin(9600);


    // Variables para el cálculo de los lÃmites
    pasada = 0;
    acumBajos = acumMedios = acumAgudos = 0;
    limBajos = limMedios = limAgudos = 50;

  }


void lightOrganGo() {
    // Realizamos el muestreo
//    Serial.println("Start sampling:");
    digitalWrite(TIMERPIN, HIGH);
    for( int i=0; i < MUESTRAS; i++) {
       data[i] = analogRead(0)/4 -128;  //Convertimos de 0..1024 a -128..127                               
       im[i] = 0;                       // parte imaginaria = 0                        
    }
    digitalWrite(TIMERPIN, LOW);
  
/*    
    {
    Serial.println(" samples\n");
    for( int i=0; i < MUESTRAS; i++) {
      Serial.print(data[i], DEC);
      Serial.print(",");
    }
    Serial.println(" ---");
  
    }
*/  


    // Aplicamos la ventana de Hann
    aplicaVentana (data);


/*
    Serial.println(" window\n");
    for( int i=0; i < MUESTRAS; i++) {
      Serial.print(data[i], DEC);
      Serial.print(",");
    }
    Serial.println(" ---");
*/
    // Calculamos la FFT
    fix_fft(data,im,LOGM,0);
  
    // Sólo nos interesan los valores absolutos, no las fases, asi que
    // calculamos el módulos de los vectores re*re + im*im.
    // Dado que los valores son pequeños utilizamos el cuadrado
    for (int i=0; i < MUESTRAS/2; i++){
       salida[i] = data[i] * data[i] + im[i] * im[i];
    }
/*
    Serial.println(" result\n");
     for( int i=0; i < MUESTRAS/2; i++) {
      Serial.print(salida[i], DEC);
      Serial.print(",");
    }
    Serial.println(" ---");
*/

    // Ahora repartimos las bandas entre las 3 salidas
    // En vez de sacar la media, utilizo sólo el valor máximo de
    // una banda
    bajos = 0;
    for (int i=2; i < BAJOS_MEDIOS; i++){
      bajos += salida[i];
    }
    bajos = bajos/2;
  
    medios = 0;
    for (int i=BAJOS_MEDIOS ; i < MEDIOS_AGUDOS; i++){
      medios += salida[i];
    }
    medios = medios/2;
  
    agudos = 0;
    for (int i=MEDIOS_AGUDOS; i < MUESTRAS/2; i++){
      agudos += 2*(salida[i]);   // jc 20150601 doubled the highs sesitivity
    }
    agudos = agudos/2;
  
   // Calculamos si el canal correspondiente
   // supera le lÃmite para encenderlo
   int siBajos  =  bajos  > limBajos;
   int siMedios =  medios > limMedios;
   int siAgudos =  agudos > limAgudos;

   digitalWrite(BPIN,siBajos ? HIGH : LOW);
   digitalWrite(MPIN,siMedios? HIGH : LOW);
   digitalWrite(APIN,siAgudos? HIGH : LOW);

   // Utilizamos las veces que se supera para
   // recalcular el lÃmite y evitar que con los
   // cambios de volumen los canales se saturen
   // o no funcionen.
   acumBajos  += siBajos;
   acumMedios += siMedios;
   acumAgudos += siAgudos;

   if ( ++pasada > MAX_PASADAS ) {
      pasada = 0;
      limBajos  = 20 + acumBajos*5;
      limMedios = 20 + acumMedios*5;
      limAgudos = 20 + acumAgudos*5;
      acumBajos  = 0;
      acumMedios = 0;
      acumAgudos = 0;
   }


   if (siBajos | siMedios /*| siAgudos*/) { // jc 20150601 renew lift up decay if a led is on,
                                            // ignore highs because I've made them more sensitive above
     uDecay = DECAY;
   } else if (uDecay > 0) {
     uDecay--;
   }

}


// arduino general


void setup()
{


  Serial.begin(9600);
  servoInit();
  lightOrganSetup();
//  Serial.println("Menu: Up: 1, Down: 0");
}


void loop()
{
  // lift debug
  while (Serial.available() > 0) {
    uDecay = (Serial.parseInt());
  }




  servoUp = (uDecay > 0);



  servoGo();
  lightOrganGo();

}

 

Next, I,ll move the code to a Yún and include MQTTing of the Highs, Mids and Lows info to the cloud.

 

 

Table of Contents
Chapter 1: Fix the turntable
1: Perpetuum Ebner Musical 1
2: A Time to Kill and a Time to Heal
3: Preparation for Motor Drive
4: Motor control with Infineon Motor Shield and Arduino UNO
5: Turntable speed sample testbed with Arduino UNO
6: Turntable Speed Sensor design
7: Control Theory - End of Chapter 1
Chapter 2: First Enchantments
8: Digital Light Organ Enchantment
9: Autonomous Servo Lift
10: SMD Time - Solder the IR Speed Sensor PCB
11: Yelp - who can Help me to Compile and Run my First SAMA5D4 C Program
12: Son et Lumiere - End of Chapter 2
Chapter 3: Taming the Board
13: Breakthrough - Run my own C++ Program on the SAMA5D4
14: Digital Light Organ Input Buffer
15: SAMA5D4 Blinky
16: Scope Creep
17: Audio Sampling with 16-bit ADC ADS8343
18: Sending Files to SAMA5D4 over USB
19: Port my Light Organ from Arduino to SAMA5D4
20: Fast Fourier Transform on the SAMA5D4 - End of Chapter 3
Epilogue: Reaching for the Clouds
21: Right-Sizing my Plans
22: My Own C++ Buffered Sampler on the SAMA5D4
Interlude
23: Building In the Motorized Light Organ
24: Up to the Clouds with Yún
25: Publish or Perish
26: Turntable Finished
Stretch & Boni
Bonus 1a: Remote Light Organ with WiFI pt. 1
Bonus 1b: Remote Light Organ with WiFI pt. 2
Grande Finale: Paho MQTT Client on the SAMA5D4
Related blog
Vintage Turntable repair: Can I fix a Perpetuum Ebner from 1958
Review 1: Atmel SMART SAMA5D4 Xplained Ultra Unboxing and First Steps
Review 2: Atmel SMART SAMA5D4 Xplained Ultra - Building the Libraries from Source
Review 3: Digital Continuous Rotation (360°) Servo Part 1
Review 4: Digital Continuous Rotation (360°) Servo Part 2
Review 5: Atmel SMART SAMA5D4 Xplained Ultra - TCP/IP running
Review 6: Atmel SMART SAMA5D4 Xplained Ultra - LINUX Distro with SSH support
poem
Enchanted Objects: Let's work together to tame the ATMEL SMART SAMA5D4 Xplained Ultra kit
17 bis: Off South...
Review 7: Atmel SMART SAMA5D4 Xplained Ultra - C++ ADC Example on Linux
Review 8: Atmel SMART SAMA5D4 Xplained Ultra - Product Review
Review 9a: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 1
Review 9b: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 2
Review 10: Atmel SMART SAMA5D4 Xplained Ultra - New Content on AT91.com
1958 Turntable from the Black Forest - Summary of the Enchanted Player Story
  • Sign in to reply
Parents
  • Workshopshed
    Workshopshed over 10 years ago

    Looks good, thanks for taking the time to upload the videos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 10 years ago

    Looks good, thanks for taking the time to upload the videos