Eye On Intelligence Challenge
  • Challenges & Projects
  • Design Challenges
  • Eye On Intelligence Challenge
  • More
  • Cancel
Eye On Intelligence Challenge
Blog Z7_Color_AID Blog #4: Architecture Discussion of Z7_Color_AID
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Eye On Intelligence Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: flyingbean
  • Date Created: 16 Nov 2024 2:53 AM Date Created
  • Views 395 views
  • Likes 5 likes
  • Comments 0 comments
  • video processing
  • arty z7
  • xilinx
  • dpu
  • Eye on Intelligence Challenge
  • pynq
  • vitis hls
Related
Recommended

Z7_Color_AID Blog #4: Architecture Discussion of Z7_Color_AID

flyingbean
flyingbean
16 Nov 2024

Table of Contents

  • Z7_Color_AID Project Background
  • Z7_Color_AID Project Introduction
  • Next Step of the Design Challenge
  • References

Z7_Color_AID Project Background

Detecting color is important for a lot of applications.  In self-driving cars, AI can help detect the traffic signals. For many industry applications, product color recognition can be used to sort products by a robot.  PYNQ_BNN can be used for fabric color/texture analysis.  There is a paper about color recognition with CNN algorithm[Reg[1]] in 2024. ML can be a good tool for color recognition related applications.

For this design challenge, I am going to explore color recognition from simple projects to PYNQ _BNN FPGA accelerator aided approach. The deadline of the challenge is the end of this week. After a short self-educated PYNQ_BNN training at home in the past month, I think I will need more time to fully understand the deep knowledge about PYNQ_BNN acceleration on FPGA platform and how to prepare datasets for a reliable PYNQ_BNN AI platform.  There will be two phases for Z7_Color_AID project. Phase one is a basic project which presenting what I learned on PYNQ platform under OpenCV framework. Phase two is an advanced project which will use PYNQ_BNN/DPU or other suitable algorithm/classifier accelerator on Zynq FPGA platform for color recognition and classification. I don’t think I can finish phase two project by end of this week. So The ML enabled Z7_Color_AID project will be implemented in the near future.

Z7_Color_AID Project Introduction

The initial Z7_Color_AID project idea was defined to recognize multiple colors for color-blind people. After learning more knowledge and features of PYNQ/OpenCV/ML, Z7_Color_AID project specification is evolved.  I would like to share my two project phases as below.

Initial Z7_Color_AID project specification: Multiple color detection in real time on PYNQ

I like LEDs, as well as color related projects. OpenCV has over 150 color space conversion methods in OpenCV (Ref [2]). Exploring color space conversion or recognition became my initial idea to join this design challenge.

RGB color space is the default color space.   In OpenCV, RGB color space is represented as BGR. This means that the order of the color channel in Blue, Green, and Red.  The initial Z7_Color_AID project was defined to use Arty-Z7-20 PYNQ framework to detect an object via a webcam. I planned to use what I learned from OpenCV framework on FPGA platform to extract the color information of the objects and label the color in the real time.

The basic architecture of Z7_Color_AID phase one project is illustrated below.

image

AMD/Xilinx does have Vitis Vision library for OpenCV. Element14 community provided quite a few blogs on this topic (Ref[3,4]). However, the overall flow of integrating AMD/Xilinx Vitis Vision library or HW accelerator into PYNQ does need manual work.  From what I read to accelerate color space manipulation on PYNQ, DPU is mostly needed. I do have strong interests to explore more on this path so that I can use Zynq FPGA as an accelerator for OpenCV related algorithm.  I hope I will find time to present another blog of this topic soon.

Updated Z7_Color_AID project specification: Traffic light detection

A good application of color recognition with ML is traffic light detection. I found that Boash Small Traffic Lights dataset (Ref[5]) can be a good candidate of the dataset for the project.  There were already some ML projects targeting traffic light detection/color recognition via Yolo_v3 or Yolo_v8 (Ref [6.7]).

I did attend online ML classes this month. I found that I did need more training of algorithms of BNN or YoLo_v3 before I could go through my customized ML training networking on Zynq FPGA. I prefer to use AMD/Xilinx HLS flow to create a customized BNN on the FPGA platform eventually.  Implementing DPU on Zynq FPGA can be very challenging from what I learned during this challenge journey. However, I think I did figure out a path to overcome the challenge. I only need more time to learn the flows in order to achieve my goal.

Next Step of the Design Challenge

 I will stick with my plan to finish  phase one project of Z7_Color_AID on time.

 

References

[1]  Color Recognition in Challenging Lighting Environments: CNN Approach             Nizamuddin Maitlo, Nooruddin Noonari, Sajid Ahmed Ghanghro, Sathishkumar Duraisamy, Fayaz Ahmed   2024 IEEE 9th International Conference for Convergence in Technology

[2] OpenCV Document, V4.10.0,                       https://docs.opencv.org/4.x/db/d64/tutorial_js_colorspaces.html                              2024

[3] ZYNQ Stereo Camera Platform - Part2 stereolbm with Vitis Vision libraries, /technologies/fpga-group/b/blog/posts/zynq-stereo-camera-platform---part2-stereolbm-with-vitis-vision-libraries                                                                                                           2020

[4] Learning Xilinx Zynq: Try to make my own Accelerated OpenCV Function - 1: Vitis HLS,    /technologies/fpga-group/b/blog/posts/learning-xilinx-zynq-try-to-make-my-own-accelerated-opencv-function---1-vitis-hls                                                                             2021

[5] https://github.com/bosch-ros-pkg/bstld                                                                                                                                           2017

[6] Detecting Traffic Lights in Real-time with YOLOv3.   https://github.com/berktepebag/Traffic-light-detection-with-YOLOv3-BOSCH-traffic-light-dataset                      2019

[7] traffic-lights-detection-and-color-recognition-using-yolov8 , https://github.com/farukalamai/traffic-lights-detection-and-color-recognition-using-yolov8                        2023

Previous Blogs:

Z7_Color_AID-Blog#01:First Impression of PYNQ on Arty-Z7-20

Z7_Color_AID Blog #2: Reproduce PYNQ Image on Ubuntu 20.04

Z7_Color_AID Blog #3: PYNQ Framework: Library and Overlay