Just Encase
  • Challenges & Projects
  • Design Challenges
  • Just Encase
  • More
  • Cancel
Just Encase
Blog Particulate Matter Monitoring System for Wildfires - #3: Circuitry and Assembly
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Just Encase to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gracemcnally
  • Date Created: 22 Jan 2022 4:28 PM Date Created
  • Views 2352 views
  • Likes 9 likes
  • Comments 8 comments
  • Arduino MKR WAN 1300
  • Hammond Manufacturing Enclosures
  • drone
  • particulate matter
  • just encase
Related
Recommended

Particulate Matter Monitoring System for Wildfires - #3: Circuitry and Assembly

gracemcnally
gracemcnally
22 Jan 2022

Up until now I have procured and tested all my sensors (see blog #2), so the next step is to put it all together! The last thing I wanted was to wire all my sensors together then have a bunch of problems I would have to troubleshoot at the same time. So, being the good little engineer in training that I am, I added each sensor one at a time and ran the test program for the sensor to make sure that everything was where it needed to be.

 

Transmitting device (drone-mounted):

Here is a sketch of the wiring for the transmitting device that will be mounted on the drone:

image

Power supply

One challenge in creating a power supply for my circuit was that the particulate matter (PM) sensor required 4.5-5.5V power input (but could still operate with 3.3V control) while the rest of the sensors worked with 3.3V power input. For the power supply, I obviously couldn’t use my laptop like I had been doing for the tests because it would be flying on the drone. The MKR 1300 board could operate off of a 3V battery input through the screw connector as long as the 5V pin didn’t need to be used. I used the battery assembly from a flashlight that uses 3 AAA batteries (1.5V each) in series as my power supply. For the 3V power supply to the board, I connected the positive wire after the second battery giving the required 3V. I connected the power supply of the PM sensor after the third battery giving the required 4.5V. I also added 0.1μF capacitors to the 3V and 4.5V power supplies from the batteries to filter out noise and protect the circuit and power supply.

 

PM and GPS sensors with I2C connections

The GPS and PM sensors communicate with the MKR 1300 board with I2C communication. This allows multiple devices to communicate through the same two pins (SCL and SDA). Each sensor also needed a power supply and ground connection. The PM sensor had a fifth connection, which when grounded indicated that the I2C operating mode was selected. To use I2C, pull-up resistors are required between the power (3.3 V) and the two communication lines (SCL and SDA). The GPS sensor had integral 2.2 kΩ pull-up resistors so no external pull-up resistors were required for the I2C connections.

 

Waterproof temperature sensor with 1-Wire connection

The waterproof temperature sensor communicated with the board with 1-Wire protocol which also allows multiple devices to communicate through the same port but uses only one digital pin for communication, in my case pin 5. A 4.7 kΩ pull-up resistor from the power (3.3V) to the communication line, as well as power and ground connections were also required.

 

TMP sensor

The TMP sensor was connected to analogue pin A6 and required power and ground connections.

 

LED

An LED was connected to digital pin 3 with a 220 Ω resistor to act as an indicator light.

 

Antenna

The antenna was connected to the board with a micro UFL connection.

 

Receiving device (ground device)

Because of a limited testing window, I didn’t end up including the LCD screen or indicator LEDs on the receiving board. Therefore, the wiring for the receiving device was simple. It was literally just the antenna with the micro UFL connection and the USB C cable that connected it to the laptop.

 

Physical Assembly

For the assembly, I had to install three cable glands in the Hammond enclosure: one for the antenna, one for the temperature sensor, and one for the particulate matter sensor, as these components were going to be mounted external to the enclosure. It was my first-time installing cable glands, but it was easy. I just drilled some holes and screwed the glands on. The next image shows what size hole I drilled for each gland.

imageimage


I threaded the wires through the cable glands which I tightened for a watertight fit around the wires. The breadboard had a sticker bottom, so I stuck it directly on the bottom of the enclosure. The antenna also imagehad a sticker back which I used to stick it to one side of the enclosure on the outside. For everything else, I used tape to make sure the components didn’t move around.

 image

After everything was assembled, I strapped it to the drone, and I was ready to go! Well not quite ready yet, I still have to talk about my code, but I’ll save that for the next blog post!

 image

  • Sign in to reply
Parents
  • beacon_dave
    beacon_dave over 4 years ago

    Spotted this which may be of interest given the hot topic of prop wash on your sensor readings.

    Wildfire Meteorology: Drones Provide a Better, Cheaper Way to Understand Fire Risk
    https://dronelife.com/2020/11/11/wildfire-meteorology-drones-provide-a-better-cheaper-way-to-understand-fire-risk/

    "...The solution was to install a carbon-fiber boom, which positioned the sensor at a distance of about two times the propeller width away from the body of the UAV, to eliminate some of the influences of the prop wash..."

    Also mentioned is the issue of extreme updraft from the fire front on small drones, but I guess you weren't planning on getting that close.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 4 years ago

    Spotted this which may be of interest given the hot topic of prop wash on your sensor readings.

    Wildfire Meteorology: Drones Provide a Better, Cheaper Way to Understand Fire Risk
    https://dronelife.com/2020/11/11/wildfire-meteorology-drones-provide-a-better-cheaper-way-to-understand-fire-risk/

    "...The solution was to install a carbon-fiber boom, which positioned the sensor at a distance of about two times the propeller width away from the body of the UAV, to eliminate some of the influences of the prop wash..."

    Also mentioned is the issue of extreme updraft from the fire front on small drones, but I guess you weren't planning on getting that close.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • gracemcnally
    gracemcnally over 4 years ago in reply to beacon_dave

    I just read the article, it's very interesting! Having the sensor out to the side would certainly be necessary for measuring wind velocity like they were in that article. The prop wash was something that I had in mind as I was designing my system but if I were to use this in real wildfire applications, even if the air was locally mixed, I would probably still be able to measure particulate matter variability on a large scale. Also, the particulate matter sensor has an internal fan which controls the flow rate past the sensing element so it's measuring concentration and not just particle count anyway. In response about the updraft, you're right, the drone wouldn't be able to fly directly above the fire, and even if it could, the sensors and the drone might not be able to handle the extreme heat anyway.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to gracemcnally

    A simple test might to be to do a candle test with the drone suspended (motors not running) vs the drone hovering (motors running).

    If there is a noticeable difference then try the hover test again but with the sensor in a different position.

    • Cancel
    • Vote Up 0 Vote Down