Low Power IoT Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Low Power IoT Design Challenge
  • More
  • Cancel
Low Power IoT Design Challenge
Blog Low Power IoT Design Challenge - Getting Started
  • Blog
  • Forum
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Blog Post Actions
  • Subscribe by email
  • More
  • Cancel
  • Share
  • Subscribe by email
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 7 Sep 2021 3:17 AM Date Created
  • Views 318 views
  • Likes 11 likes
  • Comments 7 comments
  • infineon
  • low_power_iot
  • cy8ckit-028-epd
  • cy8ckit-psoc62s2-43012
  • cypress modus toolbox 2.3
Related
Recommended

Low Power IoT Design Challenge - Getting Started

ralphjy
ralphjy
7 Sep 2021

I just received my Challenge Kit (PSoCTm 6S2 + AIROCTm Wi-Fi/Bluetooth Pioneer Kit) via UPS yesterday (9/2) - thanks danzima .  I commented to my wife that the box seemed a bit heavy for a small dev-board.  I was pleasantly surprised to find extra goodies that Infineon had provided .  Thanks Infineon for the lab notebook, pen and Hydro Flask insulated bottle.

 

I've decided to create this intro post "on the fly", so I probably won't publish it for a few days.  I'd like to be able to get the toolchain installed and a few examples working first.

 

Toolchain Installation

Application development for the PSoC 62S2 kit is supported currently by the ModusToolbox and Mbed OS tool environments.  This challenge requires that we use the ModusToobox, so I'll start by downloading the latest available version (2.3 plus 2.31 patch).  The Windows Installer made the install easy, but took quite a few minutes and installed about 3GB of files.

 

ModusToolbox runs with either a graphical user interface (GUI) or a command-line interface (CLI).  To get started I am going to use the Eclipse-based IDE (GUI).

 

 

mtw - Eclipse IDE for ModusToolbox

The IDE has a "Quick Panel" that provides easy access to frequently used tools to create, build and run application programs.

 

The Project Creator tool is invoked by selecting "New Application" in the Quick Panel.  Project Creator uses a Board Support Package (BSP) to generate all the necessary configuration files for the IDE.  It makes it extremely easy to switch between different boards for different projects.  In this case I selected the CY8CKIT-062S2-43012.

 

Once the BSP is selected, you have access to an Application Directory that contains sample applications that are available for that board configuration.  Selecting a sample application will create a project with all the required files for that project (source code, makefile, dependent libraries, etc).  If you build an application from scratch, there is a Library Manager that will allow you to add required libraries.  As usual, to test the installation and the tool pipeline, a good place to start is the "Hello World" project.

 

Hello World is the standard "blink the LED" demo.  In this case you can pause the blinking over the serial link.  Here is a quick demo with the board superimposed on the putty serial window, so you can see the serial response and the LED reaction..

You don't have permission to edit metadata of this video.
Edit media
x
Upload Preview

 

 

E-Ink Display Shield

I'll get into the description of my project in the next post, but one item that I definitely wanted to include was a display.  There are two Arduino format display shields available for this board.  The CY8CKIT-028-TFT board has a 2.4" Color TFT 320x240 display.  The CY8CKIT-028-EPD E-INK board has a 2.7" Monochrome E-Paper 264x176 display.  Both shields also have single PDM microphones and a motion sensor.  Since this is a "low power" challenge, I opted for the E-INK shield.

 

Modus Toolbox has an emWin E-Ink FreeRTOS application example that I used to check out the board.

 

Here is a short video of the emWin graphics demo.

You don't have permission to edit metadata of this video.
Edit media
x
Upload Preview

 

 

And the requisite hack to start off the challenge adventure .

 

 

Looking forward to seeing what everyone implements!

Anonymous

Top Comments

  • javagoza
    javagoza 9 months ago +4

    I'm so envious, Ralph, ha ha  . It seems to be a very interesting board. Any clues about what your project is about?

  • maxpowerr
    maxpowerr 9 months ago +3

    Good start. I will root for your project.

  • ralphjy
    ralphjy 9 months ago in reply to javagoza +3

    This summer I've been focused on trying tinyML with different development hardware and software. I hope to use ModusToolbox Machine Learning with audio and vision processing.  There appears to only…

  • javagoza
    javagoza 9 months ago

    I'm so envious, Ralph, ha ha . It seems to be a very interesting board. Any clues about what your project is about?

    • Cancel
    • Up +4 Down
    • Reply
    • More
    • Cancel
  • maxpowerr
    maxpowerr 9 months ago

    Good start. I will root for your project.

    • Cancel
    • Up +3 Down
    • Reply
    • More
    • Cancel
<