Path II Programmable
  • Challenges & Projects
  • Design Challenges
  • Path II Programmable
  • More
  • Cancel
Path II Programmable
Blog Do Not Hide the Problem - A Correct SW Lab 7 Solution
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: cmelement14
  • Date Created: 2 Nov 2019 3:26 AM Date Created
  • Views 951 views
  • Likes 5 likes
  • Comments 5 comments
  • path ii programmable
Related
Recommended

Do Not Hide the Problem - A Correct SW Lab 7 Solution

cmelement14
cmelement14
2 Nov 2019

  • SW Lab 7 Problem Description
  • A Correct SW Lab 7 Solution
image

 

 

SW Lab 7 Problem Description

 

Like other people reported here and there, I noticed the same problem in Experiment 2, SW Lab 7: the peripheral test application stuck at the point of showing message "Running Interrupt Test  for psu_csudma..." (shown in the screenshot below).

image

 

However, we did a similar peripheral test application in Experiment 3, SW Lab 5. The only difference between them is: in lab 5, the build configuration is Debug while in lab 7 the build configuration is Release. In lab 5, the test completed successfully (as shown in the screenshot below).

image

 

What's the difference between Release configuration and Debug configuration? A couple of major differences: with and without compiler optimization AND without and with debugging information. With and without debugging information should usually NOT make any behavior change. Thus, I think the problem is due to the optimization for Release configuration and the Debug version has no problem just like Experiment 3, SW Lab 5. To confirm the problem doesn't exist in Debug configuration, I slightly modified the Create Boot Image settings regarding the folder path of application binary: before the modification, we use the binary from the release folder and then we changed it to the debug folder (Please refer the highlighted difference in the following two screenshots). The test result confirmed that the BOOT.bin using the debug version application code had successfully completed the whole test.

image

 

image

 

I didn't use the solution provided in the training materials, but in P2P: SW Lab 7 Road Block blog, nerdyupdates reported the provided solution basically hides the problem (maybe because the lab creator observed the same problem and couldn't find a solution). It is very common in embedded development that a working debug version of application code stops working after switching to a release version. Usually it's because of the compiler optimization.

 

 

A Correct SW Lab 7 Solution

 

Let's take a look at the highlighted line 244 shown below. What do you think the compiler optimization will do for that line? It will generate assembly code that reads the variable DsDone just once and uses this value to check the condition (i.e., DsDone == 0) forever. It will NOT update DsDone. The reason is because the compiler optimizer considers variable DsDone doesn't change at all in the context. However, as programmer, we know the variable has to change somewhere else. Otherwise, this is a dead loop which is definitely not the programmer's intention.

image

 

How can we let the optimizer know our intention? Here's the solution - adding keyword volatile before the declaration of variable DsDone (as highlighted below). Basically, the keyword tells the optimizer not do any optimization in any reference to variable DsDone.

image

 

Test result confirmed the BOOT.bin including the above modification had successfully completed the whole peripheral test. Hope I clearly explained the problem and the solution. Please comment with your feedback or questions.

  • Sign in to reply

Top Comments

  • aspork42
    aspork42 over 6 years ago +2
    Great write up - I just found this last night. The part that worried me about it is that running this test disables the fan. The processor then deadlocks and turns into a little heater. I ended up with…
  • nerdyupdates
    nerdyupdates over 6 years ago +1
    Nice investigation into this. Thanks for sharing your knowledge on compiler optimization. One question which may not have a simple answer, but why is the "while" statement not enough for the compiler to…
  • cmelement14
    cmelement14 over 6 years ago in reply to nerdyupdates +1
    Please remember compiler itself doesn't have any intelligence so it doesn't understand programmer's intention. It does optimization based on rules given by the creator of the compiler. Ok, let's first…
Parents
  • aspork42
    aspork42 over 6 years ago

    Great write up - I just found this last night. The part that worried me about it is that running this test disables the fan. The processor then deadlocks and turns into a little heater.

     

    I ended up with the error messages shown here:

    Temperature Alarm(0) HIGH Threshold is 52.700 Centigrade.

    Temperature Alarm(0) LOW Threshold is 42.698 Centigrade.

    VCCINT Alarm(1) HIGH Threshold is 0.637 Volts.

    VCCINT Alarm(1) LOW Threshold is 1.037 Volts.

    VCCAUX Alarm(3) HIGH Threshold is 1.597 Volts.

    VCCAUX Alarm(3) LOW Threshold is 1.997 Volts.


    Alarm 0 - Temperature alarm has occured


    The Current Temperature is 63.075 Centigrade.

    The Maximum Temperature is 63.658 Centigrade.

    The Minimum Temperature is 62.516 Centigrade.

     

    So the MPSoC was over 10 Deg C higher than its threshold... Hopefully nothing got cooked too badly.

     

    I can see you had this in your screenshot as well; but it wasn't as hot as mine got...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aspork42
    aspork42 over 6 years ago

    Great write up - I just found this last night. The part that worried me about it is that running this test disables the fan. The processor then deadlocks and turns into a little heater.

     

    I ended up with the error messages shown here:

    Temperature Alarm(0) HIGH Threshold is 52.700 Centigrade.

    Temperature Alarm(0) LOW Threshold is 42.698 Centigrade.

    VCCINT Alarm(1) HIGH Threshold is 0.637 Volts.

    VCCINT Alarm(1) LOW Threshold is 1.037 Volts.

    VCCAUX Alarm(3) HIGH Threshold is 1.597 Volts.

    VCCAUX Alarm(3) LOW Threshold is 1.997 Volts.


    Alarm 0 - Temperature alarm has occured


    The Current Temperature is 63.075 Centigrade.

    The Maximum Temperature is 63.658 Centigrade.

    The Minimum Temperature is 62.516 Centigrade.

     

    So the MPSoC was over 10 Deg C higher than its threshold... Hopefully nothing got cooked too badly.

     

    I can see you had this in your screenshot as well; but it wasn't as hot as mine got...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • cmelement14
    cmelement14 over 6 years ago in reply to aspork42

    I definitely noticed that the fan stopped when running this test. I suspected the temperature would go very high, so every time after running the application, I unplugged the power and didn't let it run very long time at all. That's why my board's temperature didn't go as high as yours.

     

    Sorry, I forgot to mention this and hope no damage to your board.

    • Cancel
    • Vote Up +1 Vote Down