Path to Programmable 3
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable 3
  • More
  • Cancel
Path to Programmable 3
Blog Path to Programmable III Training Blog #04: Build a simple User API for Petalinux and Need Support for GPIO UIO API under Petalinux
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Path to Programmable 3 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: flyingbean
  • Date Created: 23 Jul 2023 5:56 PM Date Created
  • Views 1699 views
  • Likes 6 likes
  • Comments 2 comments
  • zynq
  • xilinx
  • fpga
  • Path to Programmable 3
  • minized
Related
Recommended

Path to Programmable III Training Blog #04: Build a simple User API for Petalinux and Need Support for GPIO UIO API under Petalinux

flyingbean
flyingbean
23 Jul 2023

Table of Contents

  • Objectives
  • Background Knowledge about Petalinux Drivers
  • Build Simple User APIs for Petalinux Project  
  • Conclusions

Objectives

I continued to use Lab 7 Vivado project to build a couple of simple user APIs under Petalinux environment. I don’t have a PMOD module, HTU21D, for Avnet MiniZed TTC Petalinux training labs. I tried to integrate PWM LED module into Petalinux to learn how to integrate a peripheral into MiniZed Petalinux system.

However, after a couple of days’ iterations, my GPIO UIO driver was not integrated into Petalinux successfully. I basically followed the guidance from Roy Meesigner blog[1]: GPIO and Petalinux (Embedded Linux, Yocto based). At the end of the day, I decided to publish this blog and would like to get supports from Element14.com Community on GPIO UIO API topic. It is a learning-by-doing process.

Background Knowledge about Petalinux Drivers

Let us review Lab 7 HW design first. Fig 1 is copied from my blog 3 on this topic, which illustrates Lab 7 HW design at Vivado flow.

image

Fig 1. Lab 7 Vivado HW Design Block Diagram

PWM_w_init_0 module is the targeted peripheral to be integrated into Petalinux now. PWM_w_init_0 is a simple AXI bus add-on GPIO module. The flow to integrate it into Petalinux might not be as simple as the initial thinking. There are several dependencies to be covered before we jump into Petalinux flow.

  1. Kernel and Layers

A brief overview of the embedded Linux system is helpful for integrating a peripheral into a Linux OS. One embedded Linux OS can be divided into three layers: User API/space, kernel space and hardware(HW) components.

image

Fig 2. A Simplified Structure of Embedded Linux OS (Ref from Wikipedia)

Kernel space is the center layer to connect the HW components with user space or APIs. AMD/Xilinx Petalinux GUI can help us with the kernel configuration without deep knowledge of the kernel building blocks. In general, the kernel takes care of memory management, scheduling access to different peripherals, such as input/output support. User applications cannot talk to HW components without kernel support.

From AMD/Xilinx documents, SysFs driver is a common framework for accessing various GPIOs at user space/APIs.

2. Device Tree

Device tree are a database for a kernel to manage the HW components’ interface. A proper device tree file can make the associated HW component accessible by the kernel, then by the user APIs.

3. HW components

A finished Vivado project provides all the information for the HW layer in the Petalinux flow. As today’s Vitis tool chain, XSA file contains HW component information and is used as the input for building a Petalinux project.

Build Simple User APIs for Petalinux Project  

1. A simple user API to let Petalinux print out a Hello World string after MiniZed booting up

     The basic procedure to create a Petalinux is similar to Blog 3.

Step 01: Create a Petalinux project  

$ petalinux-create --force --type project --template zynq --name MiniZed_UIO_LED

Step 02: Configure Vivado/Petalinux hardware

 

$ petalinux-config --get-hw-description=../

Step 03: Create User API

$ petalinux-create -t apps --name linuxapi
 

Configure rootfs

 

$ petalinux-config -c rootfs

Petalinux GUI will let us to select linuxapi app into user space as below.

image

Fig 3. Petatlinux Rootfs: apps configuration

Step 04: Build Petalinux Images

$ petalinux-build

After generating booting image artifacts, I am able to boot MiniZed from JTAG port as my blog 3 instructed. Here is the snapshot to get a Hello World API running on Petalinux.

image

Fig 4. Hello World Linux API Working

 2. The second user API is to create a PL GPIO API driver to dim PL LED on MiniZed after Petalinux booting up.

Step 1-2 is same as previous to create Petalinux project.

Step 3: Configure kernel

$ petalinux-config -c kernel

I did select GPIO UIO setting as below, which should mount GPIO UIO at MiniZed initial booting phase.

image

Fig 5. GPIO UIO Rootfs Configuration

Step 4: Create GPIO UIO API

$ petalinux-create -t apps --name gpio-dev-mem-test

I used Avnet source file, gpio-dev-mem-test.c to testing the UIO API which is same as Roy Meesigner blog. The source code is attached.

/*
 * This test application is to read/write data directly from/to the device 
 * from userspace. 
 * 
 */
#include <stdio.h>
#include <stdlib.h>
#include <unistd.h>
#include <sys/mman.h>
#include <fcntl.h>

#define IN 0
#define OUT 1

void usage(void)
{
	printf("*argv[0] -g <GPIO_ADDRESS> -i|-o <VALUE>\n");
	printf("    -g <GPIO_ADDR>   GPIO physical address\n");
	printf("    -i               Input from GPIO\n");
	printf("    -o <VALUE>       Output to GPIO\n");
	return;
}

int main(int argc, char *argv[])
{
	int c;
	int fd;
	int direction=IN;
	unsigned gpio_addr = 0;
	int value = 0;
	
	unsigned page_addr, page_offset;
	void *ptr;
	unsigned page_size=sysconf(_SC_PAGESIZE);

	printf("GPIO access through /dev/mem.\n", page_size);

	/* Parse command line arguements */
	while((c = getopt(argc, argv, "g:io:h")) != -1) {
		switch(c) {
		case 'g':
			gpio_addr=strtoul(optarg,NULL, 0);
			break;
		case 'i':
			direction=IN;
			break;
		case 'o':
			direction=OUT;
			value=atoi(optarg);
			break;
		case 'h':
			usage();
			return 0;
		default:
			printf("invalid option: %c\n", (char)c);
			usage();
			return -1;
		}
		
	}

	if (gpio_addr == 0) {
		printf("GPIO physical address is required.\n");
		usage();
		return -1;
	}
	
	/* Open /dev/mem file */
	fd = open ("/dev/mem", O_RDWR);
	if (fd < 1) {
		perror(argv[0]);
		return -1;
	}

	/* mmap the device into memory */
	page_addr = (gpio_addr & (~(page_size-1)));
	page_offset = gpio_addr - page_addr;
	ptr = mmap(NULL, page_size, PROT_READ|PROT_WRITE, MAP_SHARED, fd, page_addr);

	if (direction == IN) {
	/* Read value from the device register */
		value = *((unsigned *)(ptr + page_offset));
		printf("gpio dev-mem test: input: %08x\n",value);
	} else {
	/* Write value to the device register */
		*((unsigned *)(ptr + page_offset)) = value;
	}
	

	munmap(ptr, page_size);

	return 0;
}

Step 5: Update device tree

I need to update system-usr.dtsi for gpio UIO node. The file can be found from the hiercharch as below.

image

Fig 6. Hierarchy Location of system-user.dtsi

Here is the snippet of the updated device tree.

/include/ "system-conf.dtsi"
/ {
 chosen {
		bootargs = "earlycon consol=ttyPS0,115200 earlyprintk clk_ignore_unused uio_pdrv_genirg.of_id=generic-uio";
		stdout-path = "serial0:115200n8";
	};  
};


 &amba {
    	ptm@f889d000 {
    		cpu = <&cpu0>;
    	};
    };


&PWM_w_Int_0 {
        compatible = "generic-uio";   
        status = "okay";
   };

Step 6: Configure rootfs

$ petalinux-config -c rootfs

After Petalinux GUI pop up, selet app: gpio-dev-mem-test,  as Fig 3 shew.

Step 7: Build Petalinux Image and test APIs

$ petalinux-build 

After using JTAG to load the Petalinux images into MiniZed, I cannot find UIO populated under /sys/class/uio.

image

Fig 7. No PL GPIO Node Populated on MiniZed

I can only find gpiochip906 under /sys/class/gpio, which is PS GPIO for PS LED.

My very first GPIO UIO API on MiniZed was failed for now.

Conclusions

I learned how to use Petalinux to create a simple Linux version, Hello World API, which can be called at user space. However, I was not able to create a UIO API to call PL GPIO at user space. I think the root cause was the kernel configuration, which was not properly implemented. Vivado HW design should be fine since baremetal API was successfully running on MiniZed. I do need some advises from our community to fix the issues.

References

[1] https://www.hackster.io/Roy_Messinger/gpio-and-petalinux-embedded-linux-yocto-based-c71773

  • Sign in to reply
Parents
  • javagoza
    javagoza over 2 years ago

    flyingbean  Hi I think these links will be interesting for you, I have not been able to dedicate time to review them.

    Linux GPIO Driver - Xilinx Wiki - Confluence (atlassian.net)

    AXI GPIO - Xilinx Wiki - Confluence (atlassian.net)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • javagoza
    javagoza over 2 years ago

    flyingbean  Hi I think these links will be interesting for you, I have not been able to dedicate time to review them.

    Linux GPIO Driver - Xilinx Wiki - Confluence (atlassian.net)

    AXI GPIO - Xilinx Wiki - Confluence (atlassian.net)
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.