<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/"><channel><title>Lost start Blog #1</title><link>/challenges-projects/design-challenges/pathprogrammable3/b/blog/posts/lost-start</link><description>I received the kit for the Path to Programmable 3 rather quickly compared with other kits I received for RoadTesting. Usually, it took several days until I could get the kit in my hand, and several emails needed to be exchanged with the customs offic</description><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>RE: Lost start Blog #1</title><link>https://community.element14.com/challenges-projects/design-challenges/pathprogrammable3/b/blog/posts/lost-start</link><pubDate>Tue, 18 Jul 2023 07:26:33 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:63f6b0c5-4e0e-4f9e-b620-c8f34a08dfb4</guid><dc:creator>javagoza</dc:creator><slash:comments>0</slash:comments><description>&lt;p&gt;Oh! I went through the same path, I tried it with an external ssd from samsung that I now have working internally on another machine and without success with the installation of Vivado ML, neither by network nor by downloading the entire installer. In the end I had to salvage an old 1TB HDD which is working fine except creating a small 2.9GB PetaLinux image takes more than 8 hours.&lt;/p&gt;
&lt;p&gt;I&amp;#39;m sorry I didn&amp;#39;t discuss those issues on the forums, it was 2 months before I was selected for the challenge.&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=26508&amp;AppID=395&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item><item><title>RE: Lost start Blog #1</title><link>https://community.element14.com/challenges-projects/design-challenges/pathprogrammable3/b/blog/posts/lost-start</link><pubDate>Mon, 17 Jul 2023 23:59:53 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:63f6b0c5-4e0e-4f9e-b620-c8f34a08dfb4</guid><dc:creator>shabaz</dc:creator><slash:comments>0</slash:comments><description>&lt;p&gt;Hi,&lt;/p&gt;
&lt;p&gt;Glad you&amp;#39;re making progress. It sounds like it could be a faulty SSD, since it works with the new HDD. It might be worth returning the SSD, just in case. I have only ever installed Vitis on an SSD(I&amp;#39;ve not bought a HDD in a decade) so can&amp;#39;t see why it would have failed on one but not the other. Maybe it&amp;#39;s some other incompatibility at the PC/drive level.&lt;/p&gt;
&lt;p&gt;VirtualBox occasionally has issues, especially regarding compatibility with VMware.Also VMWare Workstation is a pain because although technically&amp;nbsp;that works well, it invariably needs an upgrade every few years otherwise the latest OS&amp;#39;s (e.g. the latest Ubuntu release etc) won&amp;#39;t install properly, and the cost is therefore too much.&lt;/p&gt;
&lt;p&gt;For perhaps the past 5 years, I&amp;#39;ve used a simple setup: A separate PC or server (it can be a very small PC; I use an Intel NUC, they are cheap used from ebay), running ESXi (and local vCenter), which is a type-1 hypervisor so there is no host OS cost or complication. It is all a free install on a single server, so there&amp;#39;s no additional cost, and it&amp;#39;s&amp;nbsp;been reliable. The performance impact is tiny (maybe a few percent).&amp;nbsp;I liked that it doesn&amp;#39;t require a lot of expense,&amp;nbsp;because&amp;nbsp;just a single&amp;nbsp;VM can be run if that VM needs a lot of resources (RAM, CPU etc).&amp;nbsp;From my perspective I&amp;#39;ve had good results for at least the past 5 years or so, I am happy with this solution.&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=26508&amp;AppID=395&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item></channel></rss>