Challengers are tasked with pushing the limits newly unleashed M0 Dual Core on the PSoC 62S4 with Infineon’s ModusToolbox Platform.
Save The Bees Design Challenge.
1 in 4 species of Bees are at risk of extinction, Engineers heed the call!
element14 Community will be exhibiting at electronica 2022 within the Premier Farnell Avnet Booth and announcing their Save the Bees Challenge.
Using Arduino MKR1310 and Arduino Pro Nicla Vision Boards, engineers are invited to solve the issues facing the global Bee population and win prizes.
Did you know 1 in 3 bites of food have been pollinated by Bees, This shows how important it is to maintain global Bee Populations.
Launching November 15th 2022 at Electronica 2022.
Visit Us Farnell’s Stand (Hall C2 -101 in the Avnet Village).
MayerMakes will be exhibiting his first prototype project to help combat Braulidae, or Bee Lice, within Bee hives.
Phil and MayerMakes will be present to talk about the element14 Community, as well as Announce the Save The Bees Challenge and Demo the Bee Lice Project.
https://uk.farnell.com/electronica
Examples of qualifying projects can include and are not limited to:
- Run low power applications on the Cortex-M0+, then wake the Cortex-M4 for more complex tasks requiring additional processing power
- Using the separate cores for code isolation & security
- Run trusted firmware on dedicated core
- Run communication on the Cortex-M0+ while running more complex processes on the Cortex-M4
- Porting other OS to run on the PSoC 62 microcontroller
- Applications with the Cortex-M0+ core measuring values and the Cortex-M4 visualizing or processing the data
Challenger Kit
We will be giving away 25 of each of the following items:
The Sponsored Kit | The Specs |
---|---|
Buy Now |
|
Arduino MKR WAN 1310 |
Arduino MKR WAN 1310 board provides a practical and cost effective solution to add LoRa® connectivity to projects requiring low power. This open source board can be connected to: the Arduino IoT Cloud, your own LoRa® network using the Arduino LoRa® PRO Gateway, existing LoRaWAN infrastructure like The Things Network, or even other boards using the direct connectivity mode.
|
*Or local equivalent
**Grand Prize and Runner Up winners also earn the finisher prize.
element14 Community Judges element14 Community Team |
|
Technical Judges nearBees https://www.nearbees.de/ |
Project Phases | Dates |
---|---|
Application Period | 10th October 2022 |
Live Webinar | 10th November 2022 |
Application Deadline | 24th November 2022 |
Challengers Announced | 28th November 2022 |
Build Period | 28th November 2022 - 6th February 2023 |
Projects Due | 6th February 2023 |
Winners Announced | February 2023 |
Prizes Shipped | February 2023 |
Selected official applicants will be chosen to receive the "Kit" listed above; these successful applicants will be our sponsored challengers. The sponsored challengers must use the PSoC 62S4 Pioneer Kit within their project, and publish their final code and designs on the Community for others to use. Those not chosen as sponsored challengers may also join the competition and be eligible to win prizes, but they must base their projects around the PSoC 62S4 Pioneer Kit and adhere to all terms and conditions of the challenge.
Applicants must post their progress and final project as at least 5 blog posts before the closing date (see above), when projects are due. Challengers are strongly encouraged to post their blogs regularly during the contest period, rather than posting them all close to the finish of the competition.
Projects that Demonstrate use of both M0 and M4 cores in their project.most creatively, along with posts that are media rich with photos, videos, and code samples will be viewed more favorably in the judging process.
The sponsored challengers must us ModusToolbox as well as Demonstrate use of both M0 and M4 cores in their project.
Challengers must post their progress and final project as at least 5 blog post before the closing date. Posts which show inter-core communication and are media rich with Photos, Videos and Code samples will be viewed more favorably in the Judging Process
Please read the full terms and conditions of the challenge, attached below.
Ready to join the challenge? Then apply here!
If you are not successful in becoming a sponsored challenger, but still want to enter, all you need to do is use the PSoC 62S4 Pioneer Kit as described above in your project and adhere to the same Terms and Conditions for a chance to be our winner! Non-sponsored challengers are eligible for the Finisher and Winner Prizes, as well.