Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Meditech: First step preparing the prototype container
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 27 May 2015 10:48 PM Date Created
  • Views 637 views
  • Likes 4 likes
  • Comments 3 comments
  • assembling_prototype
  • box
  • container
  • internal_architecture
Related
Recommended

Meditech: First step preparing the prototype container

balearicdynamics
balearicdynamics
27 May 2015

Starting from the selected box that will host the Meditech prototype components the first step has been to prepare the container to host the prototype components. First of all the setting of the cooling fan. The following image shows the general idea on how to use one of the two sides of the box. The other side will contain the default probes, accessories etc.

 

image

image

A modular system

To keep the system totally modular, every specialised device (based on the Raspberry PI) is hosted on one of the yellow frames. The central zone will host the cooling system only because it will contain several control components, a status display, status leds and so on.

 

Every RPI unit is simple to install and replace for any reason and to keep the things more simple the standard connectors will left untouched so that any non-expert user can repair a unit simply replacing the entire block.

 

A mechanical microswitch should disable the entire powering until the top lid is not closed.

 

The air circulation is granted by a 12 cm PWM controlled fan and the frames will be adapted to permit to the cooling system to work properly; the fan will start at a sensor detect a critical temperature.Temperature and switch will work autonomously controlled by a program running on the ChipKit PI board that also control the led and other display feedback - despite the LCD monitor - interacting with the RPImaster that controls the entire networked system.

The storage and network hub should be fixed in the center area - together with the powering system - as they will cable the entire system.

 

First modification: the cooling system

The following three images shows the installation of the fan and the preparation of the forced air circulation.

imageimageimage

  • Sign in to reply

Top Comments

  • Former Member
    Former Member over 10 years ago +1
    Nice to see the project coming along!! That case is amazing.. The compartments allow for a very clean layout. In your opinion, could this case be used to house a full desktop computer?? Lucie
  • Former Member
    Former Member over 10 years ago in reply to balearicdynamics +1
    Yep!! I've had a flitty couple of weeks, struggling to find some time to myself!! But yes back now and a bit late with my own project...:( To make things worse, my main computer started going a bit wonky…
Parents
  • Former Member
    Former Member over 10 years ago

    Nice to see the project coming along!!

     

    That case is amazing.. The compartments allow for a very clean layout.

     

    In your opinion, could this case be used to house a full desktop computer??

     

    Lucie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to Former Member

    You are welcome Lucie!

     

    After a momentary lapse of present you are here again image

    In my opinion yes, this case may fit a lot of things. I have found it on amazon at a very reasonable price respect the brand and quality (take a look here  http://www.amazon.es/gp/product/B00F2J9GBS?psc=1&redirect=true&ref_=oh_aui_detailpage_o00_s00) and when I received it it was better than expected. Then the material I think it is exceptional one: absolutely simple to manage, cut, make holes and any change but extremely robust.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to balearicdynamics

    Yep!! I've had a flitty couple of weeks, struggling to find some time to myself!! But yes back now and a bit late with my own project...:(

    To make things worse, my main computer started going a bit wonky so I switched it of and now it's dead... I'm in the process of replacing it (i've had a new motherboard etc... for a while I've been meaning to put in so that's taking up this evening!). I think it's likely to be a powerpack fault so once i'm finished it's time to open it up and have a look at what went wrong!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Former Member
    Former Member over 10 years ago in reply to balearicdynamics

    Yep!! I've had a flitty couple of weeks, struggling to find some time to myself!! But yes back now and a bit late with my own project...:(

    To make things worse, my main computer started going a bit wonky so I switched it of and now it's dead... I'm in the process of replacing it (i've had a new motherboard etc... for a while I've been meaning to put in so that's taking up this evening!). I think it's likely to be a powerpack fault so once i'm finished it's time to open it up and have a look at what went wrong!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data