Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Real life holographic projector: the projector arrived
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Former Member
  • Date Created: 12 May 2015 8:58 PM Date Created
  • Views 942 views
  • Likes 3 likes
  • Comments 8 comments
  • realife_holo
  • design_challenge
  • scifi_your_pi
  • reallife_holo
Related
Recommended

Real life holographic projector: the projector arrived

Former Member
Former Member
12 May 2015

A component that is very important for my project arrived: the projector!

image

The very generic-looking box

Projectors can get really expensive, but as you can see I went with a budget version. For around 50 bucks you can find yourself a Chinese-made projector that does 480x320 and has a brightness of 100 lumen. If you're thinking that's pretty pathetic, I agree. I decided to spend a little extra and got myself one that did 640x480 (at only 80 lumen) for 70 bucks. This way R2-D2's projector would at least meet the VGA standard.

 

After unboxing and inspecting it at work, one of my colleagues remarked that it made a rattling noise. Some part was loose inside the projector. He handed me a screwdriver and convinced me to take apart the projector I'd owned for all of 10 minutes.

 

image

Don't worry, I put it back together again


The rattling sound came from one of the speakers. It was supposed to be hot-glued to the case but had come loose. Opening it up really drove home how cheaply it was made. The plastic lens is something you'd find in a pair of toy binoculars.

 

After I took it home I hooked it up to a Pi and saw if they would play nice. Initially, they didn't. I was using a bargain bin HDMI cable and I just couldn't get the Pi to detect anything. I swapped it out with an AmazonBasics cable that I had a bit more confidence in and after that it worked fine.

image

Hooked up to HDMI and happy

The projected image itself is very blurry, even after fiddling with the lens. I could get it into focus but even then it wasn't really.. sharp. I logged in on the Pi with ssh and set up x11vnc. This allowed me to get a better look at what was going on.

Compare a screenshot of  my VNC client to the actual image being projected.


image

image

It's hard to believe but that's exactly the same image being shown. The projector presents itself with 720p as its only available resolution and then squishes that widescreen image down to 640x480. The result is predictably awful. I don't really need amazing image quality for this project but this is just awful. If you're at all interested in buying a projector, I really can't recommend a device like this. Literally save yourself the headache and get something decent.

  • Sign in to reply

Top Comments

  • Former Member
    Former Member over 10 years ago in reply to balearicdynamics +2
    Luckily the holographic projections in the Star Wars movies aren't super-high quality either. They have a distinctive blue hue and aren't very high-res. I think I can make due with this projector despite…
  • crimier
    crimier over 10 years ago +2
    I think you should force the correct resolution using xrandr - see here for details. I believe this should work in your case, did it myself when I had the same problem and it worked great.
  • DAB
    DAB over 10 years ago +1
    Thanks for sharing. Sometimes ideas do not work out, so by being honest, you help the rest of us make better decisions. DAB
Parents
  • balearicdynamics
    balearicdynamics over 10 years ago

    Sorry to hear this! Is there a workaround ? Can you use it anyway ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to balearicdynamics

    Luckily the holographic projections in the Star Wars movies aren't super-high quality either. They have a distinctive blue hue and aren't very high-res. I think I can make due with this projector despite its shortcomings. The only unintended side-effect might be that the people being projected will look a little slimmer than they should. They say the camera adds ten pounds. Maybe squishing 16:9 into 4:3 can compensate for that image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to Former Member

    Did you though to send the projected image somewhere else than a flat screen ? I suppose yes...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to balearicdynamics

    I hadn't considered doing that, no. Do you suggest projecting it on something like a cylinder to stretch out the final image? That's an interesting thought...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to Former Member

    Frankly I think that yo can do something with a better effect at a very low cost: nothing solid. Cold smoke (the CO2 used in theatres and concerts). If you create a round or any shape "screen" that emit this absolutely non-damaginf smoke, you can put the projector in the center and create a very high quality scenic effect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dmrobotix
    dmrobotix over 10 years ago in reply to Former Member

    Always a silver lining. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dmrobotix
    dmrobotix over 10 years ago in reply to Former Member

    Always a silver lining. image