Sixth Sense Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sixth Sense Design Challenge
  • More
  • Cancel
Sixth Sense Design Challenge
Blog R2B4 #5 - L298 Troubles
  • Blog
  • Forum
  • Documents
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Blog Post Actions
  • Subscribe by email
  • More
  • Cancel
  • Share
  • Subscribe by email
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: 14rhb
  • Date Created: 24 Feb 2019 10:48 AM Date Created
  • Views 337 views
  • Likes 8 likes
  • Comments 8 comments
  • l298
  • sixth_sense
  • r2b4
  • robot
  • stepper motors
  • nema17
  • sixth sense design challenge
Related
Recommended

R2B4 #5 - L298 Troubles

14rhb
14rhb
24 Feb 2019

      • 1.     Background
      • 2.     Circuit Requirements
      • 3.     An Easier Solution?
      • 4.     Drivebelts
      • 5.    Conclusions of #5
      • 6.     What Next

1.     Background

I had planned on driving the NEMA-17 stepper motors from my Sealed Lead Acid (SLA) 12v battery via a pair of L298 modules; these seemed to be idea from the specifications but fellow Element14 members commented and that got me looking around the internet to soon find they were inadequate (eg threads like this). I did do a short test run having remade my drivebelts and I'll detail a bit about those below.

 

2.     Circuit Requirements

At this point I think I need to make my own driver circuits so had a look around the internet at what schematics were available. I found this one particularly useful:

[Source: http://www.circuitdiagramworld.com/uploads/allimg/201411/A3952S-bipolar-stepper-motor-driver_463104501.jpg  ]

 

and this one:

[Source: https://www.researchgate.net/figure/H-bridge-Stepper-motor-driver-circuit_fig5_308859906 ]

 

 

Both schematics show I need four active 'switch' components per phase; eight in total. The switching of these should not be a problem as I will likely offload that from the STM32Nucelo board to a PIC microcontroller. I can see I will need four inputs for each motor. I could use bipolar transistors like the heavy duty TIP142 (10A collector current) or a suitably rated MOSFET. What is not so clear from the diagrams above is the current limiting circuitry, I will need to limit my current to 2A per coil and will accomplish that by working a simple BJT and limiting resistor into the circuit to ground.

 

In the design stages I was unsure what voltage drops would be across each component, if the constant current circuit works correctly there should be 2A flowing. AT the very worst case, with no voltage drop on the stepper coil, that means almost half of my 12v supply would be dropped across each of the two MOSFET devices...that would amount to 12W each, so those MOSFETs could get quite warm.

 

My NEMA-17 stepper is rated at 2A and 2.8v (from the spec sheet) and therefore including the 0.6v drop across the current generator, then 8.6v (12 - 3.4v) is shared between the MOSFET devices....4.3v each at 2A = 8.6W

 

This is the bit I am unsure about - does the motor coils drop 2.8v at 2A or does the MOSFET voltage drop come into play due to the gate-source voltage applied? I need to do some tests !

 

3.     An Easier Solution?

Realising that I'm deviating way off the course of this challenge I recalled the small A4988 module that I used for My First Stepper Motor - a quick check of the specifications seems to show it can provide up to 2A per coil with cooling and will run from a 12v supply. Anyone with a Reprap style 3D printer will be familiar with these and that is why I have some as well (as for the last 2-3 years my attempt at making my own 3D printer has sat on the worktop under construction).

 

Therefore for now the A4988 module is what I am going to try using, I already have some of the modules and I won't have to spend valuable programming time making a new driver circuit. An article on the A4988 can be found here. Testing them out I get the following results by using an Arduino Uno to control each stepper's direction and speed:

You don't have permission to edit metadata of this video.
Edit media
x
Upload Preview

 

As you can see, it moves....but only just. The driving program also includes some turns where one side is driven in the opposite direction to the other. R2B4 doesn't seem to like turning like this which maybe is a function of the carpet friction and the double drive wheels.

{gallery} Driving R2B4

R2B4 - A test run of motor torque

The drive and temporary tensioning (aka 4mm croc clip)

4.     Drivebelts

My first two homemade GT2 drivebelts fell apart. One was made by using rubber glue and a 50mm overlap whilst the other was a clean butt slice with superglue. To make them stronger I decided to stitch them together using a needle and some strong thread. These seem to be holding up much better. To align the belt I used a small offcut as a temporary guide.

 

5.    Conclusions of #5

I found that a bit disappointing and had hoped R2B4 would have more torque than it did - being able to turn would have been great. However this is also the first contraption I have ever made that moves along and therefore I kind of think of it as a success as well....eg I've learned quite a lot. There are a few things I need to try like measuring the current to ensure the A4988 modules are running at maximum current. I need to add proper belt tensioning (rather than the screwdriver and 4mm croc clip) and I need to secure the driver boards.

 

6.     What Next

I think from the start I was stating I needed to do some actual code dev on the STM32 boards (Nucleo and SensorTile) and with this chassis "almost usable" that is what I will concentrate on in blog #6.

Anonymous

Top Comments

  • dubbie
    dubbie over 3 years ago +6

    Rod,

     

    I wondered what the screwdriver was for!..

     

    I did find that getting these kind of step motors to work was a real dog, as you seem to be experiencing and really take some work to get going properly. I…

  • jw0752
    jw0752 over 3 years ago +6

    Hi Rod,

     

    I really like that you have fabricated so much of the structure yourself. It reminded me of a time when I was a child and a neighbor kid and I decided to build a go-kart. We had everything we needed…

  • 14rhb
    14rhb over 3 years ago in reply to jw0752 +6

    Thanks for your encouragement John.

     

    Your go-kart sounds great, like all great things that come from childrens' imagination and determined ingenuity - and probably echoes many engineers' early days …

Parents
  • jw0752
    jw0752 over 3 years ago

    Hi Rod,

     

    I really like that you have fabricated so much of the structure yourself. It reminded me of a time when I was a child and a neighbor kid and I decided to build a go-kart. We had everything we needed except the drive pulleys and we had no money. The solution was to make the pulleys from wood. Unfortunately, while the go-kart was able to move itself it was not capable of moving with one of us aboard. Still it is a nice memory.

     

    I enjoyed reading about the process you are going through to make this cool little robot.

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Reply
    • More
    • Cancel
  • 14rhb
    14rhb over 3 years ago in reply to jw0752

    Thanks for your encouragement John.

     

    Your go-kart sounds great, like all great things that come from childrens' imagination and determined ingenuity - and probably echoes many engineers' early days

     

    Like you I often made things, this was long before I earned any pocket money (and never dared ask for money) to get bits....I think this is why I still keep 'junk' and make things out of it rather than buying new.

     

    Rod

    • Cancel
    • Vote Up +6 Vote Down
    • Reply
    • More
    • Cancel
Comment
  • 14rhb
    14rhb over 3 years ago in reply to jw0752

    Thanks for your encouragement John.

     

    Your go-kart sounds great, like all great things that come from childrens' imagination and determined ingenuity - and probably echoes many engineers' early days

     

    Like you I often made things, this was long before I earned any pocket money (and never dared ask for money) to get bits....I think this is why I still keep 'junk' and make things out of it rather than buying new.

     

    Rod

    • Cancel
    • Vote Up +6 Vote Down
    • Reply
    • More
    • Cancel
Children
  • michaelkellett
    michaelkellett over 3 years ago in reply to 14rhb

    If you are using a typical 3D printer type stepper motor the low speed torque should be about 40N/cm, your wheels look about 5cm diameter, 2.5cm radius so the push should be about 16N or about 1.6kg.

    I'm guessing that your drive and wheel toothed pulleys are the same diameter.

    Try checking the torque (wind a string (thin) round a wheel a few times and see how much weight it can lift.) - If the torque is lower than expected your motors or drive may not be well matched to the battery.

    If the torque is correct but the performance bad you could increase the torque at the wheels by using bigger wheel pulleys.

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Reply
    • More
    • Cancel
  • 14rhb
    14rhb over 3 years ago in reply to michaelkellett

    Hi Michael,

     

    Good points, thank you. I did try measuring the torque a few days ago by winding string around the GT2 pulley and lifting bottles of water/washing detergent. I'll have to find the notes I made but I was getting reasonable results I recall. Once the stepper power was off it dropped the weight. The gearing is another good way - I used something similar on my "Peter the Pumpkin" turntable and just need to get another large GT2 pulley to match the one I already have (and remake those drive belts to suit). I'm surprised the belts are holding up as I hand stitched them together and they are only 6mm wide with a 2mm pitch.

     

    I've decided to dive into the STM32 side for a while.

     

    Rod

    • Cancel
    • Vote Up +5 Vote Down
    • Reply