Smart Security and Surveillance – Design Challenge

Table of contents ...  

Join the element14 community’s Smart Security and Surveillance Design Challenge

10 selected Challengers will get the following kit of Components FREE of charge to help build a Smart Security and/or Surveillance-themed Prototype. The core of this kit is ADI’s MAX32630FTHR#, a smart and agile development platform.

For the chance to win one of the prizes below, you must blog your smart security prototype's build process and the final outcome of your Project that showcases features of ADI components in the most imaginative way possible.

Good and imaginative uses of the MAX32630FTHR# features will be graded more favorably.

Examples tasks that can be performed include but are not limited to:

  • Facial Recognition Door Entry System
  • Voice and Face Detection
  • Environment monitoring
  • Crowd Sentiment Monitoring
  • Break In Monitoring
  • Remote Security Sentry

The Prizes

Prizes are subject to change but will be of similar price and style.

Prize Prize Category

First Place Prize

  

Approx. Value $670 USD

13-Piece SimpliSafe Home Security System


Multicomp Pro Hot Air Rework Station (MP740907)

Second Place Prize

 

Approx. Value $600 USD

13-Piece SimpliSafe Home Security System


39-Piece Wera Multi Screwdriver Set (TOOL-CHECK PLUS)

Third Place Prize

Approx. Value $450 USD

13-Piece SimpliSafe Home Security System

Finisher Prize

For anyone who completes their 5 Forum Posts and 1 Project Blog.

For anyone who completes a final summary blog with the featured product.
Approx. Value $30

MultiComp Pro Multimeter Set

*Grand Prize and Runner Up winners will also earn the finisher prize.
**Don't worry if a prize is out of stock in your region or does not have the right plug for you. We can ship from global stocks, include a plug adaptor, or find a local equivalent of a prize.

Sponsored Challenger Kit

10 Sponsored Challengers get the following kit free of charge to incorporate into their project.

The Sponsored Kit Quantity
            

Analog Devices MAX32630FTHR# Application Platform

MAX32630FTHR# is a MAX32630FTHR application platform board which is a rapid development platform designed to

help engineers quickly implement battery optimized solutions with the MAX32630 ARM® Cortex®-M4F microcontroller.

Buy now

2


Analog Devices FTHR-PMD-INTZ Adapter Board

Add-on feather to PMOD Adapter Board, MAX32630FTHR, MAX32650FTHR, MAX32655FTHR, MAX32666FTHR, MAX78000FTHR Boards

Buy now

2


Würth Elektronik 150015 Featherwing ICLED Display

Evaluation Kit, IC LED FeatherWing, 7x15 ICLED Display, Adafruit Feather Line of Development Board

Buy now

1

Particle FWNG-ETH Ethernet Featherwing Adapter

Development Board, Ethernet FeatherWing, Wired Connectivity, For Particle Mesh Boards

Buy now

1

Adafruit ADA2927 DC Motor + Stepper FeatherWing

Featherwing DC Motor and Stepper Motors Driver.

Buy Now

2

The Challenge Requirements

10 Applicants will be chosen to receive The Kit above, these successful applicants will be our sponsored challengers. The sponsored challengers must showcase features of the kit in the most imaginative way possible. Challengers must post their progress and final project as at least 5 Forum Thread updates and 1 Project Blog type and post before the closing date.

Posts which are media rich with Photos, Videos and Code samples will be viewed more favorably in the Judging Process.

If you are not successful in becoming an official Challenger but still want to enter, you can purchase the kit as described above and adhere to the same Terms and Conditions to still be in the running to win! All contestants are eligible for the Winner and Finisher prizes.

The Dates

Project Phases Dates
Application Period 2nd February 2026 - 15th March 2026
Application Deadline 23:59 UK time 15th March 2026
Challengers Announced 20th March 2026
Build Period 27th March - 24th May 2026
Projects Due 23:59 UK time 24th May 2026
Winners Announced 29th May 2026
Prizes Shipped June 2026

The Judges

element14 Community Judges
element14 Community Team
image

The Terms

Please read the full terms and conditions attached below.

About The Sponsor

Analog Devices, Inc. (ADI) empowers the Intelligent Edge with the most innovative analog, digital, and software solutions, accelerating breakthroughs that benefit society and the planet. 

Learn more about their technologies here.

Anonymous
Parents Comment Children
  • I will answer to some extent.  Note i am not part of an organizing team. I am a fellow participant and its my understanding:
    1. If you enroll now and if you are not selected among the 10 people for whom the kit will be sponsored, you still can submit the final project but only as long as you build a project with the same components as that of the kit. The more the better.
    2. You can start working/building for the project now itself either plan or work with the hardware if you have them. (I may have misunderstood your question)
    3. The rules  says you need to use the kit, doesnt say how much, so the more of the kit you use in a creative and coherent way to the utility of the project (i mean you are not using the components just for the competition's sake), the greater is chance. So reasonably we can assume, if you don't use the MAX32630FTHR which is sort of the main thing here, your chance can go down, although i don't think you will be disqualified if you use other components of kit
    4. Yes, if the project genuinely requires it. 
    5. Chance goes down. Again i do not see anything in the the rules that says you cannot use replacement enough to be a disqualified.

    In short:  the spirit of the challenge is to for the challengers to use this MAX32630FTHR board and establish creativity in using its features. Stress is on the work Challenge. The more of kit you use, the greater is your change of winning.

  •  The Design Challenge FAQs might help.   Competition FAQs and Judging 

      summary is also very good.

  • Hey  ,  and  have both given you great responses but just so you hear from one of the competition organizers:

    #1 If your submission is not selected as a sponsored challenger then you can always enter a project as an unsponsored challenger by purchasing the kit and adhering to the same rules. Unsponsored challengers can still win and this has happened in previous competitions.

    #2 Yes everyone can take part, either as a sponsored or unsponsored challenger, and everyone can begin planning or start making preparations ahead of the build period and submission deadline on 24th May.

    #3 It is not mandatory use the MAX32630FTHR#. However, part of the aim of the challenge is to 'showcase features of the kit in the most imaginative way possible' so if you are not using the full kit or not using it to the fullest of its capabilities then that might make it harder to qualify for a prize. At the same time though, the team and I are understanding that for unsponsored challengers there is a cost to purchasing the entire kit. This is a very supportive community so I know everyone would be really enthusiastic to see what someone created around the theme of the challenge regardless how many official kit parts they did/did not use. 

    #4 Yes you can absolutely add sensors, an enclosure, additional devices, whatever you want to do to bring your project to life. The kit is intended to help Challengers get started and provide something to build on.

    #5 Yes you could use an alternative board and then use the rest of the official kit. This would mean that to an extent you are not showcasing all the features of the kit but perhaps your project is overall highly original, innovative, and demonstrates lots of technical merit, and as a result is still highly deserving of a prize. So there is a calculation there that you need to make...

    Lastly, yes you can enroll as a team. Just let me know in your application who is in the team. Plus, when project updates are being shared maybe just let everyone know who is in the team. I would also just highlight that the number of prizes is the same for every winner, so if a team won a prize then they would need to share Wink 

    If you have any more questions, you are very welcome to reply here or you can DM me if you like.

  • thanks   this clears a bunch of my questions - much appreciated.

    Having just read the T's&C's I also note that judging will include

    1.4. Judging Criteria: All of the following, which will have equal weighting:
    1.4.1. Challengers
             must post five (5) forum posts regarding their build process plus
             one (1) project blog sharing the final outcome of their project using the Kit. Challengers ...
    1.4.2. Originality;
    1.4.3. Innovation;
    1.4.4. Technical merit;
    1.4.5. Meeting the goals and intentions of the Contest as set forth in these Terms;
    1.4.6. Completeness and clarity of posts and supporting media describing the evolution ...

    WarningWarning️ so the 5 forum posts and 1 project post are also important WarningWarning

    Hopefully I plan to work on this with  - he will help drive this forward and has a 3D printer

    For those interested, we were looking at things like fingerprinting Drone transmitting frequencies using the MAX32630FTHR but obviously we would need a bunch of RF sensors that are not part of the kit - but the T's&C's are ok with that (yes all done within legal bounds)

    Also for the other boards (Seeed XIAO Sense) and more powerful computers (Hailo, Jetson, Ras Pi) this was around an idea of having a mesh of sensors and a central AI with LLM capability to process the input and if I needed more than one MAX32630FTHR I may want to aim for a platform I already have at hand (at the reduced chance of winning)

    all good thanks for all the responses Clap