Smart Security and Surveillance – Design Challenge

Table of contents ...  

Join the element14 community’s Smart Security and Surveillance Design Challenge

10 selected Challengers will get the following kit of Components FREE of charge to help build a Smart Security and/or Surveillance-themed Prototype. The core of this kit is ADI’s MAX32630FTHR#, a smart and agile development platform.

For the chance to win one of the prizes below, you must blog your smart security prototype's build process and the final outcome of your Project that showcases features of ADI components in the most imaginative way possible.

Good and imaginative uses of the MAX32630FTHR# features will be graded more favorably.

Examples tasks that can be performed include but are not limited to:

  • Facial Recognition Door Entry System
  • Voice and Face Detection
  • Environment monitoring
  • Crowd Sentiment Monitoring
  • Break In Monitoring
  • Remote Security Sentry

The Prizes

Prizes are subject to change but will be of similar price and style.

Prize Prize Category

First Place Prize

  

Approx. Value $670 USD

13-Piece SimpliSafe Home Security System


Multicomp Pro Hot Air Rework Station (MP740907)

Second Place Prize

 

Approx. Value $600 USD

13-Piece SimpliSafe Home Security System


39-Piece Wera Multi Screwdriver Set (TOOL-CHECK PLUS)

Third Place Prize

Approx. Value $450 USD

13-Piece SimpliSafe Home Security System

Finisher Prize

For anyone who completes their 5 Forum Posts and 1 Project Blog.

For anyone who completes a final summary blog with the featured product.
Approx. Value $30

MultiComp Pro Multimeter Set

*Grand Prize and Runner Up winners will also earn the finisher prize.
**Don't worry if a prize is out of stock in your region or does not have the right plug for you. We can ship from global stocks, include a plug adaptor, or find a local equivalent of a prize.

Sponsored Challenger Kit

10 Sponsored Challengers get the following kit free of charge to incorporate into their project.

The Sponsored Kit Quantity
            

Analog Devices MAX32630FTHR# Application Platform

MAX32630FTHR# is a MAX32630FTHR application platform board which is a rapid development platform designed to

help engineers quickly implement battery optimized solutions with the MAX32630 ARM® Cortex®-M4F microcontroller.

Buy now

2


Analog Devices FTHR-PMD-INTZ Adapter Board

Add-on feather to PMOD Adapter Board, MAX32630FTHR, MAX32650FTHR, MAX32655FTHR, MAX32666FTHR, MAX78000FTHR Boards

Buy now

2


Würth Elektronik 150015 Featherwing ICLED Display

Evaluation Kit, IC LED FeatherWing, 7x15 ICLED Display, Adafruit Feather Line of Development Board

Buy now

1

Particle FWNG-ETH Ethernet Featherwing Adapter

Development Board, Ethernet FeatherWing, Wired Connectivity, For Particle Mesh Boards

Buy now

1

Adafruit ADA2927 DC Motor + Stepper FeatherWing

Featherwing DC Motor and Stepper Motors Driver.

Buy Now

2

The Challenge Requirements

10 Applicants will be chosen to receive The Kit above, these successful applicants will be our sponsored challengers. The sponsored challengers must showcase features of the kit in the most imaginative way possible. Challengers must post their progress and final project as at least 5 Forum Thread updates and 1 Project Blog type and post before the closing date.

Posts which are media rich with Photos, Videos and Code samples will be viewed more favorably in the Judging Process.

If you are not successful in becoming an official Challenger but still want to enter, you can purchase the kit as described above and adhere to the same Terms and Conditions to still be in the running to win! All contestants are eligible for the Winner and Finisher prizes.

The Dates

Project Phases Dates
Application Period 2nd February 2026 - 15th March 2026
Application Deadline 23:59 UK time 15th March 2026
Challengers Announced 20th March 2026
Build Period 27th March - 24th May 2026
Projects Due 23:59 UK time 24th May 2026
Winners Announced 29th May 2026
Prizes Shipped June 2026

The Judges

element14 Community Judges
element14 Community Team
image

The Terms

Please read the full terms and conditions attached below.

About The Sponsor

Analog Devices, Inc. (ADI) empowers the Intelligent Edge with the most innovative analog, digital, and software solutions, accelerating breakthroughs that benefit society and the planet. 

Learn more about their technologies here.

Anonymous
Parents Comment Children
  • I still did not understand, If you had submitted one or even multiple ideas for consideration of the Sponsored kit, you have to build the idea which was selected. That is a requirement. You can build more ideas as bonus.

    and there is a menu below the top comments for sorting the comment by newest. I do agree the top comments is something of a bad UX when it comes to an engaging discussion. Breaks the flow of timeline

    image

  • wow Oldest | Best | Newest - hidden just below the top 3 comments Face palm

    I still did not understand

    If I win Checkered flag "sponsored challenger kit" - then I have to build the thing I won, as I entered 4 ideas I need to know which one gets chosen

    If I don't win the "sponsored challenger kit" - then I need to decide what to build and seeing what the sponsored challenger kit is awarded for, will give me a better idea of what I should build or focus on - technically I could build anything at that point - for example if all the awards are for ideas that require the use of TinyML and training a model - the I would incorporate that in my final build