Smart Security and Surveillance – Design Challenge

Table of contents ...  

Join the element14 community’s Smart Security and Surveillance Design Challenge

10 selected Challengers will get the following kit of Components FREE of charge to help build a Smart Security and/or Surveillance-themed Prototype. The core of this kit is ADI’s MAX32630FTHR#, a smart and agile development platform.

For the chance to win one of the prizes below, you must blog your smart security prototype's build process and the final outcome of your Project that showcases features of ADI components in the most imaginative way possible.

Good and imaginative uses of the MAX32630FTHR# features will be graded more favorably.

Examples tasks that can be performed include but are not limited to:

  • Facial Recognition Door Entry System
  • Voice and Face Detection
  • Environment monitoring
  • Crowd Sentiment Monitoring
  • Break In Monitoring
  • Remote Security Sentry

The Prizes

Prizes are subject to change but will be of similar price and style.

Prize Prize Category

First Place Prize

  

Approx. Value $670 USD

13-Piece SimpliSafe Home Security System


Multicomp Pro Hot Air Rework Station (MP740907)

Second Place Prize

 

Approx. Value $600 USD

13-Piece SimpliSafe Home Security System


39-Piece Wera Multi Screwdriver Set (TOOL-CHECK PLUS)

Third Place Prize

Approx. Value $450 USD

13-Piece SimpliSafe Home Security System

Finisher Prize

For anyone who completes their 5 Forum Posts and 1 Project Blog.

For anyone who completes a final summary blog with the featured product.
Approx. Value $30

MultiComp Pro Multimeter Set

*Grand Prize and Runner Up winners will also earn the finisher prize.
**Don't worry if a prize is out of stock in your region or does not have the right plug for you. We can ship from global stocks, include a plug adaptor, or find a local equivalent of a prize.

Sponsored Challenger Kit

10 Sponsored Challengers get the following kit free of charge to incorporate into their project.

The Sponsored Kit Quantity
            

Analog Devices MAX32630FTHR# Application Platform

MAX32630FTHR# is a MAX32630FTHR application platform board which is a rapid development platform designed to

help engineers quickly implement battery optimized solutions with the MAX32630 ARM® Cortex®-M4F microcontroller.

Buy now

2


Analog Devices FTHR-PMD-INTZ Adapter Board

Add-on feather to PMOD Adapter Board, MAX32630FTHR, MAX32650FTHR, MAX32655FTHR, MAX32666FTHR, MAX78000FTHR Boards

Buy now

2


Würth Elektronik 150015 Featherwing ICLED Display

Evaluation Kit, IC LED FeatherWing, 7x15 ICLED Display, Adafruit Feather Line of Development Board

Buy now

1

Particle FWNG-ETH Ethernet Featherwing Adapter

Development Board, Ethernet FeatherWing, Wired Connectivity, For Particle Mesh Boards

Buy now

1

Adafruit ADA2927 DC Motor + Stepper FeatherWing

Featherwing DC Motor and Stepper Motors Driver.

Buy Now

2

The Challenge Requirements

10 Applicants will be chosen to receive The Kit above, these successful applicants will be our sponsored challengers. The sponsored challengers must showcase features of the kit in the most imaginative way possible. Challengers must post their progress and final project as at least 5 Forum Thread updates and 1 Project Blog type and post before the closing date.

Posts which are media rich with Photos, Videos and Code samples will be viewed more favorably in the Judging Process.

If you are not successful in becoming an official Challenger but still want to enter, you can purchase the kit as described above and adhere to the same Terms and Conditions to still be in the running to win! All contestants are eligible for the Winner and Finisher prizes.

The Dates

Project Phases Dates
Application Period 2nd February 2026 - 15th March 2026
Application Deadline 23:59 UK time 15th March 2026
Challengers Announced 20th March 2026
Build Period 27th March - 24th May 2026
Projects Due 23:59 UK time 24th May 2026
Winners Announced 29th May 2026
Prizes Shipped June 2026

The Judges

element14 Community Judges
element14 Community Team
image

The Terms

Please read the full terms and conditions attached below.

About The Sponsor

Analog Devices, Inc. (ADI) empowers the Intelligent Edge with the most innovative analog, digital, and software solutions, accelerating breakthroughs that benefit society and the planet. 

Learn more about their technologies here.

Anonymous
  • HO HO HO , santa brought something in march

  •  The Design Challenge FAQs might help.   Competition FAQs and Judging 

      summary is also very good.

  • I will answer to some extent.  Note i am not part of an organizing team. I am a fellow participant and its my understanding:
    1. If you enroll now and if you are not selected among the 10 people for whom the kit will be sponsored, you still can submit the final project but only as long as you build a project with the same components as that of the kit. The more the better.
    2. You can start working/building for the project now itself either plan or work with the hardware if you have them. (I may have misunderstood your question)
    3. The rules  says you need to use the kit, doesnt say how much, so the more of the kit you use in a creative and coherent way to the utility of the project (i mean you are not using the components just for the competition's sake), the greater is chance. So reasonably we can assume, if you don't use the MAX32630FTHR which is sort of the main thing here, your chance can go down, although i don't think you will be disqualified if you use other components of kit
    4. Yes, if the project genuinely requires it. 
    5. Chance goes down. Again i do not see anything in the the rules that says you cannot use replacement enough to be a disqualified.

    In short:  the spirit of the challenge is to for the challengers to use this MAX32630FTHR board and establish creativity in using its features. Stress is on the work Challenge. The more of kit you use, the greater is your change of winning.

  • I'm a little confused at how this work? I submitted a proposal, it seems now the dates have shifted so technically I have till 15 March to alter or submit other proposals - I kind of get that White check mark

    After my submission, there is a chance to be one of ten sponsored challengers and get some gear to help build a prototype - I kind of get that White check mark

    but what happens to the rest of us?

    1. can my submission be rejected, and that is it?
    2. is they idea "ALL" other submissions will now have the opportunity to "build" their prototype to enter the actual challenge by 24 May?
    3. how mandatory is it to use the MAX32630FTHR# ? is it a show stopper if one is not used? ie. if I don't get selected as a sponsored challenger, I need to buy one?
    4. presumably if I do use the MAX32630FTHR# (unless it is optional) the I can choose to use any "other" sensors, devices, actuators and even another, potentially more powerful platform to offload more complex calculations like
      1. Jeston Nano - https://developer.nvidia.com/embedded/jetson-nano
      2. Google Coral - https://www.coral.ai/docs/dev-board/get-started/
      3. Hailo 8 M.2 AI - https://hailo.ai/products/ai-accelerators/hailo-8-m2-ai-acceleration-module/
      4. ArmSoM-LM7 Maker Kit - https://www.armsom.org/lm7
      5. Brainy PI - https://brainypi.com/
      6. Orange Pi - http://www.orangepi.org/html/hardWare/computerAndMicrocontrollers/details/Orange-Pi-5.html
      7. Intel Neural Compute stick (discontinued so there may be some discounts) https://cdrdv2-public.intel.com/749742/neural-compute-stick2-product-brief.pdf
    5. or presumably I could use an alternative edge board? maybe be somewhat penalised?
      1. Arduino Nano 33 BLE sense - https://store.arduino.cc/products/nano-33-ble-sense-rev2-with-headers
      2. Seeed Studio XIAO nRF52840 Sense (XIAO BLE Sense) https://www.seeedstudio.com/Seeed-XIAO-BLE-Sense-nRF52840-p-5253.htm
      3. Seeed Arch Max - https://www.seeedstudio.com/Arch-Mix-p-2901.html
      4. Seeed Wio Lite MG126 - https://www.seeedstudio.com/Wio-Lite-MG126-p-4189.html

    I have put in the names and links in case anyone has some feedback on things I have missed or better or worse alternatives

    Finally if I want to enrol as a team, is there something I need to do to get my team mates to join my submission?

    thanks in advance! - looking forward to it

  • Ive been waiting for someone to send me a ring camera so I can collect the Luis Rossman bounty on secure security camera conversion. 

  • I must admit I felt a little disappointed at first since I was looking forward to the original timeline, but it’s completely understandable. A few extra days won’t hurt, and it’s good that everyone gets additional time to refine their submissions.

  • Some extra time to send in submissions has been requested due to the upcoming Embedded World conference in Germany so I am going to extend out the deadline for submissions to Sunday 15th March and we will set that as the final cutoff for submissions. I will adjust the rest of the dates for the challenge accordingly.

    Thank you to everyone who has already sent in their application, there have been some very interesting ideas for projects!

  • 2nd March is the deadline for submitting proposals, so a few extra days for anyone who needs it Slight smile Good spot, I've just updated the T&Cs.

    Edit: I am going to extend out the deadline for submissions to Sunday 15th March to give everyone a bit more time.

  •   The End date to submit the proposal for contenders is shown as 2 March as per the countdown but  as per the Terms PDF document and the Dates in the challenge page is shown as 27th Feb. Can you kindly clarify which one is it?

  • Interesting kit - lots of capabilities. It might be a bit of a stretch to include the whole kit in one application. Maybe worth proposing an auxiliary application to use the extra kit components.