• Modernize a GBA

    So, the Game Boy Advance came out in 2001, and is notorious for having a bad LCD screen, as it doesn't have a backlight. It wasn't until 2005 that they finally released a model with one.

    But I was thinking that the original GBA (which has a great…

  • Gaming Tablet?

    Make a tablet running Windows 8.1 for portable gaming. And maybe a geforce gpu?

  • Custom Project

    Hi, just wondering, if its possible to male, from scratch a dual-screen vita-like gaming console. Basically in the shape of a vita, but not truly a vita. I'm looking to make something I. That shape that is essentially a gaming laptop, in terms of speed…

  • Could Ben possibly make old handhelds more power efficient?

    Like the Game Boy and the Game Gear for instance, which are known for consuming batteries like crazy.

  • Custom car stereo build...

    Here's a challenge for you Mr. Heck!! I want to get a "smart" double din stereo, but they want about $1,500.00+! I could build my own mini-PC for cheaper!! I have a 2015 Camaro, and the MyLink factory option is waaaay over priced and an aftermarket option…

  • I need help

    I’m study computer science in university of Jordan , I have project about tracking system of cameras

    This about where is exactly cameras and find it.

    I need help

  • Raspberry PI Tablet (PiPad)

    Hello,

     

    After looking around on the internet I saw tons of cool raspberry pi projects but none of them were really mobile. So after doing some thinking I was wondering if you could maybe build a raspberry pi tablet. One that is like a iPad but better. Maybe…

  • any idea on a proable gaming console?

    Greetings everyone.

     

    I know that nowadays it's really convenient to play games on the cell phones or tablets, but I do think a D-pad or a joystick is the right way to enjoy game.

    And yes, there are controllers made for this purpose, but it's not as portable…

  • Nintendo Advance SP / Own mobile console

    Couple weeks ago my friend found an old Nintendo Advance SP (Zelda Version). I thought:

    ,,Can I make my own one? Or a custom  mobile console which can handle some 3ds and Advance games.

    I don't like the 3ds desgin."It's price also shocked me. So i think…

  • Combination Gameboy and 3ds

    Hi Ben,

     

    Would it be possible to build a combination of all previous nintendo handheld consoles into one console? This would allow a device to play all versions/generations of pokemon which would be awesome.

     

    Thanks

    Martin

  • I would like to see a raspberry pi portable specificly for n64 gaming

    Hi I am a younger gamer and want to be a engineer but I can't find anyone who knows how to so the basic computer skills that I am looking for. Ben I would like your help! I have been trying to learn the basics to circuitry and soldering and I'm not doing…

  • XBOX One/Xbox 360 laptop

    Hey. The xbox one tablet you built recently was nice, but I would like to see an xbox one/xbox 360 laptop because the xbox one has the hdmi pass through and there should be an xbox laptop that can play both xbox 360/xbox games and xbox one games. all…

  • Portable GameCube/wii

    ben should make a portable GameCub/wii laptop using a wiikey fusion so games can be loaded from an sd card to save space

  • Playstation 1 Portable

    Hey there my name is Marco and i have an idea for you to build something i heard you like those challanges and i have an awsome idea i like this channel and i want to see you building a Playstation 1 portable what do you think about this

  • Portable street fighter

    I have been looking for a way to play the street fighter games and I thought it would be fun to play on the plane because I travel a lot. Also it would be cool to be able to play 2 player if you have two.

  • Portable PS4

    Hi,

     

    I am a huge fan of the Ps4...more than the xbox one. However, I've always wanted a portable gaming rig, like Alienware and what not, but those are way out of my budget range. As the PS4 is more cost sufficient, It would be nice if you guys could build…

  • Giant Game boy Color - Ayuda-help

    Hola,   estoy en un proyecto el cual deseo crear un game boy color gigante y mi idea es lograr usar una placa de game boy color original.

    realice un diseño en fusion 360 y con mi impresora 3d ( tiene buen tamaño) y lo estoy imprimiendo de a partes.

    quiero…

  • i would like to make a computer using an xbox,will,and xbox1 and make them all compatable, into one huge gaming computer.

    Hi my name is Ricky, and i would like to build my own gaming computer combing four systems. I have an xbox 360, xbox origional, a wii, and a origional nintendo.

    what can i do. i am new to doing this and want to make an awesome gaming system, with outragious…

  • SEGA Switch! *louder snap*

    Hmm, I guess if you had an even louder Snap then you'd have the power?

     

    Anyways...  the Sega Master System and the Sega Game Gear were apparently quite similar.

    So my suggestion would be to make a hybrid console + portable in which you could play both…

  • build a retro boom box 80s style from a old ampped dvd 3.1 sound system printedd / laser cut body prtable

    i have an old 3.1 sound system just sitting here. would love some ideas on how to turn it into a big old boom box battry powered fully portable even with a little pi3 action  on it portable retro media centre ?

  • Sinclair ZX Spectrum Vega+

    The ZX Spectrum will be rebuild called 'Sinclair ZX Spectrum Vega+', currently on Indiegogo. The Vega+ is a new low cost hand-held games console with a colour LCD screen and 1,000 licensed games already installed.

     

     

    Visit:

    https://www.indiegogo.com…