element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Voltage doubler for beaglebone black fan
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 29 subscribers
  • Views 579 views
  • Users 0 members are here
  • icl7660
  • voltage
  • BeagleBone
  • doubler
Related

Voltage doubler for beaglebone black fan

Former Member
Former Member over 11 years ago

Hi,

 

I've been working on a circuit that will take the 5V from the beaglebones GPIO and boost it up so that I can drive a fan, I started with getting a ICL7660 chip, and found I was getting 13V and could drive a little 12V 10mA fan quite happily but I wanted to switch to a blower which takes 900mA and it wont even start, I monitored the power into the beagle and its not even close to 1A let alone the 2A PSU I'm using so I'm guessing the chip is limited to a few mA, do any of you know of a circuit that will eliminate this problem or is it the beaglebone itself?

 

I dont want to run this on a separate circuit as it will be used in a situation where additional plugs are impossible

 

As always thanks to anyone that can help

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 11 years ago

    Hi Kevin,

    Voltage boost modules are readily available or you can build your own - here is an example based on an LM2577 - you can make your by following the example in the datasheet:

    DC DC Auto Boost Buck Step UP Step Down Converter Module Solar Voltage LM2577 | eBay

     

    To convert 5 Volts to 12 V at 900 mA will require at least 2160 mA from your 5 V source and probably more like 2400 mA.

    If you are getting your 5 V source from the Beaglebone Black connector it will likely not be able to supply enough current due to the size of the copper traces on the PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 11 years ago

    Hi Kevin,

    Voltage boost modules are readily available or you can build your own - here is an example based on an LM2577 - you can make your by following the example in the datasheet:

    DC DC Auto Boost Buck Step UP Step Down Converter Module Solar Voltage LM2577 | eBay

     

    To convert 5 Volts to 12 V at 900 mA will require at least 2160 mA from your 5 V source and probably more like 2400 mA.

    If you are getting your 5 V source from the Beaglebone Black connector it will likely not be able to supply enough current due to the size of the copper traces on the PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to dougw

    Thanks, I knocked up this circuit and it is working like a charm though the diode is massive, and as its only drawing 0.9A, I don't think I need the 3A one that was recommended though I did go for the fixed 12V version as voltage change is not necessary.