Hi,
I've been working on a circuit that will take the 5V from the beaglebones GPIO and boost it up so that I can drive a fan, I started with getting a ICL7660 chip, and found I was getting 13V and could drive a little 12V 10mA fan quite happily but I wanted to switch to a blower which takes 900mA and it wont even start, I monitored the power into the beagle and its not even close to 1A let alone the 2A PSU I'm using so I'm guessing the chip is limited to a few mA, do any of you know of a circuit that will eliminate this problem or is it the beaglebone itself?
I dont want to run this on a separate circuit as it will be used in a situation where additional plugs are impossible
As always thanks to anyone that can help