Maker Film Festival
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Hack Like Heck
  • Maker Film Festival
  • More
  • Cancel
Maker Film Festival
Documents Hack Like Heck - ShockSlayer - Portable Wii: The WaveRider
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Maker Film Festival to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 2 Apr 2018 6:13 PM Date Created
  • Last Updated Last Updated: 8 Apr 2018 3:08 AM
  • Views 4940 views
  • Likes 20 likes
  • Comments 37 comments
Related
Recommended

Hack Like Heck - ShockSlayer - Portable Wii: The WaveRider

image

A Hack Like Heck Project Video

Vote for this Video by using the Like or Share buttons

Voting Instructions image

About Hack Like Heck
Content Partner Program
All Hack Like Heck Videos

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The WaveRider is a fully featured Wii Portable, designed to be as comfortable to play as possible. With its never-before-seen software integration and no-expense-spared feature list, it's sure to turn a few heads this year at MGC. Follow ShockSlayer as he takes you on a journey through the advancement of the portablizing community, with the WaveRider as your final destination.

 

 

Parts:

 

  • 1x OMEGA trimmed Wii motherboard
    • Fully featured, including the MX chip, Wifi module, BlueTooth module, etc.
  • 3x 3.7v 2500mAh Li-ion battery cells
  • 1x 800x480 LCD w/HDMI driver board
  • 1x GCVideo-DVI digital signal to HDMI converter board
  • 1x Prototype BGA-style NAND relocation board
  • 1x Prototype "PowerMii" regulator board
  • 1x Prototype "WiiHUD" audio amplifier
    • Prototype boards have too many individual components to list
  • 1x Power button circuit (D flip-flop w/debouncer)
  • 2x Speakers
  • 1x USB port
  • 4x 3D printed case parts
    • Screen assembly, bezel, back plate, and front extended
  • 1x Hand-made battery cover
  • 1x WaveBird controller
    • Gutted for the case, controller board cutouts, and supporting buttons and trigger assemblies
  • 1x Replacement mini rumble motor
  • 2x GC+ Controller replacement board
    • One of which has custom firmware for controlling RGB LEDs via custom controller protocols
  • 2x RGB LEDs
  • 1x Lasered acrylic cutout for the front logo
  • 1x 5v Sunon blower fan
  • 1x Custom copper heatsink w/soldered copper cutouts
  • 20+ Male/Female Headers of varying amounts of pins
  • 1x 3.5mm headphone jack
  • 1x Charging jack
  • 7x Tact switches
  • 8x Triwing Screws
  • 1x Pig of unknown purpose
  • Plus an incalculable amount of various wire types, kapton tape, thermal paste, paint/gloss, solder, and of course hot glue.
  • hlh_mff
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • nobble
    nobble over 7 years ago +14
    THIS is the Ultimate Portable Wii!
  • shockslayer
    shockslayer over 7 years ago +5
    I've been told by a few people that they're unable to comment on this page; is that intentional? Thanks.
  • shockslayer
    shockslayer over 7 years ago in reply to makerkaren +3
    I've being using the same two rolls of 38 and 34 gauge wire for about 2 years now for lots of different commissions and projects, and I've never had an issue with wires being scratched and bridging/shorting…
Parents
  • makerkaren
    makerkaren over 7 years ago

    Very impressive build. You sure crammed a ton of information and explanation into your video. I'm seeing a pattern of BitBuilt-ers and magnet wire being used in projects. image Given the nature of TBHS, I wish there had been more video your project progress rather than mostly panning still images. However, I see how much information you jammed into this video and I know how difficult it can be to get all the information you want condensed into the time given while including video explanation.

    PS. I enjoyed the pig Easter eggs.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nobble
    nobble over 7 years ago in reply to makerkaren

    The red noodle is my favorite way to get arthritis! But it works like magic.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 7 years ago in reply to nobble

    I would be afraid that, if it gets taken apart a few times, you run the risk of the enamel getting scratched off the wire in unintended spots and causing shorts. Have you heard of this ever being a problem?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to makerkaren

    makerkaren I don't trust that wire at all, it is very hard to detect any shorts if they happen. so i avoid using it unless I have to because of space.
    nobble what's your experience?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to mayermakes

    Hi Clemens,

     

    There is some super-thin (30AWG or less for the overall conductor diameter) insulated wire, usually some special insulation like PTFE to keep it really thin (needs good wire-strippers), and multistranded for flexibility. But also the interface to the connector is important, usually something like heat-shrink tubing can help (even better would be adhesive-lined, but maybe that's not available in very thin tubing) - I guess hot glue could be used! I've not tried it, but perhaps that is worth experimenting with.

     

    Generally for flying wire connections I'll try to use heat shrink if there is no grip for the insulation bit. Another possibility is to avoid connecting to SIL header pins with wires (since they are intended for PCB, not on flying wires) and find very long SIL pins so that SIL sockets can be used on each end back-to-back so-to-speak - but such long SIL header pins are more rare these days, they were popular for 'wire-wrap' assembly procedures. Sometimes when prototyping, I'll try to find very small connectors with wires pre-attached, e.g. JST 'SH' series  is 1mm pitch - nearly impossible to hand assemble those connectors without the correct tools, but fortunately they come with wires pre-attached from ebay etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to mayermakes

    Not the best example, but you can see what I mean here - the connectors at the top-right are something like JST or similar, these may be bigger than the 1mm 'SH' series, I can't recall what I used. But it came as a connector with the wires attached so I didn't need to crimp anything. Also on the panel, they are going to three 3mm LEDs, so heat-shrink was used there, and then the LED was secured using epoxy glue.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to shabaz

    thanks, I also use those premade JST-conectors from time to time, you can see one in my VRpi build video for HLH.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 7 years ago in reply to shabaz

    For modding game handhelds, modders want to keep everything as small as possible. I assume, that's why they use the magnet wire instead of insulated wire. Wouldn't adding all those connectors add bulk as well? Is there a small solution?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • makerkaren
    makerkaren over 7 years ago in reply to shabaz

    For modding game handhelds, modders want to keep everything as small as possible. I assume, that's why they use the magnet wire instead of insulated wire. Wouldn't adding all those connectors add bulk as well? Is there a small solution?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 7 years ago in reply to makerkaren

    Hi Karen,

    It's a good question, I guess in most cases the stranded version of 30AWG may be usable, (it is about 0.5-0.6mm thick with the insulation depending on the version, e.g. this Alphawire ThermoThin wireAlphawire ThermoThin wire is 0.56mm thick) but might not suit extremely cramped projects. Enamelled wire is fine I think, since it is a one-off project, just makes maintainability a bit awkward, and knowing if there are shorts or not is harder. The 'SH' and similar connectors are quite small, e.g. for 8 circuits, the Molex Picoblade is 1.5mm pitch, and the mated connectors together would take up 15x9x3.2mm space overall, i.e. smaller footprint than using 0.1" SIL header pins for connections, but just a bit thicker (maybe just under 1mm thicker). Another option if needing to go even smaller could be to make a custom PCB, with a small high density connector on it, a bit like those in mobile phones. Then you're down to less than 1cm2 footprint and a few mm thick, for 20+ circuits including a few mm for soldering 30AWG wires.