In this episode of element14 presents, Clem designs and builds a unique USB card reader, starting from the initial idea to the first prototype. Facing various challenges and pitfalls during the process, he learns valuable lessons in iterative prototyping and testing. Clem emphasizes the significance of adding test points for easy debugging, and shares insights into using standard enclosures for small-batch production. Throughout the video, he showcases the importance of collaboration and learning within the maker community, encouraging viewers to share their experiences on the element14 platform.
Watch the Video:
In this episode of element14 presents, Clem takes us from idea to prototype as he builds a unique USB card reader. He starts by explaining that many new products are iterations of existing ones, and he wants to create a card reader that caters to electronics enthusiasts like himself. His old card reader was failing and he couldn't find a suitable replacement, so he decided to make his own.
Clem breaks down the components of a USB card reader. For his project, he chooses a combined USB hub and media controller. To help determine if the form factor is achievable, he’ll need to design a PCB for the controller. He uses a separate ESP microcontroller to enable control of output current via software.
Throughout the process, Clem faces challenges and pitfalls. There are issues with the USB connectors in the initial prototype, which he attributes to errors in the reflow soldering process. Some of the pins in the USB hub were not properly connected. He also faces problems with SD card detection, which he diagnoses with additional measurements and a look back at the datasheet. Despite these issues, he emphasizes that such troubles are typical during the initial prototyping phase and can be invaluable for learning.
Clem discusses his choice of standard enclosures from Hammond Manufacturing, which offers a cost-effective and reliable solution for small-batch production. He also points out the importance of adding test points to the PCB for easier debugging in future iterations.
The video showcases the importance of iterative prototyping and testing. Clem acknowledges that the first prototype may not be perfect, but it helps him identify and resolve potential problems early on.
Bonus Content:
- Download CAD and Schematics
Bill of Material:
Product Name | Manufacturer | Quantity | Buy Kit |
---|---|---|---|
LM317AT/NOPB | TI | 1 | Buy Now |
VISHAY SMD Current Sense Resistor, 0.1 ohm, WSL, 2512 [6432 Metric], 1 W, ± 1%, Metal Strip | Vishay | 1 | Buy Now |
MOLEX USB Connector, USB Type C, USB 3.1, Receptacle, 24 Ways, Surface Mount, Right Angle | 2 | Buy Now | |
MULTICOMP PRO SMD Multilayer Ceramic Capacitor, 18 pF, 50 V, 0603 [1608 Metric], ± 5%, C0G / NP0, MC | Multicomp pro | 2 | Buy Now |
PRO SIGNAL USB 2.0 A Plug to USB Type-C Cable, 1m White | Pro signal | 1 | Buy Now |
HAMMOND Metal Enclosure, 1455 Series, Extruded With Metal End Panels, Small, Extruded Aluminium, 49.7 mm | Hammond | 1 | Buy Now |
MICROCHIP USB Interface, Flash Media Controller, USB 2.0, 3 V, 3.6 V, QFN, 48 Pins | Microchip | 1 | Buy Now |
HAMMOND Metal Enclosure, Small, Extruded Aluminium, 12 mm, 70 mm, 101 mm, IP54 | Hammond | 1 | Buy Now |
MULTICOMP PRO Memory Card Connector, SD, Push-Push, 9 Contacts, Copper Alloy, Gold Plated Contacts, SDAMB | Multicomp | 1 | Buy Now |