Finally, the BeagleBone AI has been released and Clem is very excited to take it for a spin! He goes beyond his comfort zone and explore PRU (programmable real-time units), OPENCV (Image recognition) and much more on his journey to build an animatronic Terminator inspired skull. It even cites badly impersonated Arnold Schwarzenegger quotes when it detects a human face. This might not be the beginning of Skynet, but it may lead you to build your own AI powered projects!
Supplemental Content:
- Episode 418: Deep Diving the Code: Animatronic Terminator Skull
- Get the BB-AI Cooler add-on board PCB: https://aisler.net/p/SWHBYGQV
- You can find more information and the bill of materials of the BB-AI Cooler add-on board here: BB AI cooling Addon board available
- BeagleBone AI (BB-AI) - Getting Started
- BeagleBone
AI - Technical Specifications
Bill of Material:
Product Name | Manufacturer | Quantity | Buy Kit |
---|---|---|---|
Beaglebone AI | Beaglebone | 1 | Buy Now |
Arduino Nano | Arduino | 1 | Buy Now |
Fan 5V 25mm | Nidec | 1 | Buy Now |
Header | Adafruit | 1 | Buy Now |
HD-Webcam, 3MP, C270 | Logitech | 1 | Buy Now |
relais module | dfrobot | 1 | Buy Now |
microphone module | dfrobot | 1 | Buy Now |
BeagleBone AI Cooling Add-on Board Bill of Materials available here.
Additional Parts:
Product Name |
---|
BBAI-Cooler PCB available at Aisler.net |
Plastic Skull |
Standard Metal Gear Servos (3 pcs) |
Plywood, Paint, Filament |
USB Hub |
DFPlayer MP3 player module |
Animatronic Terminator Skull with BeagleBone
AI
Top Comments
I've been noticing a few Terminator projects recently, it is almost as if there's a new film out
tariq.ahmad, cstanton, Wow, this seems to be a good opportunity to get our hands on the BB AI and the MayerMakes' Add-On Cape.
Also, this terminator skull by mayermakes is really a motivation to think…
Yes I followed the blocks and raised that issue on github.
there is some work to be done to get back full BBIO compability, the Pinout is different for the BB Ai processor and the BBB so we either need…