Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Designing a More Capable Dual Motor Driver Beyond the L298N (What worked and what didn't)
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Toptech-Voices
Engagement
  • Author Author: cstanton
  • Date Created: 30 Apr 2026 9:16 AM Date Created
  • Last Updated Last Updated: 30 Apr 2026 12:27 PM
  • Views 8622 views
  • Likes 11 likes
  • Comments 19 comments

Designing a More Capable Dual Motor Driver Beyond the L298N (What worked and what didn't)

For any project where something moves, there is almost always an electric motor involved somewhere in the system. In this project, Milos Ras̆ić takes a deep dive into how brushed DC motors are actually driven, why many off‑the‑shelf modules fall short, and what it looks like to design a fully custom, open‑source dual motor driver PCB from scratch with real robotics use in mind.

Rather than jumping straight to a finished board, Milos deliberately walks through his entire engineering process: defining requirements, selecting components, validating assumptions, designing the PCB, assembling it methodically, debugging real‑world mistakes, and finally building firmware and a custom GUI to make the hardware genuinely usable. As he explains early on, this board is intended to become the low‑level motor control layer for his future robotic platforms, not a one‑off demo.
“I wanted to design my own custom PCB with certain requirements… and also take this chance to show you my whole engineering process – from the idea, through evaluation, and then iterating into the next versions.”

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

How Do Motor Drivers Work?

Milos begins by stripping motor control down to its simplest form. A brushed DC motor will spin if you connect it directly to a power source – effectively simulating a battery. That approach works, but only in the most basic sense. There’s no speed control, no direction control, and no feedback. The next step is switching the motor on and off rapidly. By toggling a switch hundreds or thousands of times per second and varying how long it stays on versus off, you create Pulse Width Modulation (PWM). A wider pulse delivers more energy to the motor; a narrower pulse reduces it.
To do this electronically, Milos demonstrates a simple N‑channel MOSFET circuit. A MOSFET behaves like a fast electronic switch and is far better suited to high‑frequency PWM than a relay. In his bench example, he uses an op‑amp as a level translator so that a 3.3 V microcontroller can properly drive a MOSFET that expects a much higher gate voltage. This approach works well for speed control, but it has a fundamental limitation: the motor only spins in one direction. As Milos points out:
“There really is no way to switch the direction of the motor driving besides flipping the wires around.”
Direction control requires a different topology altogether.
image

H‑Bridges and Direction Control

To reverse a motor electronically, you need to flip the polarity of the voltage applied to it. This is achieved using an H‑bridge, which arranges four transistors so current can flow through the motor in either direction.
Milos explains the logic clearly, including the importance of never enabling both transistors on the same side of the bridge at once, which would effectively short the supply. With an H‑bridge and PWM applied to the appropriate control line, you gain full control over both speed and direction. At this point, he references a familiar module:
“If you’ve ever played around with an Arduino… you’ve probably used an L298N.”
While popular, the L298N relies on BJTs rather than MOSFETs, making it inefficient and unsuitable for higher‑power applications. This inefficiency, combined with voltage drop and heat dissipation, is one of the main motivations for designing a custom solution.
image

Defining the Requirements

Before touching any schematic software, Milos creates a system requirements list. This list drives every design decision that follows and serves as a reference during revisions.
Key requirements include:
  • Driving two brushed DC motors
  • A single, compact PCB with the MCU onboard
  • At least 5 A continuous current per motor
  • A wide input voltage range (targeting 5 V–36 V, with ambitions beyond)
  • Clean, stable 3.3 V power for measurement and control
  • Current sensing for each motor
  • Extensive connector support for daisy‑chaining boards
“The requirement list is a really nice thing to have since it keeps you on track… and when you do revisions, you can fall back onto this and see if you’ve missed something.”

imageimage

image

Electronics and Power Architecture

With the requirements defined, Milos starts with the most critical component: the motor driver IC. After filtering options and reviewing datasheets, he selects a Texas Instruments dual H‑bridge driver capable of handling the required current in a compact package. That choice introduces an immediate design challenge: the driver requires a stable 12 V supply, regardless of the board’s input voltage. To solve this, Milos implements a buck‑boost converter, allowing the board to operate from roughly 4 V up to 40 V while still generating a clean 12 V rail.
From there, power is stepped down in stages:
  1. Buck‑boost → 12 V
  2. Buck → ~5 V
  3. LDO → 3.3 V
This staged approach reduces noise on the 3.3 V rail, which is critical for ADC measurements, current sensing, and encoder feedback.
“The LDO is like a smart resistor… you get a clean nice output of 3.3 V in the end.”
For current sensing, Milos chooses Hall‑effect current sensors rather than shunt resistors, valuing their stability and isolation.
The board also includes:
  • Input voltage measurement via a divider
  • A fuse for protection
  • XT‑style power connectors with additional communication pins
  • Switchable I²C pull‑ups
  • An RGB status LED controlled over I²C

imageimage

PCB Layout and Physical Design

Once the schematics are complete, Milos moves on to PCB layout. The final board measures 50 mm × 60 mm and uses a 4‑layer stack‑up (SIG–GND–GND–SIG). Much of the board size is dictated by the Raspberry Pi Pico 2 module, which Milos mounts directly rather than designing a custom RP2040 layout for this revision.
The PCB is dense but carefully partitioned:
  • Power conversion sits centrally
  • High‑current motor paths are kept short and wide
  • Sensitive analog and MCU sections are isolated
  • Large copper pours and a defined heatsink area help with thermal management
The result is a compact yet expandable board, complete with Milos’ Platypus mascot and a clear “GO VROOM!” silkscreen reminder of its purpose.
imageimage

Assembly, Checklists, and Debugging

Rather than soldering everything at once, Milos relies on a soldering and testing checklist, assembling and validating the board in stages:
  1. Buck‑boost converter
  2. Buck converter
  3. LDO
  4. Motor driver
  5. MCU and peripherals
This method quickly pays off. While the board works almost entirely as intended, two errors are discovered:
  • An incorrect footprint for one IC, requiring hand‑extended pins
  • A buck converter enable pin that could not tolerate 12 V, repeatedly destroying the IC
“Because of the checklist, I managed to identify what was wrong and why… otherwise I would’ve probably burned a lot more chips.”
Milos documents these issues in an errata sheet, reinforcing the idea that revision‑friendly design is part of good engineering.
On the software side, the board runs firmware that deliberately avoids high‑level robotics logic. Instead, it exposes a command‑driven motor control interface over USB, UART, and I²C.
The firmware is structured around several key components:
  • DualMotorController
    Handles PWM generation, fault detection, current measurement, and direction control.
  • ClosedLoopController
    Implements manual control, speed PID, and position PID modes.
  • As5600Encoder
    Interfaces with the AS5600 magnetic encoder, handling wrap‑around, filtering, and unit conversions.
  • CommandProcessor
    Parses human‑readable ASCII commands (M‑codes) and compact binary frames.
image
Notably, PWM is capped at 95% duty cycle (PWM_ACTIVE_MAX = 950) to ensure bootstrap capacitors in the motor driver remain charged – a subtle but important hardware‑aware firmware detail. Speed and position control are implemented using the PidController class, with tunable gains, integral limits, and output clamping.
In practice:
  • Speed control works best as a PI controller, since derivative action introduces too much noise at the encoder sampling rate.
  • Position control benefits from P and I terms, with careful tuning to avoid integral wind‑up.
“If you try doing anything with the derivative part, you just get a bunch of noise… so we’ll essentially just use a PI controller instead.”
The firmware also includes:
  • Automatic direction self‑checks
  • Encoder zeroing
  • Gain scheduling hooks for future improvements

To make tuning and testing practical, Milos builds a custom Python GUI using PySide6. The GUI provides:

  • Real‑time plots of speed, position, current, and PWM duty
  • Live status indicators for faults and thermal warnings
  • Manual control sliders
  • PID tuning panels
  • Encoder configuration and zeroing
  • Binary and ASCII telemetry support
This interface turns the board from “just hardware” into a usable development tool and makes PID behavior visually intuitive.
imageimage

Finished Project and What’s Next

In the end, Milos considers the project a success:
“I’m really happy with how this PCB turned out… it’s bigger than the module we started with, but it’s a lot more capable.”
The board meets nearly all of its original requirements, and the few shortcomings are clearly documented. Future plans include:
  • Integrating multiple boards into a robotic platform
  • Supporting mecanum wheel control
  • Further refining PID tuning and control abstractions
  • Iterating the PCB with lessons learned from revision one

Supporting Links and Files

-  Episode 712 Resources 

 

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
LT8350 ANALOG DEVICES 1 Buy Now
Inductor XAL6060-682MEC COILCRAFT 1 Buy Now
Resistor 0603 270k - MCWR06X2703FTL MULTICOMP PRO 1 Buy Now
Resistor 0603 100k - MCMR06X1003FTL MULTICOMP PRO 4 Buy Now
Capacitor 22uF 0805 25V - CL21A226MAYNNNE SAMSUNG 9 Buy Now
Connector PCB 2+2 - MP011760 MULTICOMP PRO 2 Buy Now
Connector Cable 2+2 - MP011759 MULTICOMP PRO 2 Buy Now
3V3 LDO - BD33HC0VEFJ-ME2 ROHM 1 Buy Now
Heatsink LTN20069 WKEFIELD THERMAL 1 Buy Now
Resistor 0603 - 1k MULTICOMP PRO 4 Buy Now
Resistor 0603 - 2k MULTICOMP PRO 1 Buy Now
Resistor 0603 - 4k7 MULTICOMP PRO 5 Buy Now
Inductor - ME3220-472MLC COILCRAFT 1 Buy Now
Capacitor 4.7uF 0603 MURATA 1 Buy Now
Resistor 0603 5k1 MULTICOMP PRO 1 Buy Now
Resistor 0603 10k MULTICOMP PRO 5 Buy Now
Capacitor 0805 10uF 50V MURATA 4 Buy Now
Capacitor 0603 22nF SAMSUNG 1 Buy Now
Capacitor 0603 100nF 50V SAMSUNG 17 Buy Now
Resistor 0603 143k MULTICOMP PRO 1 Buy Now
Capacitor 0603 470nF SAMSUNG 1 Buy Now
Fuse with Fuse Holder SMD - 0154010.DR LITTELFUSE 1 Buy Now
Buck Converter IC - AP62200Z6-7 DIODES INC 1 Buy Now
LED Red 0603 MULTICOMP PRO 1 Buy Now
LED Green 0603 MULTICOMP PRO 1 Buy Now
LED Blue 0603 MULTICOMP PRO 1 Buy Now
Inductor Ferrite Bead MPZ2012S221ATD25 TDK 1 Buy Now
Resistor 0603 1R MULTICOMP PRO 1 Buy Now
Capacitor 0603 1uF 25V SAMSUNG 7 Buy Now
Resistor 0603 3R3 MULTICOMP PRO 1 Buy Now
Resistor 0603 5R MULTICOMP PRO 4 Buy Now
Capacitor 0603 10nF 50V SAMSUNG 1 Buy Now
Resistor 0603 24K MULTICOMP PRO 1 Buy Now
Capacitor 47uF KEMET 1 Buy Now
Capacitor 330uF AISHI 1 Buy Now
Current Sensor IC - ACS722 ALLEGRO 2 Buy Now
Motor Driver IC - DRV8412DDWR TEXAS INSTRUMENTS 1 Buy Now
Capacitor 470uF 50V KYOCERA 2 Buy Now
Motor Connector - XT30 DFROBOT 2 Buy Now
SPI/GPIO Connector - PCB AMPHENOL 1 Buy Now
SPI/GPIO Connector - Cable AMPHENOL 1 Buy Now
SPI/GPIO Connector - Pins AMPHENOL 6 Buy Now
RGB LED WURTH ELEKTRONIK 1 Buy Now
Debug Connector JST 1 Buy Now
LED Driver IC NXP 1 Buy Now
Raspberry Pi Pico 2 RASPBERRY-PI 1 Buy Now
PullUp Resistor Switch RN2905 TOSHIBA 2 Buy Now
 

Additional Parts

Product Name Manufacturer Quantity
2mm pitch JST style SMD connectors N/A
Blank PCBs N/A
Brushed DC Motors N/A
AS5600 Encoder Module N/A
WAFER-PH2.0-4PLB N/A 4

  • wide coltage motor driver
  • robotics motor controller
  • motor driver debugging
  • high currentmotor driver
  • robotics electronics
  • h bridge motor driver
  • dual motor driver pcb
  • brushed dc motor control
  • pid motor control
  • raspberry pi pico motor driver
  • embedded motor control
  • motor driver design
  • current sensing motor driver
  • Custom PCB design
  • custom motor driver
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply
Parents
  • genebren
    genebren 6 days ago

    Excellent presentation.  I really like that you focused a lot on your requirements and tracking of errors and corrections. I have seen a lot of projects fail due not having clear/concise objectives. I look forward to seeing how this controller works in you robot project.

    Well done!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • milosrasic98
    milosrasic98 6 days ago in reply to genebren

    Thank you! Glad you liked that part, really tried putting the focus on how the whole process goes for me, thought it might be useful for someone! Not writing it down has come back to bite me way too many times, so I always do these types of lists now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • milosrasic98
    milosrasic98 6 days ago in reply to genebren

    Thank you! Glad you liked that part, really tried putting the focus on how the whole process goes for me, thought it might be useful for someone! Not writing it down has come back to bite me way too many times, so I always do these types of lists now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data