WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Documents How to Program Test Tools with Python - Workbench Wednesdays 66
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 28 Dec 2022 7:30 PM Date Created
  • Last Updated Last Updated: 14 Jun 2024 5:21 PM
  • Views 36012 views
  • Likes 5 likes
  • Comments 57 comments
Related
Recommended

How to Program Test Tools with Python - Workbench Wednesdays 66

If your test tools have a USB or LAN port, there is a good chance that they support SCPI. Using pyVISA, you can write automated test programs for most equipment without expensive software. This video explains terms like VISA, SCPI, and USBTMC. Then it shows how to use Python and pyVISA to connect to test equipment with a Raspberry Pi (or any Linux computer.)

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bonus Content:

  • PyVISA
  • RsInstrument, R&S Python Implementation (also uses pyvisa!)
  • Keysight IO Suite
  • R&S VISA
  • Standard Commands for Programmable Instruments (SCPI) Syntax. (web archive mirror IVI Foundation)
  • SCPI Specification
  • Blog post, Early peak at bode plot script
  • Snapshot of Code
  • Github link for code

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
34465A Bench Multimeter, Truevolt, 6.5 digit Keysight 1 Buy Now
TL081 - JFET General Purpose, 4 MHz SOIC-8 ST Microelectronics 1 Buy Now
Bench Oscilloscope - 200 MHz, 1 GSa/s, 14-bit, AFG, DMM Multicomp Pro 1 Buy Now
MXO4 - 4 Channel Oscilloscope 200 MHz Rohde & Schwarz 1 Buy Now
HMC8043 Bench Power Supply, Programmable, 3 Output, 0 V, 32 V, 3 A Rohde & Schwarz 1 Buy Now
RPI400-KIT-US Raspberry Pi 400 Kit, BCM2711, Quad-Core, 64bit, ARM, Cortex-A72, US PSU, US Keyboard Layout Raspberry Pi 1 Buy Now
 

element14 presents

element14 Presents  |  About James |  Workbench Wednesdays

  • Remote Programming
  • VXI
  • gpib
  • USBTMC
  • visa
  • lxi
  • IVI
  • scpi
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 2 years ago in reply to zack_el +3
    For some reason, posting these instructions here causes errors. You need to create a udev rule. Here's how to do it: www.baldengineer.com/accessing-usb-instruments-with-pyvisa-on-linux.html
  • mayermakes
    mayermakes over 3 years ago +1
    ohoh..I sense some automation i have to implement....
  • mayermakes
    mayermakes over 3 years ago in reply to baldengineer +1
    if anyone has a gripe with using a pi, I can warmly recommend doing it with a Beaglebone black. this also gave me the idea of maybe developing some sort of plug and play box with a pocketbeagle that reads…
Parents
  • halnaabi
    halnaabi over 2 years ago

    Thank you for sharing this informative video! I found it really helpful in understanding how to program and test tools with Python.

    I have a question regarding the VICTOR 8246A DMM. Despite my efforts, I couldn't locate any proper documentation for this model, especially concerning remote connectivity. I'm attempting to establish a remote connection with the instrument but haven't had much luck. Do you have any advice or resources you could recommend?

    Thanks in advance for any assistance you can provide!

    Here is the Hello World code: 

    import pyvisa
    from time import sleep  # for delays
    
    # Initialize the PyVISA resource manager
    ResourceManager = pyvisa.ResourceManager()
    
    # List all connected resources
    print("Resources detected\n{}\n".format(ResourceManager.list_resources()))
    #Resources detected ('ASRL4::INSTR', 'USB0::###############', 'ASRL3::INSTR')
    
    
    # Open a connection to the DMM (Digital Multimeter) device
    DMM = ResourceManager.open_resource('ASRL3::INSTR')
    
    # Set the baud rate for the serial interface
    DMM.baud_rate = 115200
    DMM.query_delay = 0.3
    DMM.write_termination = '\n'
    DMM.read_termination = '\n'
    
    # Print information about the connected device
    print(DMM) # SerialInstrument at ASRL3::INSTR
    
    # Send command to the DMM to query its identification
    print(DMM.query("*IDN?"))
    
    # Close the connection to the DMM
    DMM.close()

    Here is the error that I got: 

    , line 251, in handle_return_value raise errors.VisaIOError(rv)
    pyvisa.errors.VisaIOError: VI_ERROR_TMO (-1073807339): Timeout expired before operation completed.
    

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to halnaabi

    I would try using a serial terminal to connect to it first. That way you might be able to figure out what it is doing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • halnaabi
    halnaabi over 2 years ago in reply to baldengineer

    import serial
    import time
    
    # Define serial port settings
    port = 'COM3'
    baud_rate = 115200 #9600
    timeout = 1
    
    # Open serial port
    ser = serial.Serial(port, baud_rate, timeout=timeout)
    
    try:
        # Send SCPI command to query instrument identification
        command = "*IDN?\n" #\n\r
        ser.write(command.encode())  # Send the command as bytes
        time.sleep(0.3)
    
        # Read response from the DMM
        response = ser.read_all().decode()
        print("Instrument Identification:", response.strip())
    except serial.SerialException as e:
        print("Serial communication error:", e)
    finally:
        # Close serial port
        ser.close()

    Output: 

    Instrument Identification: 
    
    Process finished with exit code 0

    A serial connection is established successfully, but the digital multimeter (DMM) does not respond to the commands sent to it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to halnaabi

    Does it work when you connect through a serial terminal and type commands?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • baldengineer
    baldengineer over 2 years ago in reply to halnaabi

    Does it work when you connect through a serial terminal and type commands?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • halnaabi
    halnaabi over 2 years ago in reply to baldengineer

    Unfortunately not, 

    import serial; ser = serial.Serial('COM3', 115200, timeout=5); ser.write(b'*IDN?')

    Output: 

    4 or 5

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to halnaabi

    Try to add a newline.

    SCPI Command Terminators:

    A command string sent to the instrument must terminate with a <new line> (<NL>) character. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • halnaabi
    halnaabi over 2 years ago in reply to Jan Cumps

    Type "help", "copyright", "credits" or "license" for more information.
    >>> import serial; ser = serial.Serial('COM3', 115200, timeout=5); ser.write(b'*IDN?\n\r'); ser.close()
    7
    >>> import serial; ser = serial.Serial('COM3', 115200, timeout=5); ser.write(b'*IDN?\n'); ser.close()
    6
    >>> import serial; ser = serial.Serial('COM3', 115200, timeout=5); ser.write(b'*IDN?'); ser.close()
    5
    >>> import serial; ser = serial.Serial('COM3', 115200, timeout=5); ser.write(b'RST'); ser.close()
    3
    >>>

    • Cancel
    • Vote Up 0 Vote Down