WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Documents Workbench Wednesday 24: No-Contact Current Measurements
  • Blog
  • Forum
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
WorkBench Wednesdays requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 28 May 2020 5:39 PM Date Created
  • Last Updated Last Updated: 19 Aug 2020 2:05 PM
  • Views 975 views
  • Likes 4 likes
  • Comments 13 comments
Related
Recommended

Workbench Wednesday 24: No-Contact Current Measurements

No-Contact Current Measurements

element14 Presents  |  Bald Engineer: James Lewis' VCP Profile |  Workbench Wednesdays

 

You don't have permission to edit metadata of this video.
Edit media
x
Upload Preview

 

One of the safest ways to measure current is with a clamp. Clamps do not require you to break the circuit and they safely measure wires with thousands of amps. In this video, we measure DC current in the lab, AC current of a reflow oven controller, and the DC current in a car using a Tenma 72-722672-7226 True RMS Clamp Meter.

 

Bill of Material:

 

Product NameManufacturerQuantityBuy KitBuy Kit
72-722672-7226 - Clamp Meter, Auto, True RMS, 600 A AC, 600 V AC, 600 V DC, 28 mm Jaw Opening Max.Tenma1Buy NowBuy Now
  • current clamp
  • ac current
  • clamp meter
  • Share
  • History
  • More
  • Cancel
Anonymous

Top Comments

  • baldengineer
    baldengineer over 2 years ago in reply to koudelad +3

    Hey David, for low currents, that is a good way to improve the overall measurement accuracy. I did not mention it in this video because I was focused on getting closer to the meter's maximum current.…

  • jw0752
    jw0752 over 2 years ago +3

    Hi James,

     

    Your blog inspired me to run an experiment. I had in stock this current measuring board with a ACS712T ECL20 Chip on it.

     

     

    I cut a notch in a ferrite core that was just big enough to slip over the…

  • jw0752
    jw0752 over 2 years ago +3

    Hi James,

     

    I purchased one of these meters from Newark and I have been quite happy with it. I have also found another use for it. Over the years my experiments have often involved magnets. Sometimes the…

Parents
  • kb3gkc
    kb3gkc over 2 years ago

    Great episode! Thank you.

     

    I'm more of a tech (hack) than an engineer so I need some help with a project.

    I need to build an over current alarm circuit for AC. The current in the circuit is typically between 70mA and 200mA. I'm going to have it alarm around 350mA.

    I've been looking at different current sensors and I'm not really sure what to use. Hall effect or Current transformer.

    Then there's the actual circuit to make the alarm. I'm assuming a differential opamp but I'm a little lost as to how to configure it.

    I've been researching it but I'm a bit confused. My plans is to drive a small piezo buzzer.

    I would rather not break the circuit and would like to use a split core CT for ease of installation. But I'm not sure if that will give me enough sensitivity/resolution.

     

    I'd really appreciate any advice or pointing me in the right direction.

    Thanks!!!

    Mitch

    • Cancel
    • Vote Up +1 Vote Down
    • Reply
    • More
    • Cancel
  • jw0752
    jw0752 over 2 years ago in reply to kb3gkc

    Hi Mitch,

     

    There are specially configured Op Amps called Comparators that might work well for your application. They will not only trigger at a tipping point like the 350 mA that you mentioned but they also have some hysteresis so that you get a definite On - Off from them. I have used the LM 339 quite a bit but here are others that you can look at as well.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Reply
    • More
    • Cancel
  • kb3gkc
    kb3gkc over 2 years ago in reply to jw0752

    Thanks John!

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • More
    • Cancel
Comment
  • kb3gkc
    kb3gkc over 2 years ago in reply to jw0752

    Thanks John!

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • More
    • Cancel
Children
No Data