WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Documents Op Amps Without Op Amps - Workbench Wednesdays 39
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: Matt
  • Date Created: 8 Jun 2021 4:49 PM Date Created
  • Last Updated Last Updated: 16 Jun 2021 7:24 AM
  • Views 3863 views
  • Likes 11 likes
  • Comments 9 comments
Related
Recommended

Op Amps Without Op Amps - Workbench Wednesdays 39

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Okay, technically, this circuit *does* use Op-Amps. However, the ones shown here are integrated into an ATmega128DB microcontroller from Microchip. The DIP package breaks out two operational amplifiers that are controllable entirely by software. Even better, you can program like they are an Arduino!

 

Supplemental Content:

  • Pocket Op-Amp Lab technoblogy: Technoblogy - Pocket Op Amp Lab
  • The Learning Circuit 68: How Op Amps Work
  • DxCore ATmega128DB for Arduino IDE:  https://github.com/SpenceKonde/DxCore
  • 7 reasons why I like the ATmega128Dx MCUs

 

Bill of Material:

Product Name Manufacturer Quantity Buy Now
AVR128DB MCU, 8BIT, 24MHZ, SPDIP-28 ROHS COMPLIANT: YES Microchip 1 Buy Now
Evaluation Board, MCU 8-Bit, Arduino Nano, AVR, ATmega328 Arduino 1 Buy Now
USB to UART (Serial) Board FTDI 1 Buy Now
Digital Oscilloscope, 14-bit, 4-in-1, 2+1 Channel, 200 MHz, 1 GSPS, 40 Mpts, 1.7 ns Multicomp 1 Buy Now

Attachments:
Op_Amps_Without_Op_Amps_Resources.zip

 

Workbench Wednesday
element14 presents  |  About James |  Workbench Wednesdays

  • opampsch
  • programmable gain amplifier (pga)
  • amplifier
  • amplifer
  • e14presents_baldengineer
  • microcontroller
  • workbench wednesdays
  • op amps
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 4 years ago in reply to rsjawale24 +2
    I would recommend against this method. Voltage dividers are lousy voltage sources, especially for a circuit like an op-amp. As the current draw changes, the supply voltages are going to change. The result…
  • DAB
    DAB over 4 years ago +1
    Very cool chip. You did a good job of showing off some of its capabilities. You could easily do a series of shows to really put the chip to some use cases. DAB
  • baldengineer
    baldengineer over 4 years ago in reply to koudelad +1
    Ouch. I know there are some other mixed-signal chips out there. Silego? I don't think this microcontroller is meant to compete there. I really think this is a case where they had amplifiers for the DAC…
Parents
  • koudelad
    koudelad over 4 years ago

    Great demonstrations of the chip features.

     

    At first I wanted to write that it seems like the competition is only slowly trying to catch up with Cypress PSoCs that also feature ADC, voltage / current DAC, op amps / comparators and analog multiplexors and most importantly a graphical IDE (PSoC Creator) that makes the development super easy - you can draw a schematics that is part of the project.

    However, newer PSoC 6 is recommended to be developed on a multiplatform Eclipse-based IDE (Modus Toolbox) that lacks the graphical editor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • koudelad
    koudelad over 4 years ago

    Great demonstrations of the chip features.

     

    At first I wanted to write that it seems like the competition is only slowly trying to catch up with Cypress PSoCs that also feature ADC, voltage / current DAC, op amps / comparators and analog multiplexors and most importantly a graphical IDE (PSoC Creator) that makes the development super easy - you can draw a schematics that is part of the project.

    However, newer PSoC 6 is recommended to be developed on a multiplatform Eclipse-based IDE (Modus Toolbox) that lacks the graphical editor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • baldengineer
    baldengineer over 4 years ago in reply to koudelad

    Ouch. I know there are some other mixed-signal chips out there. Silego? I don't think this microcontroller is meant to compete there.

     

    I really think this is a case where they had amplifiers for the DAC and ADC already and just extended the functionality a little bit.