DIY Test Equipment
  • Challenges & Projects
  • Project14
  • DIY Test Equipment
  • More
  • Cancel
DIY Test Equipment
Blog Vintage 555 - A general-purpose button debouncer
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join DIY Test Equipment to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 12 Aug 2017 2:24 PM Date Created
  • Views 13927 views
  • Likes 8 likes
  • Comments 26 comments
  • mini-project
  • micro controller
  • vintage
  • diytestequipch
  • ne555
  • genuino 101
  • button tool
  • debouncer
  • testing equipment
  • arduino
Related
Recommended

Vintage 555 - A general-purpose button debouncer

balearicdynamics
balearicdynamics
12 Aug 2017

Too many button clicks

Buttons and tactile switches are frequently used in many projects involving micro controllers; one of the most frequent issue is related to unwanted multiple transitions when the button is pressed once.

Tactile switches as well as push buttons are mechanical components subject to the problem of bouncing. When a button is connected to a digital GPIO input pin (i.e. an Arduino pin configured as INPUT) we ideally expect that when the button is pressed we get only one high signal; unfortunately this rarely happens. During the mechanical movement the physical material vibrates affecting the voltage and the transitions between the On/Off status are not so clear as we usually need. Micro controllers and FPGA are fast enough reading the microseconds oscillations when the button is pressed, resulting multiple transitions while apparently we are pressing the button only once.

 

Button debouncing

To solve this problems we should apply a button debouncing to reach the goal: pressing a button only one signal should be detected by the micro controller digital input. We can identify two possible approaches: software and hardware.

There are plenty of source examples on how to debounce a button via software; the software approach seems the easiest way but in my opinion this is one of the cases where a hardware solution may be more efficient and resource saving. Micro controllers have memory and resource limits so adding a debouncing routine maybe critical in many cases.

 

The hardware choice

As I had to add a button debouncer to a test project based on Arduino 101 I decided to make something as much general as possible, easy to adapt to almost any micro controller and possibly platform independent. I figured two possible approaches: RC (resistor-capacitor) method and IC method. The RC option is easier to realise but I am not so confident it can be applied to very different operating conditions (e.g. very different micro controllers types and clock speed). It is not so difficult to calculate the values of resistor and capacitor for a RC debouncing circuit but I see a limitation restricting the application range. The calculation of the RC circuit is  dependent on the voltage of the board used; this means that for different voltage boards (1.8V, 3.3V, 5V etc.) we should provide a different RC calculation.

The RC simple circuit shown in the image below can be calculated with the nice RC Debounce online calculator

image

The parameters involved in the calculation are:

 

  • Voltage
  • High logic level
  • Bounce time (ms)
  • Capacitor value
  • Resistor value

 

The other hardware alternative is adopting a debouncing IC.

There are many specific IC for mechanical contacts debouncing, but they are almost expansive and oriented to manage power buttons while we generally use a push button is to generate a logic signal. The LTC2951CTS8 for example sounds good (not sure if the DIL version is available) with a base price of about 5$.

This is why I decided to move to a general-purpose debounce circuit based on the Vintage NE555. TI provides a wide range of 555 ICs including DIL packaging covering a range supply levels from 1.5V up to 16V; the most common is the DIL package NE555-P in the range between 4.5V and 16V. Just what I need, sold at 1/10 (one tenth) of the specialised debouncing ICs average price!

 

The NE555 circuit

image

I designed the circuit based on the popular NE555 monostable configuration shown above and detailed in the below schematics:

image

In this specific case using the two 10uF capacitors connected in parallel to the discharge pin and the 10K resistor for charging we get a timing of about 220 ms. It is a reasonable value to debounce a tactile switch connected to a digital input pin of an Arduino board; changing the values of the capacitors and the resistor we can increase or reduce the charge time resulting a different timing to the output pin (debounced signal.

 

Wiring the circuit

Using the NE555-P IC the circuit can be powered by the Arduino itself; the images below show the circuit placed as part of the Arduino 101 project where a push button is needed. The small board can also host the designated button making a compact object independent by the platform (an external power source can also be used) involving only the debounced signal connected to the desired GPIO micro controller pin.

imageimage

imageimage

imageimage

The resulting PCB is about 30x35 mm; I have provided a tactile switch button surface mounted on the opposite side of the components to make easier assembling the module in any project.

imageimage

The button in action

The video below shows the debouncer module at work powered by the Arduino 101 and a couple of screenshots showing the stability of the signal

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

imageimage

 

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 8 years ago +3
    Hi Enrico, Thanks for this post. It will be very useful for anyone with a switch that needs debouncing. I love the production of your videos, always so professional. I always think of you and smile when…
  • koudelad
    koudelad over 8 years ago in reply to balearicdynamics +3
    I agree. I just wanted to point out that the Debouncer datasheet shows the circuit diagram and it can even be built by the internal components manually (Or even external discreet components, but this would…
  • dougw
    dougw over 8 years ago in reply to balearicdynamics +3
    These are just alternatives for particular requirements: Sometimes the priority is for minimum hardware cost - software debounce is the lowest hardware cost and easiest to wire up. The other hardware solutions…
Parents
  • dougw
    dougw over 8 years ago

    Great topic - good job on the blog.

    Good way to use up those 555s.

     

    A couple of additional points:

    • As Michael points out, if the switch is connected to an arduino, it can be debounced with software - no extra components or wiring.
    • If you need perfect and instantaneous debouncing you can use two switches (one for set and one for reset) or a double throw switch also performing set and reset - my favourite is to connect a SPDT switch to cross-coupled inverters or NAND gates.
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 8 years ago in reply to dougw

    Doug,  I know that exist software debouncing and not only for the Arduino. But you should involve timing in a loop, counting and more. This result in spending MCU resources, just on an Arduino device where resource are rarely redundant. Then, if you debounce via software as far as I know you can't use the button interrupt driven that is useful in a lot of cases.

     

    Instead, about the two switches, also in this case I think it is more mechanical complex and I lose the elegance of a button that works as a button. Or I have not understood clear what you wrote.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 8 years ago in reply to dougw

    Doug,  I know that exist software debouncing and not only for the Arduino. But you should involve timing in a loop, counting and more. This result in spending MCU resources, just on an Arduino device where resource are rarely redundant. Then, if you debounce via software as far as I know you can't use the button interrupt driven that is useful in a lot of cases.

     

    Instead, about the two switches, also in this case I think it is more mechanical complex and I lose the elegance of a button that works as a button. Or I have not understood clear what you wrote.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 8 years ago in reply to balearicdynamics

    These are just alternatives for particular requirements:

    Sometimes the priority is for minimum hardware cost - software debounce is the lowest hardware cost and easiest to wire up.

    The other hardware solutions are for when you need instant response and perfect debounce.

    In some circumstances instant response can also be achieved in software.

    • Cancel
    • Vote Up +3 Vote Down