Fighting Germs
  • Challenges & Projects
  • Project14
  • Fighting Germs
  • More
  • Cancel
Fighting Germs
Blog Japanese Product to Fight Covid-19 Using Safe UV Light
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Fighting Germs to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 7 Oct 2020 9:53 PM Date Created
  • Views 1110 views
  • Likes 5 likes
  • Comments 3 comments
  • japan
  • lighting
  • ppe
  • covid
  • uv light
  • covid-19
  • cabeatwell
  • medical
  • innovation
Related
Recommended

Japanese Product to Fight Covid-19 Using Safe UV Light

Catwell
Catwell
7 Oct 2020

image

A Japanese company built a UV lamp that can destroy Coronavirus present on surfaces without harming humans. Care 222 being demonstrated in a dark space. (Image credit: Toshiba)

 

In a world where people are still dying from being infected by the Coronavirus, it is vital to tackle the disease from all fronts: on surfaces, outside the body, in the air, every front  until we find a vaccine. One of the many contributors to the fight, Ushio Inc., a company specialized in light making, wants to use UV light to sanitize spaces where the virus can spread quickly due to the volume of people utilizing those spaces.

 

There are three types of UV light commonly used: UVA, UVB and UVC. For decades now, UVC, the most effective of the 3 types, has been used in the healthcare industry to kill off and stop the spread of infectious diseases such as tuberculosis. UVC light has been nicknamed the germicidal light. According to the FDA, UVC is effective in destroying the outer protein layer of the SARS-Cov-2 virus, which ultimately leads to its destruction, but only when the virus is exposed directly to the light. Besides, the current UVC lamps sold for home use offer only a low dose of light, so it requires a long application to a surface in order to be effective against Covid-19. In other words, it makes sense for a company to create a UV light product to aid the fight against COVID-19 if they can address those limitations.

 

Ushio Inc. created the Care 222 UV lamp in collaboration with researchers at Columbia University. The lamp is meant to disinfect high foot traffic spaces such as buses, elevators and offices as it would be easier to be exposed to the virus in those places. In the past, the sterilization with a UV lamp could only happen when there was no human being in the space to be disinfected. Otherwise, people could develop skin cancer and vision problems from the radiation. Ushio, Inc. solves that issue by lowering the wavelength of its product to 222 nanometers from the conventional 254 nanometers. The research team explained that, at that wavelength, Care 222 cannot penetrate the human skin and, therefore, cannot cause any damage.

 

The Care 222 must be attached to the ceiling of the space to be disinfected. At a weight of 1.2 KG, the Care 222 is light enough to be carried around easily but powerful enough to kill about 99 percent of germs in a 3-square-meter space, both in the air and on the surface of objects. A research team of the Hiroshima University tested Care 222 and found that it was effective, even on surfaces placed 8.2 feet away from the lamp. Unfortunately, Care 222 is only offered to the medical field at the moment and sells for ¥300,000 or about $2,850. At that price tag, it’s hard for many households to own Care 222. But Ushio Inc. is partnering with Toshiba lighting and technology Corp., a branch of Toshiba Corp., to offer alternatives.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • dougw
    dougw over 5 years ago

    Yikes. I would like to see real proof that high-energy UVC can't penetrate skin, cause sun burn, damage cells or cause cataracts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sunnyiut
    sunnyiut over 3 years ago in reply to dougw

    Right. Recent studies show results in favor of it but still it is a matter of concern indeed. actually it's FAR UVC and 200 - 222 nm cannot penetrate human skin at the dose we need to have germicidal effect to germs. Like, as far as I know SARS Cov-2 gets inactivated only at 2-3 mJ/cm2 exposure. Recent studies proved that it's safe for human skin. I think it is already approved by FDA too. However, I believe more research needs to be carried out in multidimensional clinical test to increase the credibility of this technology. Here are a couple of links just for your reference -
    https://www.nature.com/articles/s41598-020-67211-2
    www.ncbi.nlm.nih.gov/.../

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • sunnyiut
    sunnyiut over 3 years ago in reply to dougw

    Right. Recent studies show results in favor of it but still it is a matter of concern indeed. actually it's FAR UVC and 200 - 222 nm cannot penetrate human skin at the dose we need to have germicidal effect to germs. Like, as far as I know SARS Cov-2 gets inactivated only at 2-3 mJ/cm2 exposure. Recent studies proved that it's safe for human skin. I think it is already approved by FDA too. However, I believe more research needs to be carried out in multidimensional clinical test to increase the credibility of this technology. Here are a couple of links just for your reference -
    https://www.nature.com/articles/s41598-020-67211-2
    www.ncbi.nlm.nih.gov/.../

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data