Merry Boxes & LEDs
  • Challenges & Projects
  • Project14
  • Merry Boxes & LEDs
  • More
  • Cancel
Merry Boxes & LEDs
Blog JackBox #4 : Some Decoration and LEDs
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Merry Boxes & LEDs to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 5 Jan 2019 2:45 PM Date Created
  • Views 1872 views
  • Likes 12 likes
  • Comments 7 comments
  • merryboxesledsch
  • leds.
Related
Recommended

JackBox #4 : Some Decoration and LEDs

dubbie
dubbie
5 Jan 2019
image

Merry Boxes & LEDs

Enter Your Project for a chance to win a Maker Tool Kit, an Oscilloscope Grand Prize for the project that brings the Most Joy to the Heart, and Gift to Gives!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

I wanted to have some decoration appearing out of the box when the lid opens so I decided to add a wooden laser-cut white star. I didn't make this, it came from a set of battery operated LED Christmas lights that I purchased in the clearance sale after Christmas. The LED lights were just push fixed into a double star so I unclipped the LED, separated one of the stars and worked out how to fix it to the lid. I wanted it to sort of dangle as the lid opened so I decided to use a pivot. By pure coincide the pivot I had already made for the lid opening mechanism seemed about right so I just printed off two more.  I initially tried printing these together with the rafts overlapping, thinking the printer would be smart enough to work out a combined raft. I was wrong. It attempted to print both rafts so where they overlapped it became very lumpy and looked likely to fail. So I stopped that printed and used auto-place to fit the two parts in and printed that way. It worked OK, so I will not be overlapping rafts again on my 3D printer.

 

The wooden stars were just a little bit too large to fit inside the box so I used by cutters to remove the points, tided up the cut with a sharp blade and it is fine. For the dangling hinge mechanism I had to round off the corners so that they would rotate nicely. So after a bit of cutting and some sand papering they look OK and the star dangles, sort of. I hadn't realised that the centre of gravity would be behind the star so it dangles at an angle rather than straight down. I do not think there is anything much I can do about that.

 

I had some LED strip salvaged from a bathroom vanity mirror so I decided to stick a few of those inside the box. The strip is 12V so I have had to use an external power supply for that, but they are nice and bright so I will probably leave them. I had already decided that I wasn't going to be able to get the Arduino and batteries inside the box so I eventually gave-up and drilled some holes in the back, as suggested by Enrico Miginno. Below is the video showing these enhancements. The LEDs are turned down in brightness because the camera just overloads on white on full LED power and you just cannot see anything. It does work quite well in real life.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

I will just spruce it up a bit now, maybe some more stars, more LEDs and see if I can get the sound part to work.

 

Dubbie

  • Sign in to reply

Top Comments

  • anupash.1002
    anupash.1002 over 6 years ago +5
    works nicely. could do with some music in the background. Then you will not hear the motor cranking
  • dougw
    dougw over 6 years ago +4
    Looking good. If you want to change the hanging angle, you try a counterweight to move the C of G directly below the suspension point.
  • genebren
    genebren over 6 years ago +3
    Looking good! Looking forward to seeing the whole package together and working. Keep up the good work. Gene
Parents
  • ipv1
    ipv1 over 6 years ago

    Cool idea for the box decor. Nicely done.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ipv1
    ipv1 over 6 years ago

    Cool idea for the box decor. Nicely done.

    • Cancel
    • Vote Up +2 Vote Down
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.