Remote Monitoring & Control
  • Challenges & Projects
  • Project14
  • Remote Monitoring & Control
  • More
  • Cancel
Remote Monitoring & Control
Blog Air Quality Monitoring Using Particle Photon
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Remote Monitoring & Control to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ruchir1674
  • Date Created: 22 Jun 2019 6:23 PM Date Created
  • Views 2722 views
  • Likes 10 likes
  • Comments 8 comments
  • remotemonitoringcontrolch
Related
Recommended

Air Quality Monitoring Using Particle Photon

ruchir1674
ruchir1674
22 Jun 2019
image

Remote Monitoring & Control

Enter Your Electronics & Design Project for a chance to win up to a $200 Shopping Cart of Product!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

                                                                         image

 

Introduction

 

In this project PPD42NJ particle sensor is used to measure the air quality (PM 2.5) present in the air with Particle Photon. It not only display the data on Particle console and dweet.io but also indicate the air quality using RGB LED by changing its color.

 

Components

 

Hardware

  • Particle Photon ==> $ 19
  • Seeed PPD42NJ dust sensor ==> $7.20
  • RGB anode / cathode LED ==> $ 1
  • 10k Resistor ==> $ 0.04
  • 3 x 220 Ω Resistor ==> 0.06

Software

  • Particle Web IDE
  • dweet.io

Total price is around $ 28

About PM (Particulate Matter)

 

 

Particulate matter (PM) in the atmospheric air or in any other gas cannot be expressed in terms of ppmv, volume percent or mole percent. PM is expressed as mg/m^3 or μg/m^3 of air or other gas at a specified temperature and pressure.

 

Note:- One volume percent = 10, 000 ppmv (parts per million by volume) with a million being defined as 10^6.

 

Care must be taken with the concentrations expressed as parts per billion by volume (ppbv) to differentiate between the British billion which is 10^12 and the USA billion which is 10^9.

 

Particulate matter is the sum of all solid and liquid particles suspended in air many of which are hazardous. This complex mixture includes both organic and inorganic particles.

Based on size, particulate matter is often divided into two groups.

 

1. Coarse particles (PM 10-2.5) such as those found near roadways and dusty industries range in diameter from 2.5 to 10 micrometers (or microns). The existing coarse particle standard (known as PM 10) includes all particles less than 10 microns in size.

 

2. "Fine particles" (or PM 2.5) are those found in smoke and haze have diameters less than 2.5 microns. PM 2.5 is referred to as "primary" if it is directly emitted into the air as solid or liquid particles, and is called "secondary" if it is formed by chemical reactions of gases in the atmosphere.

 

Which of PM2.5 and PM10 is more harmful?

 

The smaller particles or PM2.5 are lighter and go deeper into the lungs and cause greater damage longer term. They also stay in the air longer and travel farther. PM10 (big) particles can stay in the air for minutes or hours while PM2.5 (small) particles can stay in the air for days or weeks.

 

Note:- PM2.5 or PM10 data on online websites is represented as AQI or ug/m3. If the PM2.5 value is 100, then if it is represented as AQI then it will fall in the 'Satisfactory' category but if it is represented as ug/m3 then it will fall under the 'Poor' category.

 

                                                                               image

 

 

PPD42NJ Dust Sensor

 

Based on the light scattering method, it detects airborne particles continuously. Pulse output that corresponds to concentration per unit volume of particles can be obtained with using an original detection method based on light scattered principle similar to the particle counter.

 

Front side

 

On the front, it has 2 pots labelled VR1 and VR3 that have been already factory-calibrated. The IR detector is covered under the metal can. Interestingly there’s a slot by the side labelled SL2 which is unused.

 

                    image

 

                                                                    image

 

 

 

 

 

Back side

The circuit consists largely of passives and an op-amp. RH1 is the resistor heater which, in theory, could be removed to save power if there was some other method of air circulation.

 

                                            image

Sensor Placement (important)

 

 

There are several points that should be observed when deciding how the sensor is placed.

 

  • The sensor must be placed in a vertical orientation. Any other orientation would not achieve the desired airflow.
  • The sensor should be kept in a dark condition.
  • Soft cushioning material to seal the gap between sensor and housing is necessary.

 

Seal the gap using foil paper as shown below

                                                                                    image

 

The sensor output is normally high, but goes low in proportion to the PM concentration, hence by measuring what they call Low Pulse Occupancy (LPO), the PM concentration can be determined. This LPO is recommended to be measured over a unit time of 30 seconds.

 

RGB LED

 

There are two kinds of RGB LEDs

  • Common anode LED

In a common anode RGB LED, the three LEDs share a positive connection (anode).

  • Common cathode LED

In a common cathode RGB LED, all three LEDs share a negative connection (cathode).

 

                                                                 image

 

Particle Photon

 

Photon is a popular IOT board.The board houses STM32F205 120Mhz ARM Cortex M3 microcontroller and has 1 MB flash memory, 128 Kb RAM and 18 mixed signal general purpose input output (GPIO) pins with advanced peripherals. The module has on-board Cypress BCM43362 Wi-Fi chip for Wi-Fi connectivity and Single band 2.4GHz IEEE 802.11b/g/n for Bluetooth. The board comes equipped with 2 SPI, one I2S, one I2C, one CAN and one USB interface. It should be noted that 3V3 is a filtered output used for analog sensors. This pin is the output of the on-board regulator and is internally connected to the VDD of the Wi-Fi module. When powering the Photon via VIN or the USB port, this pin will output a voltage of 3.3VDC. This pin can also be used to power the Photon directly (max input 3.3VDC). When used as an output, the max load on 3V3 is 100mA. The PWM signals have a resolution of 8-bit and run on a frequency of 500 Hz.

 

Pin Diagram

 

                                                    image

 

Pin Description

 

                                                                               image

 

Dweet.io

 

dweet.io enables your machine and sensor data to become easily accessible through a web based RESTful API, allowing you to quickly make apps or simply share data.

 

1. Go to dweet.io

 

                image

 

2. Go to dweets section and create dweet for a thing.

 

              image

3. You will see page like this. Enter a unique name of a thing. This name will be used in Particle photon.

                                   

 

              image

 

Now, we are done with dweet.io setup.

 

Particle Web IDE

 

For writing the program code for any Photon, developer needs to create an account on Particle website and register the Photon board with his user account. The program code then can be written on Web IDE at the Particle's website and transferred to a registered photon over the internet. If the selected Particle board, Photon here, is switched on and connected to cloud service of the Particle, the code is burnt to the selected board over the air via internet connection and the board starts operating according to the transferred code. For controlling board over the internet, a web page is designed which uses Ajax and JQuery to send data to the board using HTTP POST method. The web page identifies the board by a device ID and connects to the Particle's Cloud Service through an access token.

 

How to connect photon with Internet


1. Power your device

  • Plug the USB cable into your power source.
  • As soon as it is plugged in, the RGB LED on your device should begin blinking blue.If your device is not blinking blue, hold down the SETUP button.If your device is not blinking at all, or if the LED is burning a dull orange color, it may not be getting enough power. Try changing your power source or USB cable.

 

2. Connect your Photon to the Internet

There are two ways either you use web application or mobile app


a. Using web application

  • Step 1 Go to particle.io
  • Step 2 Click on setup a Photon
  • Step 3 After clicking on NEXT, you should be presented with a file (photonsetup.html)
  • Step 4 Open the file.
  • Step 5 After opening the file connect your PC to the Photon, by connecting to the network named PHOTON.
  • Step 6 Configure your Wi-Fi credentials.

Note:- If you mistype your credentials, the Photon will blink dark blue or green. You have to go through the process again (by refreshing the page or clicking on the retry process part)

  • Step 7 Rename your device. You will also see a confirmation if the device was claimed or not.

 

b. Using smartphone

  • Open the app on your phone. Log in or sign up for an account with Particle if you don't have one.
  • After login, press the plus icon and select the device you'd like to add. Then follow the instructions on the screen to connect your device to Wi-Fi. If this is your Photon's first time connecting, it will blink purple for a few minutes as it downloads updates. It may take 6-12 minutes for the updates to complete, depending on your internet connection, with the Photon restarting a few times in the process. Do not restart or unplug your Photon during this time.

 

Once you have connected your device. Your device can store up to five networks. To add a new network after your initial setup, you'd put your device into Listening Mode again and proceed as above. If you feel like your device has too many networks on it, you can wipe your device's memory of any Wi-Fi networks it has learned. You can do so by continuing to hold the setup button for 10 seconds until the RGB LED flashes blue quickly, signaling that all profiles have been deleted.

 

Modes

 

  • Cyan, your Photon is connected to the Internet.
  • Green, it is trying to connect to the internet.
  • Magenta, it is currently loading an app or updating its firmware. This state is triggered by a firmware update or by flashing code from the Web IDE or Desktop IDE. You might see this mode when you connect your Photon to the cloud for the first time.
  • White, the Wi-Fi module is off.

Web IDE

 

Particle Build is an Integrated Development Environment, or IDE that means that you can do software development in an easy-to-use application, which just so happens to run in your web browser.

 

  • To open build, login to your particle account and then click on Web IDE as shown in image.

 

                                                                image

 

  • Once you clicked you will see console like this.

                                                                                                                                                                                                                                                                      

               image

  • To create a new create app, click on create new app.

                                                                                           image

  • To verify the program. Click on verify.

                                                                                              image

  • To upload the code, click on flash but before doing that select a device.If you have more than one device you have to make sure that you have selected which of your devices to flash code to. Click on the "Devices" icon at the bottom left side of the navigation pane, then when you hover over device name the star will appear on the left. Click on it to set the device you had like to update (it won't be visible if you have only one device). Once you have selected a device, the star associated with it will turn yellow. (If you only have one device, there is no need to select it, you can continue.

 

                                                                 imageimage

 

Connections

 

Particle Photon ==> PPD42NJ sensor (placed in vertical direction)

 

GND ==> Pin1(GND)

D6 ==> Pin2 (Output)

Vin ==>Pin3(5V)

GND ==> 10k resistor ==> Pin5 (Input)

 

Particle Photon ==> RGB LED

 

D1 ==> R

D2 ==> G

D3 ==> B

GND ==> Common Cathode

 

 

 

                                                      

           image

 

 

Program

 

int SensorPin = D6;  //  reads data from the sensor
int REDled = D1; // RED
int GREENled = D2; //GREEN
int BLUEled = D3; //BLUE

unsigned long starttime;
unsigned long sampletime_ms = 30000;  //Length of sampling time before it reports. 30,000=30 sec.  You can change this
unsigned long triggerOnP2;
unsigned long triggerOffP2;
unsigned long pulseLengthP2;
unsigned long durationP2;
boolean valP2 = HIGH;
boolean triggerP2 = false;
double ratioP2 = 0;  // start the code with the ratio set to 0.  This clears any previous data
double PM25 = 0; // start the code with the PM25 set to 0.  This clears any previous data

String colour; // tells the color
String category;  // tells the category of air


//used to control the wifi if being used in an area where there is no wifi
const uint32_t msRetryTime  =   30000; // stop trying to connect to the internet after 30sec of boot up
SYSTEM_MODE(SEMI_AUTOMATIC)
SYSTEM_THREAD(ENABLED)
// end of Wifi checking

TCPClient client;

#define THINGNAME "AirQualDev" // Name you give to your device on dweet.io  Don't use spaces.


void setup()
{
  
  
  pinMode(REDled, OUTPUT);
  pinMode(GREENled, OUTPUT);
  pinMode(BLUEled, OUTPUT);
  pinMode(SensorPin,INPUT);
  starttime = millis();//millis() is the on chip timer that starts running when the program starts running.
  //Tells you how many milliseconds since the program started

   Particle.connect();  //if it can't connect to the internet in 30 seconds of booting up it will turn the Wifi off and keep running
     if (!waitFor(Particle.connected, msRetryTime))
    WiFi.off(); // if the wifi comes back it will not turn the wifi on the photon.  You must reset it to get it back on wifi.

    delay(120000); //this delays the sensor for 2 minutes while it warms up

}

void loop(){ 

      valP2 = digitalRead(SensorPin);

     if(valP2 == LOW && triggerP2 == false){
    triggerP2 = true;
    triggerOnP2 = micros();
  }

    if (valP2 == HIGH && triggerP2 == true){
      triggerOffP2 = micros();
      pulseLengthP2 = triggerOffP2 - triggerOnP2;
      durationP2 = durationP2 + pulseLengthP2;
      triggerP2 = false;
  }
    if ((millis() - starttime) > sampletime_ms) {  //if the difference between what time it is right now and when this sample started is greater than our sample time
    //than end this sample and report the data.

    ratioP2 = durationP2/(sampletime_ms*10.0);  //  percentage 0=>100   Percent of time this pin was triggered during sampling.
    //a higher ratio tells dirtier air. 

    PM25= ratioP2 * ratioP2 * .1809 + 3.8987 * ratioP2;  //This is the calibration between the ratio and PM25 in ug/m3

    //this section controls what color the LED is at on different PM25 levels.

    if (PM25 < 10)   
    {
        digitalWrite(REDled, LOW); 
        digitalWrite(GREENled, HIGH); 
        digitalWrite(BLUEled, LOW); 
        colour = "Green";
        category = "Good";
    }
    if (PM25 < 20 && PM25 > 10) 
 {
        digitalWrite(REDled, LOW); 
        digitalWrite(GREENled, HIGH); 
        digitalWrite(BLUEled, HIGH); 
        colour = "Cyan";
        category = "Satisfactory";

    }
     if (PM25 < 30 && PM25 > 20) 
 {
        digitalWrite(REDled, LOW); 
        digitalWrite(GREENled, LOW); 
        digitalWrite(BLUEled, HIGH); 
        colour = "Blue";
        category = "Moderately satisfactory";
        
    }
     if (PM25 < 40 && PM25 > 30) 
 {
        digitalWrite(REDled, HIGH);
        digitalWrite(GREENled, LOW);
        digitalWrite(BLUEled, HIGH);
        colour = "Magenta";
        category = "Poor";

    }
     if (PM25 < 100 && PM25 > 40)
 {
        digitalWrite(REDled, HIGH); 
        digitalWrite(GREENled, LOW);
        digitalWrite(BLUEled, LOW);
        colour = "Red";
        category = "Very poor";

    }
       if (PM25 > 100)  
 {
        digitalWrite(REDled, HIGH);
        digitalWrite(GREENled, HIGH);
        digitalWrite(BLUEled, HIGH);
        colour = "Black";
        category = "Severe";
        
    }


    //ends the LED control section
    
  


    
    Particle.publish("colour", String(colour));
    delay(2000);
    Particle.publish("PM25", String(PM25));
    delay(2000);
    Particle.publish("ratioP2", String(ratioP2));
    delay(2000);
    Particle.publish("category", String(category));
    delay(2000);
    // Starts the section that will publish the results to DWEET
   
    if (client.connect("dweet.io", 80))
    // Go to  http://dweet.io/follow/thingname  to see the results in your browser. change "thingname" to your thingname in the web address.
    {
      client.print("GET /dweet/for/");
      client.print(THINGNAME);
      client.print("?ratioP2=");  // Don't use spaces for data names
      client.print(ratioP2);
      client.print("&PM25=");  // Don't use spaces for data names
      client.print(PM25);
      client.println(" HTTP/1.1");
      client.println("Host: dweet.io");
      client.println("Connection: close");
      client.println();
           }
           // ends publishing to DWEET
    
  
  

   durationP2 = 0;  //resets the lowpulseoccupancy back to zero to start the next sample
      starttime = millis(); // set the start time to what time it is now.
      // go back to the top of the loop and start sampling again

}

}

 

Result

 

                                                                        

                                            image

 

                                                             

              image

 

            

                                                      

              image

 

                                                               

               image

 

                             

                  image

 

How to Make PCB in Eagle

What is PCB


PCB is a printed circuit board which electrically connects a set of electronic components by using copper tracks on a non-conductive board. In PCB, all components are connected without wires, all components are connected internally, so it will reduce the complexity of the overall circuit design.

 

Types of PCB

 

1.Single-sided PCB

2.Double-sided PCB

3. Multi-layered PCB

In this, I am only talking about Single-sided PCB

 

Single-sided PCB

A single layer PCB is also known as single-sided PCB. This type of PCB is simple and most used PCB because these PCBs are easy to design and manufacture. One side of this PCB is coated with a layer of any conducting material. Copper is used as conducting material because it has a very good conducting characteristic. A layer of solder mask is used to protect PCB against oxidation followed by silkscreen to mark out all of the components on the PCB. In this type of PCB, only one side of the PCB is used to connect different types of components.

 

Different Parts of PCB
1. Layers

Top and bottom layer: In the Top layer of PCB, all SMD components are used. Generally, this layer is Red-colored. In the bottom layer of PCB, all components are soldered through the hole and lead of components is known as the bottom layer of PCB. In this DIP components are used and the layer is blue.

            

                                                                                                                                    image

 

2. Copper tracks
It's generally a conducting path between components in the circuits for an electrical contact or a track is a conductive path that is used to connect 2 points in the PCB. For instance, connecting 2 pads or connecting a pad and a via or between vias. The tracks can have different widths depending on the currents that flow through them.

We Use Copper because it is highly conductive. This means that it can easily transmit signals without losing electricity along the way. In the most common configuration, an ounce of copper can be turned into 35 micrometres about 1.4 thousandths of an inch thick, which can cover an entire square foot of the PCB substrate.

3. Pads
A pad is a small surface of copper in a printed circuit board that allows soldering the component to the board or we can say points on the circuit board where the terminals of the components are soldered.

There are 2 types of pads; thru-hole and SMD (surface mount).

  • Thru-hole pads are intended for introducing the pins of the components, so they can be soldered from the opposite side from which the component was inserted.
  • The SMD pads are intended for surface mount devices, or in other words, for soldering the component on the same surface where it was placed.

Shapes of Pads

  1. Circular
  2. Oval
  3. Square

 

                                                                                               image

 

4. Soldermask
For mounting the electrical components on the printed circuit boards, an assembly process is required. This process can be done by hand or through specialized machinery. The assembly process requires the use of solder to place the components on the board. For avoiding or to prevent the solder to accidentally short-circuit two tracks from different nets, PCB manufacturers apply a varnish called soldermask on both surfaces of the board. The most common colour of the soldermask used in printed circuit boards is green. This insulating layer is used to prevent accidental contact of pads with other conductive material on PCB.

5. Silkscreen
Silk-screening (Overlay) is the process where the manufacturer prints information on the soldermask conducive to facilitate the processes of assembly, verification, and debugging. Generally, the silkscreen is printed for indicating test points as well as the position, orientation, and reference of the electronic components that are part of the circuit. Silkscreen can be printed on both surfaces of the board.

6. Via
A via is a plated hole that allows the current to pass through the board. It is used in the multilayer PCB to connect to more layers.

 

Types of Via

 

1. Thru-hole Vias or Full Stack Vias

When an interconnect must be made from a component that is located on the top layer of the printed circuit board with another that is located at the bottom layer. For conducting the current from the top layer to the bottom layer, a via is used for each track.

Green ==> Top and bottom soldermasks

Red ==> Top layer ( conductive )

Violet ==> Second layer. In this case, this layer is used as a power plane ( i.e. Vcc or Gnd )

Yellow ==> Third layer. In this case, this layer is used as a power plane ( i.e. Vcc or Gnd )

Blue ==> Bottom Layer ( conductive )

 

                                                                                                image

2. Blind vias
blind vias are used, which allows a connection to be made from an external layer to an internal layer with minimum via height. A blind via starts on an external layer and ends on an internal layer, that's why it has the prefix "blind". In multilayer system designs where there are many integrated circuits, power planes ( Vcc or GND) are used to avoid excessive routing for power rails.

To know if a certain via is blind, you can put the PCB against a source of light and see if you can see the light coming from the source through the via. If you can see the light, then the via is thru-hole, otherwise, the via is blind.

It is very useful to use these kinds of vias in printed circuit board design when you don't have too much space for placing components and routing. You can put components on both sides and maximize the space. If the vias were thru-hole instead of blind, there would be some extra space used by the vias on both sides.

 

                                                                                                   image

 

3. Buried Vias

These vias are similar to the blind ones, with the difference that they begin and end on an inner layer.

                                                                                               image

7. ERC
After creating the schematic and annotating circuit, it is necessary to check whether the circuit has any electrical errors such as, if Nets are not connected properly, the input is not connected to the input pin, Vcc and GND shorted anywhere in the circuit, or any pin electrical type not selected properly, etc. All these are electrical error types. If we have made any such mistake in the schematic, and if we are not performing any ERC, then after completing the PCB we cannot get the desired result from the circuit.

ERC Detail

8. Design rule check
DRC Detail

How to make PCB in Eagle

 

Make a schematic diagram

 

To make a schematic go to File ==> new ==> Schematic You will see a page like this

 

                                                                                              

 

As there are no Particle parts so we have to add Particle devices libraries.

particle lib

 

Next, after downloading it move it to the folder C:\Users\.....\Documents\EAGLE\libraries

 

                                                                                              image

 

In Eagle open Schematics go to Library ==> open library manager

 

                                                                                               image

 

you will see a page like this, go to option Available and browse to the library particledevices.lbr

 

                                                                                               image

 

After opening it click on use

                                                                      image

Now, we can see particle devices.

Next step is to make a schematic for that we use add part as shown in figure

 

                                                                                                                                  image

 

When you click on add part you will see a page like this

 

                                                                                          image

 

The components we needed are Particle photon, headers, resistors, GND, Vcc. Search components in add parts

  • For a resistor, there are two types US and EU. Here I am using a European one
  • For header search header and you will see lots of headers choose according to yours.
  • For ground search gnd
  • For VCC search vcc
  • For Particle Photon search it

Once components are selected next step is to join it together for that you can use line or nets or both.

 

                                                                                                                 imageimage

 

Join it as shown in the image below

                                             image

 

Next step is giving name and value.

                                                                                                                            imageimage

 

For giving names select name and then click on the component to which you wanna give a name.

For giving values select value and then click on the component to which we want to give a name.

 

After that check ERC

                                                                                                                                                        image

 

Once checked we are done with Schematic. Next step is to switch to boards from schematics

 

                                                                                                                                          imageimage

 

After that assemble all the components as per your convenience. For joining the components use route airwire make sure you will use the bottom layer, the grid will be in mm and route airwire width 0.4064

                          imageimageimageimage

 

After joining all the components Use mirror tool to generate an image of values and names.

                                                                                                                                                 image

 

                                                                                          image

 

For using mirror first select mirror tool and then values, names.
Next, save the board with any name, check DRC to check errors. If no error we are good to go ahead.

To see a preview of the board go to manufacturing.

 

                                          imageimage

 

Now we are done with the board part.

Next step is to print the ckt on glossy paper. For that click on print, you will see a page as shown below.

 

                                                                                                    image

 

  • Select black in option, if you are using multiple layers then you also have to select mirror.
  • Select scale factor 1.042 After that save it to pdf or print it.

 

After printing the ckt,

 

1. Remove the oxidation layer from FR4 sheet using sandpaper (400) use a light hand.

                                                                                                    image

 

2. Clean it using isopropanol or propan-2-ol or if you want you can use thinner also.

3. Place the printed ckt on FR4 sheet using paper tape.

4. Heat it using heating iron (5 -10 minutes) so that ckt will print on FR4 sheet. Soak board in water for 2-3 minutes. After that remove the tape and paper.

 

                                                                                                    image

 

5. Place it in ferric chloride solution for 10 minutes to remove access copper then wash it with water.

                                      imageimage

 

6. Remove the layer using sandpaper(400) or Acetone.

 

                                                                                                         image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 6 years ago +1
    Nice project. DAB
  • ruchir1674
    ruchir1674 over 6 years ago in reply to aswinvenu +1
    Thanks Aswin !!!!
  • ruchir1674
    ruchir1674 over 6 years ago in reply to dubbie +1
    Thanks for the comment DAB. yeah it is cheap. I have not tried it much so can't say about it. I tried it indoor. I will share it soon.
Parents
  • dubbie
    dubbie over 6 years ago

    A comprehensive, impressive and interesting project. I was not aware of this type of sensor before and it seems so low cost. Does it have any limit on how long it will operate before needing replacement or does it last forever.

     

    Did you try this indoors or outdoors? It would be interesting to see some more results.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago

    A comprehensive, impressive and interesting project. I was not aware of this type of sensor before and it seems so low cost. Does it have any limit on how long it will operate before needing replacement or does it last forever.

     

    Did you try this indoors or outdoors? It would be interesting to see some more results.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ruchir1674
    ruchir1674 over 6 years ago in reply to dubbie

    Thanks for the comment DAB. yeah it is cheap. I have not tried it much  so can't say about it. I tried it indoor. I will share it soon.
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.