RF Radio Frequency
  • Challenges & Projects
  • Project14
  • RF Radio Frequency
  • More
  • Cancel
RF Radio Frequency
Forum Question on Harmonics and Filters
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RF Radio Frequency to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 17 subscribers
  • Views 1729 views
  • Users 0 members are here
  • harmonics
  • rf
  • filters
  • rasperry pi
Related

Question on Harmonics and Filters

kmikemoo
kmikemoo over 6 years ago

A discussion going on about filters at Episode 355: Raspberry Pi Pirate Radio has me wondering.  I have always thought about harmonics (and the need to filter them out) as things that happen above the base frequency; 3rd, 5th, 9th, etc.  Is there such a thing as sub-harmonics?

 

If my primary issue is harmonics (bit banged Raspberry Pi RF output), why go for a bandpass filter over a lowpass filter?     Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +3 suggested
    Hi Mike, I may not have understood the use-case (I didn't follow it entirely). As I understood, the Pi was generating something at some low-ish frequency (e.g. 10 MHz) and a harmonic of that (i.e. an exact…
  • fmilburn
    fmilburn over 6 years ago +3 suggested
    Good question Mike. I had the same thought to be honest but did not pursue it. I found this post from the Imperial College Robotics Society (unrelated fact: I used to walk by Imperial College on my way…
  • shabaz
    shabaz over 6 years ago in reply to fmilburn +3 verified
    Ahh interesting! In that case Mike your're certainly right, a low-pass is all that's needed. Sorry, I should have looked into it before I assumed wrong that it was being generated at some lower freq :…
Parents
  • fmilburn
    0 fmilburn over 6 years ago

    Good question Mike.  I had the same thought to be honest but did not pursue it.  I found this post from the Imperial College Robotics Society (unrelated fact: I used to walk by Imperial College on my way to work when I lived in London)  which developed the method:  Turning the Raspberry Pi Into an FM Transmitter - Imperial College Robotics Society .  They have since made it stereo!  From their posting...

     

    it sets the clock generator module to enabled and sets it to output on GPIO4 (no other accessible pins can be used). It also sets the frequency to 100.0Mhz (provided from PLLD@500Mhz, divided by 5), which provides a carrier. At this point, radios will stop making a "fuzz" noise, and become silent.  Modulation is done by adjusting the frequency using the fractional divider between 100.025Mhz and 99.975Mhz, which makes the audio signal.

    There might be lower frequency noise from elsewhere picked up and present in the signal as well but I have no real idea.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 6 years ago in reply to fmilburn

    fmilburn Thanks for the link.  It was extremely helpful.  It gives me hope that it will work on slightly higher frequencies - like 146MHz.  We'll see... once the new RPi3 comes in.  I managed to kill mine over the weekend.  Not sure how but all I get is the lightning bolt of death.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kmikemoo
    0 kmikemoo over 6 years ago in reply to fmilburn

    fmilburn Thanks for the link.  It was extremely helpful.  It gives me hope that it will work on slightly higher frequencies - like 146MHz.  We'll see... once the new RPi3 comes in.  I managed to kill mine over the weekend.  Not sure how but all I get is the lightning bolt of death.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data