So I picked my laptop up today to use it as per normal (I rarely use it I admit) and well turns out it will not turn on, the battery is not charging and I have to repair it. I of course as per usual cannot find any schematics for this laptop it is to an extent ancient so I figured by now some schematics would show up since I cannot find any I was wondering if you guys have free schematics for an HP Envy 3D (17).
I mean I could probably work it out after a long period of time but I figured I would try to figure it out before I dive in narrow it down etc. I have a feeling it is a surface mount component since I hear something rattling around and well I have no magnifying device they all ran away at the same time not even kidding (I had two head ones and a regular magnifying glass lying around when I need one they all were gone). I know that I may very well can just figure out where a surface mount component goes and figure it out but this is not my first rodeo I know in the future other things will go wrong as well.
Also is there just normal surface mount resistors etc buyable online?