Tech Connection
  • Learn
  • Learning Center
  • Tech Connection
  • More
  • Cancel
Tech Connection
Polls Poll: Internal or Independent Data Logger: What's Your Preferred Choice for Sterilization Autoclaves?
  • Blog
  • Forum
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Tech Connection requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 5 Jun 2020 9:03 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:59 PM
  • Views 74 views
  • Likes 1 like
  • Comments 3 comments
Related
Recommended

Poll: Internal or Independent Data Logger: What's Your Preferred Choice for Sterilization Autoclaves?

Sterilization autoclaves use steam sterilization to expose each item being sterilized to direct steam contact at the required temperature and pressure for the specified time. Since autoclaves work in cycles, they need to be validated to ensure that the sterilization has been effective, so the temperature and pressure should be monitored and logged.

 

Because sterilization requires high temperatures and high pressure, it can be a challenging environment for electronics. Most regular data loggers cannot withstand more than about 80°C for short periods of time. However, to eliminate any microbicidal activity and ensure sterilization, steam sterilization temperatures should be within a 121°C (250°F) and 132°C (270°F) range.

 

There are two options for logging temperature and pressure data at these temperatures.

 

  • The first option is to build the data logger into the autoclave. This option is the most inexpensive solution because everything is integrated. However, it can be hard to tell if the data logger is malfunctioning and improperly sterilized loads could occur.

 

  • The second option is to use an independent data logger. The benefit is that it’s simple to use and because it is independent of the autoclave system, it’s much easier to determine if it’s operating correctly or not. The downside is that this is a more expensive solution.

 

 

Poll Question: What is your preferred choice for a data logger for a sterilization autoclave: built-in internal or independent.

  • datalogging for sterliization applications
  • tech spotlight
  • omega
  • community survey
  • omega engineering
  • Share
  • History
  • More
  • Cancel
Anonymous

Top Comments

  • kmikemoo
    kmikemoo over 1 year ago +2

    Interesting question.  I'm going with internal as I don't believe that one will be more reliable than the other.  There has to be a current procedure to calibrate/validate these.  After all, it's…

  • rsc
    rsc over 1 year ago +2

    Most of our Autoclaves are simple with no data logging.  They have a thermocouple or RTV temperature probe and gage, pressure transducer with display, a timer of some sort, and a safety interlock on the…

  • BigG
    BigG over 1 year ago +1

    IMHO, you start with the data requirements. How much data are you needing to collect in total before downloaded/removed (storage capacity), how much data is needed to be captured concurrently (bandwidth…

  • BigG
    BigG over 1 year ago

    IMHO, you start with the data requirements. How much data are you needing to collect in total before downloaded/removed (storage capacity), how much data is needed to be captured concurrently (bandwidth), how often (frequency) and over what continuous period (resilience/reliability). Then comes the technical/commercial evaluation... so can't really answer the question without making assumptions.

    • Cancel
    • Up +1 Down
    • Reply
    • More
    • Cancel
  • rsc
    rsc over 1 year ago

    Most of our Autoclaves are simple with no data logging.  They have a thermocouple or RTV temperature probe and gage, pressure transducer with display, a timer of some sort, and a safety interlock on the door to make sure temperature and pressure are at safe levels to open the unit.  Most have an emergency manual steam release valve.  Some have outputs from the displays for data logging.

    • Cancel
    • Up +2 Down
    • Reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 1 year ago

    Interesting question.  I'm going with internal as I don't believe that one will be more reliable than the other.  There has to be a current procedure to calibrate/validate these.  After all, it's medical equipment.  Every so often, you check it against an external device and rock on.  My opinion.

    • Cancel
    • Up +2 Down
    • Reply