Publications
  • Learn
  • More
Publications
Blog Robotic 3D printer concept aims to create architecture out of soil
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 10 Aug 2012 6:24 PM Date Created
  • Views 1028 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • test
  • transportation
  • robotics
  • robot
  • on_campus
  • Design
  • 3d_printing
  • cabeatwell
  • 3d_printer
  • prototyping
  • concept
  • university
  • Architecture
  • innovation
  • communication
Related
Recommended

Robotic 3D printer concept aims to create architecture out of soil

Catwell
Catwell
10 Aug 2012

image

Stone Spray concept image. (via Institute for Advanced Architecture of Catalonia)

 

We have seen the good and the bad of 3D printer's influence on the world. Still fledgling in maturity, the devices are limited when it comes to the materials it can use to create objects. It is also limited in that it can only print in one direction (usually up) and do it in a confined area, which incidentally, limits the size of the object being created.

 

Architects Petr Novikov, Inder Shergill, and Anna Kulik, from the Institute for Advanced Architecture of Catalonia, have adapted 3D printing technology to design structures that are clearly constructed ‘outside the box’ (pun intended). The team's research project, known as Stone Spray, is a robotic 3D printer that is capable (albeit limited) of creating 3D structures using onsite natural soil and sand. Their robotic 3D printer design features an arm that is equipped with 3 lower joints equipped with stepper motors, enhanced (for workloads) with a gear transmission system, along with 2 other joints that use servomotors which give the arm 5-DOF of movement. The motors are controlled by an Arduino UNO unit along with three Easydriver shields (which can drive 7V-30V bipolar 2-phase magnetic-stepping motors). The system uses two tanks, one for the soil and the other for a binding agent, that send the material through 2 plastic tubes to the arms nozzle that is equipped with a distance sensor. The sensor determines the correct distance needed for the printing applications design specifications. The software that robotic printer uses was designed with the open-sourced Processing language and features a ‘manual mode’ (for pre-positioning of the nozzle) along with an ‘automatic mode’ that can print designs based off of G-code text files.

 

So far, the Stone Spray 3D printer is capable of small rudimentary designs, such as columns, that are constructed using an internal wire frame. Further development of the printer could see it capable of actually building larger structures (such as bridges and canopies) without the need for a frame in the not too distant future.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • DAB
    DAB over 13 years ago

    This application is more to what I envisioned for 3D printing.

    You send in a bunch of these with robotic control and they use the natural elements to construct shelters and infrastructure ready for human habitation. 

     

    Just think about what a thousand of these could do in a desert area.  They could quickly cover the loose sand with small structures to trap the sand and channel any rainfall such that it does not erode the surface.  In no time at all, you could convert large areas to a stable ground from which to build structures.

     

    Have them build green houses on the desert and you could quickly increase the area of arable land by significant amounts.  The boon to the population would be huge.  You could have the 3D robots build water storage tanks, solar cells, and waste recycling pits very quickly.

     

    Hopefully, the research and development of these devices will move quickly into implementation.

     

    DAB