<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/"><channel><title>need help</title><link>/members-area/b/blog/posts/need-help</link><description>dear engineers,
I am a 15-year-old starting out with PCB design. I recently designed a continuity tester circuit to check if a wire is properly connected or two pieces of wire are properly connected together. I built the circuit using an A1357 PNP tr</description><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>RE: need help</title><link>https://community.element14.com/members-area/b/blog/posts/need-help</link><pubDate>Sun, 15 Nov 2026 20:06:23 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:09015363-2991-49b9-a0ee-c9b94e7e46f4</guid><dc:creator>shabaz</dc:creator><slash:comments>1</slash:comments><description>&lt;p&gt;Hi,&lt;/p&gt;
&lt;p&gt;That circuit is not convenient to follow, there are at conventions for drawing circuits:&lt;/p&gt;
&lt;p&gt;(1) High voltage at the top, low voltage at the bottom&lt;/p&gt;
&lt;p&gt;(2) Inputs on left, outputs on right.&lt;/p&gt;
&lt;p&gt;The circuit here may work (you may still need to tweak it, but it will provide you with results you can move forward with so I&amp;#39;d strongly suggest just restarting and putting your current circuit to one side, maybe desolder the parts and reuse.&lt;/p&gt;
&lt;p&gt;&lt;img alt=" " height="475" src="/resized-image/__size/1612x950/__key/commentfiles/f7d226abd59f475c9d224a79e3f0ec07-09015363-2991-49b9-a0ee-c9b94e7e46f4/cont_5F00_cct.png" width="806" /&gt;&lt;/p&gt;
&lt;p&gt;Better to test without the buzzer, just the LED, and then add the buzzer once you have confirmed it works with the LED.&lt;/p&gt;
&lt;p&gt;You mention you forgot the LED resistor, but it&amp;#39;s essential, you won&amp;#39;t get expected results if it is missing.&lt;/p&gt;
&lt;p&gt;The values you can adjust, if you don&amp;#39;t have the same values as the ones in the diagram. For example, R1 can be anything between 470 ohm and 10 kohm. R2 can be from 47 kohm to 470 kohm. R3 can be from 1 kohm to 10 kohm.&lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=30417&amp;AppID=75&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item></channel></rss>