Member's Forum eZ8 minimal configuration
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 583 subscribers
  • Views 458 views
  • Users 0 members are here
Related

eZ8 minimal configuration

Former Member
Former Member over 11 years ago

Hi,

 

I'm trying to get an eZ8 microcontroller running with the minimal configuration necessary to communicate with the on-chip debugger.  Currently I'm using a Parallax Propeller QuickStart board in my attempt, mainly because the operating voltages of the Propeller and the eZ8 match.  I have not had any luck so far.  I'm doing this purely out of curiosity and an interest in learning how these things work.  It seems like a fairly basic task

 

Initially, I was trying to use a square wave output generated by the Propeller as a clock input to the eZ8, but have since connected an 18.432MHz crystal as shown on page 217 of the eZ8 manual.  I have full-duplex serial communication set up on the Propeller, which I have connected to the eZ8's DBG pin, as shown on page 204 of the eZ8 manual.  I have kept the baud rate relatively low, in the 75-150 range.  I have also connected the eZ8's reset pin to a pin of the Propeller so that I can reset it as needed, and I've connected all of the VDD and VSS pins of the eZ8 (6 total) to the appropriate connections; all of this is on a solderless breadboard.  All of the other pins have been left unconnected.

 

I am trying to send the 0x80 required to initialize the AutoBaud detector (p. 206, eZ8 manual), followed by various read commands (p. 209, eZ8 manual), checking for a response after each.  I am getting no responses.  I believe that the serial library is working on the Propeller side because when I turn off the library's FDSERIAL_MODE_IGNORE_TX_ECHO flag, I can see the commands that I've sent via the transmit pin being returned via the receive pin.

 

So, my questions:

Did I miss something?  Is more than clock/reset/VSS/VDD required to get the eZ8 running?

It would be helpful if I could separate the minimal configuration problem from the serial communication problem. Is there a way to tell that the eZ8 is in fact running that is less complicated than attempting to communicate with the on-chip debugger?

Any additional thoughts are welcome..
Here's the eZ8 manual: http://www.zilog.com/docs/z8encore/PS0199.pdf