This is a quick blog post about using my NooElec SDR for the first time.
Back last year I was luckily chosen to roadtest three Molex Antennas Molex 2.4GHz / 5GHz Antenna Kit - Review and that re-kindled my interest in RF work at home. Wanted to have a 'play around' I bought myself a low-cost SDR for fun and it arrived today. It cost me just over £20 (UK) and plugs into the USB port of my computer plus it has a SMA connector for the antenna. I actually made a misjudgment and bought the basic unit before realising I didn't really have the bits to make a decent antenna but I have many plans to address that.
I initially ran this on my Linux machine - having downloaded the drivers and installed rtl-sdr and another package called Gqrx. That all ran really well and with a basic wire antenna I was able to tune to local FM radio stations and hear the music etc.
I then tried using the SDR with my Windows 10 laptop and installed the software described on the NooElec website called CubeSDR. That too was fun and I was able to scan the airwaves - looking at the signals in the frequency domain. The Digital Audio Broadcast (DAB) band looked particularly regimented - as shown below:
That was all fun but the SDR was being configured using the software and I had also read an article that mentioned I could make my own designs using the GNU Radio software.
I downloaded and installed that from their website and was met with a very interesting window....it then dawned on me how great this software was. I was going to be able to draw out the various block parts of my receiver to do exactly as I wanted. As a newbie I was going to struggle and so followed a useful online article https://www.instructables.com/id/RTL-SDR-FM-radio-receiver-with-GNU-Radio-Companion/ and, after some tweaks, I ended up with this:
And even using an out-of-band antenna (the Molex 433MHz from my kit) I was able to demodulate and hear a local radio station on my PC's speakers
All I can say is, I'm now hooked. I need a decent outside antenna (or two ) and a few connectors /cable length.
Browsing around at what I can pick up threw up some interesting links; apparently I can even receive the meteorological photos from an orbiting weather satellite. This needs a bespoke antenna but the design looks quite simple.
Rod
Top Comments
I've played a bit with it... Its fun stuff... With the right antennas and equipment you can get weather sat images. There are many interesting things that are being transmited in air waves. For instance…
Hi Rod,
Great idea! Looking forward to seeing it.
By coincidence I started some work on an RF amp recently, although it's hard finding time to finish.. It is to be a 1W amp, intended for transmit. I've only…
Hi Rod,
Great to see your radio experiments!
It is really addictive, and so much to explore - I can see why radio hams enjoy their hobby.