After having had a horrendous time fighting through the traffic into the office in Leeds today, I was greeted by a lovely surprise from our friend John Alexander at the Shropshire Linux User Group (SLUG for short). It was a reasonable sized jiffy bag with two Perspex cases for the Raspberry Pi. One in bright Orange (I wasn't a fan of this colour to start with but I've grown to like it after having it on my desk for the morning) and a rather nice blue one.
To be honest I turned into a big kid on Christmas morning and instantly opened the orange one and had my Raspberry Pi safely inside in under 3 minutes, it was so easy to put together and keeps the Pi save and sound.
After the excitement I has feeling a bit creative, so I put together this animated GIF of the case being built.
Edit: It is an animated GIF honest but you will need to click the image to open the full sized image in a lightbox
I've only 1 Raspberry Pi, so I've got the blue one spare, if anyone fancies owning one of these feel free to drop me a comment below
Please note: I only have ONE so apologies if you are disappointed