Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Filter Coefficient Translator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dhmarinov
  • Date Created: 23 Aug 2019 4:52 PM Date Created
  • Views 2158 views
  • Likes 7 likes
  • Comments 8 comments
  • 2's complement
  • fixed point
  • c
  • fir
  • vhdl
  • translator
  • matlab
  • coefficients
  • floating point
  • filters
  • iir
Related
Recommended

Filter Coefficient Translator

dhmarinov
dhmarinov
23 Aug 2019

Hello there,

 

Lately I have been working a lot with filter design and implementation on FPGA.

As you know the most common way to design a filter is through MATLAB or a suite with the similar capabilities.

Either way the produced result is an array of floating point values. FDAtool has the ability to translate the values from decimal

to binary floating point, however, if the implementation is in fixed point, then this functionality is useless.

In order to make use of the coefficients, they have to be represented as 2's complement.

At first I used to translate each value by making use of the online decimal-to-2's complement converters, but as you can imagine

this can get quite tedious. To combat this problem I developed a simple Python program, which does the whole work (almost) in a click of a button.

 

image

 

The concept is quite simple:

 

1.Browse to the filter coefficient file (.fcf) or any other file containing decimal values that range between 0.999 and -0.999.

There has to be only one value per row!

 

2. Chose the desire structure of the output file.

2.1 Array will return the data enclosed in a VHDL, Verilog or C array. The options to select the language are available only for the array option.

2.2 List will return a list of values. Chosing this option gives the user the opportunity to enter a separator between the values.

 

3. There are 4 possible output formats - binary, hexadecimal, signed and unsigned integer.

All of them represent the equivalent of the 2's complement value.

 

4. Elements per line determines how many values are ther per row in the output file.

 

5. Output bit width determines the desired bit length of the output product.

If the selected format is hexadecimal and the selected bit width is not multiple of 4, then the output width will be extended to the next value multiple of 4.

 

6. File extention sets the type of the output file - typical choice is text (txt), however, by using a data format (data), the user can

create a list of values that can be used to initialize block RAMs in Vivado.

 

7. The Translate button creates the output product.

 

8. The console in the bottom displays various information such as data that has been rejected by the translator in the form of warnings,

tips about the input file, and errors.  

 

Done!

 

Here is a video demonstarion:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

You can it from my Github.

Enjoy image

 

PS: A small update on 26.09.2019 was done on the Git repository - all files except the source code and the application were removed.

  • Sign in to reply

Top Comments

  • dhmarinov
    dhmarinov over 6 years ago in reply to clem57 +2
    Sorry it was in private mode. Can you try again? https://github.com/DHMarinov/Coefficient_Translator
  • dhmarinov
    dhmarinov over 6 years ago in reply to genebren +1
    Sounds cool, but didn't that have an influence on the frequency response , or it was insignificant?
Parents
  • genebren
    genebren over 6 years ago

    Interesting tool.  I have created Excel worksheets to do something similar.  In my case, I just wanted to simplify the math (signed fixed point) where all of the coefficients were whole numbers and the result was divided by a power of two (actual shifted) so the math was fast enough for even a small microprocessor.

     

    Thanks for sharing,

    Gene 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dhmarinov
    dhmarinov over 6 years ago in reply to genebren

    Sounds cool, but didn't that have an influence on the frequency response , or it was insignificant?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dhmarinov
    dhmarinov over 6 years ago in reply to genebren

    Sounds cool, but didn't that have an influence on the frequency response , or it was insignificant?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • genebren
    genebren over 6 years ago in reply to dhmarinov

    The goal is to minimize the effects by choosing integer coefficients and divisor (or shift) that produces the minimal error.  It most cases, the filters have been a close fit to the desired characteristics.