Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs MLCC Shortage: When You Can’t Find The Cap You Need
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: nikhilstephen
  • Date Created: 2 Aug 2018 9:03 PM Date Created
  • Views 615 views
  • Likes 4 likes
  • Comments 3 comments
  • polymer capacitors
  • kemet
  • power electronics
  • electronics.
  • ceramic capacitors
Related
Recommended

MLCC Shortage: When You Can’t Find The Cap You Need

nikhilstephen
nikhilstephen
2 Aug 2018

image

It is 2018 and you’re probably reading this because you’re wondering when you’re gonna get your order of MLCCs. Either that or you’ve used some four-letter word to describe the lead times at your favorite distributor. Yes, the MLCCs industry is experiencing quite the capacity crunch. The last time it was like this we were back in the.COM days of ’99-2000. Manufacturers are putting in capacity, but that will take some time to come up. I know that’s cold comfort for the engineers who are dealing with a line down situations, and the supply chain managers who are having to beg, borrow and steal parts. It is times like this that make engineers explore new options and alternative techniques without having to do a massive redesign. Our polymer electrolytic capacitors are one type of alternative that, given certain conditions, can help. Going to KO-CAP isn’t always trivial, but if certain things align, they can be of great relief.

A Primer On KO-CAPs

Let’s all get to the same baseline. KO-CAP is KEMET’s tantalum-based polymer electrolytic capacitor. Like any other tantalum capacitor, it is a slug of sintered tantalum powder that has a tantalum pentoxide layer grown on it, with a layer of conductive polymer acting as the cathode. This conductive polymer gives the capacitor much lower ESR than “traditional” tantalum capacitors. That’s all I have to say about that. If you want to know more about KO-CAP, click here.

MLCC to KO-CAP

I am not delusional, I was (am) an engineer too and selling me on tantalum when I’m looking for MLCCs isn’t exactly the way to my heart. But, as engineers, solving problems is what we do and that means doing things we haven’t previously considered. As with anything else in engineering, making the decision to go to KO-CAP from MLCC is just a matter of managing tradeoffs. There is a slew of things that must be considered when making that decision. The critical design parameters that must be considered when attempting to make the change are; capacitance, voltage, ESR, frequency, leakage current, size, and qualifications. The flow chart below serves as a guide to making that decision when considering each of those critical design parameters. We are going to look at it from the standpoint that you’re trying your best to get as close as possible to the characteristics of your ceramic capacitor.

image

Capacitance

KO-CAPs tend to have more capacitance than a similarly sized ceramic capacitor. They don’t come in values smaller than 680nF. So, if your total capacitance is less than that, KO-CAP is not a suitable option. When it comes to capacitance, it is usually a very strong value proposition to replace a bank of MLCCs with one or two KO-CAPs.

Voltage

In KO-CAP or any tantalum-based capacitor for that matter, the dielectric layer is very thin. A typical value is about 20nm. Having such a thin dielectric gives you a large amount of capacitance, but it also has the effect of limiting your voltage. A “high voltage” KO-CAP would be anything more than 35V. In general, if your operating voltage is more than 50V, KO-CAP is not a suitable option.

ESR

Ceramic capacitors, in a general sense, have lower ESR than an equivalent KO-CAP counterpart. That is not to say that there aren’t some very low ESR KO-CAPs. Some even go as low as 8mΩ, but a typical cutoff of 10mΩ is adequate. If you need ESR less than that, then KO-CAPs may not be a suitable option.

Frequency

What you have to watch out for when considering frequency characteristics of KO-CAP is the self-resonant frequency. You generally want to operate capacitors below this point. It isn’t always the case, but if your switching frequency goes beyond 1MHz, then you may be approaching the limits.

Reverse Bias

KO-CAPs are polar devices, as such, they can not take reverse bias voltage. If the capacitor is placed in a location in which reverse bias is possible or needs to be tolerated, KO-CAPs are not suitable.

A Replacement-Example

Alright, we have our guidelines, so what do we do now? What does this all mean? Let’s take a look at an example using a TI TSP54560B-Q1, that’s a buck for automotive applications.

image

I am an engineer and I have this circuit designed and everything is great. Until my sourcing person tells me that they can’t find some of the MLCCs I need. After berating them for a little while, I decide it is time to get creative and find a solution. Using the replacement guidelines I come to the conclusions below.

Input Side

C1, C2, C3, and C10 are my input side capacitors. They are 2.2uF 50V 1206 X7Rs. There isn’t a drop-in replacement for the ceramics, but I can take the total 8.8uF capacitance and replace the 4 ceramics with one 10uF 35V KO-CAP. It is more than the original capacitance we need, but it is still within the required range for this regulator. ESR, Leakage, and frequency are not of concern on the input side, as long as the input isn’t direct battery voltage. Our simulation tool, K-SIM, show their side by side comparison.

image

Yes, I hear your concern, “what’s this going to cost me?” Well, let’s do the math. The total cost of the 4 MLCCs is $4.16. Replacing those 4 with one KO-CAP save about a bit over a dollar.

image

Output Side

On the output side we have C6, C7, C9, and C11; 22uF 10V X7R 1206s. In this case, we are lucky, there is a drop-in replacement of that in KO-CAP. It is 6.3V but more than the output voltage range. In this case the KO-CAP ESR is higher than the ceramic equivalents, but still within the design spec. The switching frequency of the circuit is 300kHz and the SRF of my replacement is around 1MHz, so I am good there.Money-wise, we have a similar story on the output side. That MLCC is nearly $2! Yeah, I know it is a very expensive cap, but you can’t even get it anyway, so it is a moot point. The KO-CAP replacement is just over a dollar. Saving you a whopping 45%.image

image

Other Capacitors and Considerations

C4, C5, and C8 are other caps that support the functionality of the device. There are suitable candidates for substitution because of both their physical size and capacitance value. Caps of this type are not experiencing quite the same capacity crunch. I didn’t mention leakage current very much because, in truth, that is only a concern in systems that have fixed non-rechargeable batteries.

MLCC Substitution Conclusions

Finding a drop-in replacement is doable but it isn’t the same level of the value proposition as replacing a bank of capacitors with a much lower quantity of KO-CAPs. Sometime a substitution won’t be feasible, but during times of capacity crunches such as this, finding solutions through other avenues could make you the hero your project deserves. Remember to contact your local KEMET FAE or head over to our Ask an FAE page if you’re considering options but need some help.

 

 

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 7 years ago +2
    This is a great way to get engineers to think outside the box and consider your product. I enjoyed the background information too. John
  • shabaz
    shabaz over 7 years ago +1
    Very useful blog post! Quite astonishing how hard it's getting to obtain MLCC in a short timeframe..
  • shabaz
    shabaz over 7 years ago +1
    It's so extreme right now, I'm having difficulty finding small quantities of RF ceramic caps too : ( I had to order a small quantity from overseas, just three values in a qty of 10, and a few minor other…
Parents
  • shabaz
    shabaz over 7 years ago

    It's so extreme right now, I'm having difficulty finding small quantities of RF ceramic caps too : (

    I had to order a small quantity from overseas, just three values in a qty of 10, and a few minor other passives (less than a dozen resistors), for £100GBP : ( And I had to guess those capacitor values, since I want to try them out in a circuit to see what works.So I have three attempts : ) A fourth guess would have been nice, but at approx £25 a guess it's pretty bad.. The current market situation is awful for designing stuff : (

     

    Also I'm going to have to be super-careful with the tweezers.. can't risk more than a few caps to be mishandled and go pinging through the air : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 7 years ago

    It's so extreme right now, I'm having difficulty finding small quantities of RF ceramic caps too : (

    I had to order a small quantity from overseas, just three values in a qty of 10, and a few minor other passives (less than a dozen resistors), for £100GBP : ( And I had to guess those capacitor values, since I want to try them out in a circuit to see what works.So I have three attempts : ) A fourth guess would have been nice, but at approx £25 a guess it's pretty bad.. The current market situation is awful for designing stuff : (

     

    Also I'm going to have to be super-careful with the tweezers.. can't risk more than a few caps to be mishandled and go pinging through the air : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data