Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Talking BLE with the TI SensorTag CC2650 and the Cypress CySmart USB Dongle
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 17 Apr 2015 3:55 PM Date Created
  • Views 3567 views
  • Likes 2 likes
  • Comments 7 comments
  • bluetooth
  • ble
  • sensortag
  • pioneer_kit
  • bluetooth_low_energy
  • texas_instruments
  • proc
  • iot
  • simplelink
  • cypress
  • cc2650
Related
Recommended

Talking BLE with the TI SensorTag CC2650 and the Cypress CySmart USB Dongle

Jan Cumps
Jan Cumps
17 Apr 2015

I have a new The specified item was not found. CC2650 SensorTag.

element14 is running a roadtest on that soon: TI CC2650STK SimpleLinkTm IoT SensorTag.

 

image

 

I have made a test setup to connect it with the BLE dongle of the Cypress Bluetooth Low Energy PIONEER Kit..

 

That works very well. The SensorTag broadcasts itself when you push the small button on the left side (if you hold it like I show on the photo above).

You can then pair it with the Cypress SySMART USB dongle using the CySmart software.

 

Starting up the CySmart USB Dongle and Pairing the Devices

 

The USB dongle is a Programmable BLE radio on chip (PRoC) on its own. It comes with a software tool called CySmart.

This tool allows you to let the dongle scan for BLE devices, connect to them and run a conversation.

 

And that's what we're doing here.

Once you are in CySmart and you've connected to the dongle, you can press the scan button.

That's the right time to press the small button on the left side of the SensorTag.

A green light on the SensorTag goes flashing, and the dongle finds your device:

 

image

 

The info you see in the screen capture is that what the SensorTag is publicly broadcasting. Once you connect the two up, you can engage in conversation and get at the BLE characteristics.

 

The Meta Characteristics

 

The first thing you can look at is the metadata that's available via Bluetooth.

There are a number of readable characteristics that tell us more about the device.

 

imageimage

 

Apart from the manufacturer name and firmware version, there's others (Model Number, Device Name, ...).

 

Getting Push Button Notifications

 

It's possible to subscribe to events. There is a button on the right side of the device that can send BLE notifications when pressed and released.

image

By default, the notifications are inactive. You can activate them by writing a '1' to a characteristic:

 

image

Once you press the Write Value button, the message is sent to the SensorKit. It will start sending notifications:

 

[15:03:11:412] : 'Characteristic Value Notification' event received
[15:03:11:412] :    Attribute Handle: 0x0049
[15:03:11:412] :    Value: [01]
[15:03:12:847] : 'Characteristic Value Notification' event received
[15:03:12:847] :    Attribute Handle: 0x0049
[15:03:12:847] :    Value: [00]

 

In the log above, you see one push and one release notification arriving back from the SensorTag to the dongle. The attribute value is [01]for push down, and [00]for released button.

In CySmart, you get these events in the console, and the atrtributes are updated real time too.

The following pictures show the capture of the two events above:

 

image

 

I haven't shown any of the 10 sensors embedded in the SensorTag at this point, but we've seen what the BLE traffic looks like.

If you subscribe to the TI CC2650STK SimpleLinkTm IoT SensorTag roadtrest, good luck to you!

 

Related Posts
TI SensorTag CC2650 as BLE sniffer - talk to Cypress PSoC
  • Sign in to reply

Top Comments

  • clem57
    clem57 over 11 years ago +1
    Wow. Fantastic use of BLE and sensor tags. What do you think of Cypress kit? Jan Cumps Thanks for the heads up, Clem
  • DAB
    DAB over 11 years ago +1
    Nice post. I am looking forward to the webinar. DAB
  • clem57
    clem57 over 11 years ago in reply to DAB +1
    Coming this week on Wed webinar.
  • Jan Cumps
    Jan Cumps over 10 years ago

    I've done the inverse too: use the SensorTag to sniff Cypress PSoC4 and PRoC BLE traffic:

    TI SensorTag CC2650 as BLE sniffer - talk to Cypress PSoC

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to Jan Cumps

    I have put in what I think is a good idea. Wish me good fortune. I plan on using a BBB and this kit to debug the interface...

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to clem57

    I hope that the webinar and road test are a starting point for some nice ideas.

    The suitcase-like form factor may be an inspiration for what you can build with the kit.

    Now that the debugger is added to the road test package, it's possible to change the Tag's firmware. You could turn it into a spy mini-suitcase if you know how to address the microphone...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to DAB

    Coming this week on Wed webinar.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    Nice post.

     

    I am looking forward to the webinar.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>