<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/"><channel><title>Thoughts on Scaling and Biasing an ADC Input Signal</title><link>/members-area/personalblogs/b/blog/posts/thoughts-on-scaling-and-biasing-an-adc-input-signal</link><description>I&amp;#39;ve been spending some time thinking about best using an ADC and I&amp;#39;ve done some weighing up of suitable components. I&amp;#39;ve half settled on a Microchip MCP3248 rather than a TI ADS1115 . The Microchip has slightly better specs than the TI bu...</description><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>RE: Thoughts on Scaling and Biasing an ADC Input Signal</title><link>https://community.element14.com/members-area/personalblogs/b/blog/posts/thoughts-on-scaling-and-biasing-an-adc-input-signal</link><pubDate>Sun, 17 May 2020 19:32:36 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:970cceb5-e6e5-434b-b11d-af11c2f248b5</guid><dc:creator>shabaz</dc:creator><slash:comments>1</slash:comments><description>&lt;p&gt;Hi Andrew,&lt;/p&gt;&lt;p&gt;&amp;nbsp;&lt;/p&gt;&lt;p&gt;I was going to say usually ADS1115 is an easy justification because it is low-cost, but it doesn&amp;#39;t seem to be that any more, at least for one-offs. I don&amp;#39;t understand TI pricing.. a circa £20 dev-board for a different chip I was looking at is now over £200..&lt;/p&gt;&lt;p&gt;There&amp;#39;s no need for negative supplies or negative voltages to be buffered (or were you discussing the difference between two positive voltages?), the differential inputs can be driven from dual op-amps, known as a differential driver (example is ADA4941 but there are probably lower-cost alternatives, or it could be formed from two op amps). That will generate differential outputs centred around a value you choose based on an input reference voltage. For example, if your ADC only accepts 0-2.048V on its inputs, then you could use 1.024V as a reference. Then, your input, single-ended, between 0 and any positive voltage, will (theoretically) use the full range, based on the gain value you set (caveat; the op-amps won&amp;#39;t completely go rail to rail, so you&amp;#39;ll lose some range). By differential output I mean each of the two signals will be positive (i.e. between 0-2.048V for instance) but subtracting one from the other gets you the -2.048 to +2.048 range, and no negative supplies are used.&lt;/p&gt;&lt;p&gt;However, if you just want to measure between 0V and 5V, it could be easier to just use a single ended ADC and if you definitely need the extra resolution you could choose (say) an 18-bit ADC, if all else is equal (which it rarely is!). I&amp;#39;m not sure I ever end up picking the &amp;#39;right&amp;#39; ADC. But for &amp;#39;just a redesign&amp;#39; for the input circuitry or references, something better or cheaper always seems to be missed : ( &lt;/p&gt;&lt;img src="https://community.element14.com/aggbug?PostID=9355&amp;AppID=293&amp;AppType=Weblog&amp;ContentType=0" width="1" height="1"&gt;</description></item></channel></rss>