Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator Flight Simulator 101 or back to college - part 16: C Structures with in Structures
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 3 May 2023 5:34 PM Date Created
  • Views 1795 views
  • Likes 9 likes
  • Comments 12 comments
  • flight simulator
  • nexgen
  • back to college
  • c programing
  • flight simulation 101
  • data structures
  • struct as member of a struct
Related
Recommended

Flight Simulator 101 or back to college - part 16: C Structures with in Structures

phoenixcomm
phoenixcomm
3 May 2023

imageNow, Somewhere on the Stack Exchange, I heard some crud about you just can't have a struct as a member of a struct. Well, you sure can and now for all the curious minds out there I will show you how to do it. Remember I work with flight simulation, so you always need to know where you are. This is called position, and it is made up of both a Latitude and a Longitude which are both structures of themselves, enclosed in an outer structure. 

First I need to create two structs called Lat and Lon and I will make them out of a structure that I call DM, or Degrees and Minutes, and you also need to know the Hemisphere or hemi. 

struct DM {
	int degrees;
	float minutes;
	char hemi; 
	};

struct DM Lat;
struct DM Lon;
Now that I have that out of the way, I need to put this                   together and create my three structures: Current, Start, and Finish. You will note they all have a             structure type of Position. So you ask how do I access them? Well, you just use dotted notation.

struct Position{
	struct DM Lat;
	struct DM Lon; } Current, Start, Finish;
// Carswell: 32-46.151167N 097-26.492083W
	Start.Lon.degrees  = 32;
	Start.Lon.minutes  = 46.151167;
	Start.Lon.hemi     = 'N';
	Start.Lat.degrees  = 97;
	Start.Lat.minutes  = 26.492083;
	Start.Lat.hemi     = 'W';

Now, I hope I have helped some of you.. I think this will close this blog.  

  • Sign in to reply
Parents
  • Andrew J
    Andrew J over 3 years ago

    I’m not an experienced C or C++ programmer so please bear with a probably simple question: why do you have to declare Lat and Lon as DM types on the first code block lines 7 and 8, and then again within Struct Position on lines 2 and 3 of the second code block?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to Andrew J

     /user/conversations?New=True&UserId=188728 Andrew, I actually tried that but the compiler did not like it. So do it the long way define the struct then stick it in the outside struct. hence a struct as a member of the struct.  così va

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to phoenixcomm

    Ok; I’d like to say it makes sense but it doesn’t really - compilers often have their quirks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to Andrew J

    I must have had a typo when I first put a struct in a struct. I use GCC and It works fine. -enjoy

    struct test {
    struct member {
    float x;
    float y;
    int degress; } angle
    int itemNumber;
    char discription[50];
    float weight; }TEST;

    I might have tried to declare an array char[50] description -LOL
    In my simulator, my aircraft model consists of a STRUCT with more than a few more STRUCTs in it. ie.:

    where things are measured from the tip of the tail forward, right wing to left, and the top of the tail to the ground.
    struct XYZ {
    float X;
    float Y;
    float Z;} XYZpart, XYZac, XYZmate;

    struct Locations {
    struct XYZpart;
    struct XYZac;
    struct XYZmate;}
    float partWeight;
    char partName[50];
    char partNumber[50];
    char atachName[50];
    char atachNumber[50];}Parts;
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to Andrew J

    I must have had a typo when I first put a struct in a struct. I use GCC and It works fine. -enjoy

    struct test {
    struct member {
    float x;
    float y;
    int degress; } angle
    int itemNumber;
    char discription[50];
    float weight; }TEST;

    I might have tried to declare an array char[50] description -LOL
    In my simulator, my aircraft model consists of a STRUCT with more than a few more STRUCTs in it. ie.:

    where things are measured from the tip of the tail forward, right wing to left, and the top of the tail to the ground.
    struct XYZ {
    float X;
    float Y;
    float Z;} XYZpart, XYZac, XYZmate;

    struct Locations {
    struct XYZpart;
    struct XYZac;
    struct XYZmate;}
    float partWeight;
    char partName[50];
    char partNumber[50];
    char atachName[50];
    char atachNumber[50];}Parts;