In the last couple of days my Microsoft Edge browser has stopped being able to present the blog editing screen correctly. It ends up like this, without menus and tool buttons. Initially, it seems that it paints the usual screen (bit difficult to tell because it's just a momentary flash in front of the eyes), then immediately repaints it with this one where the 'Body' box just shows two lines.
Edge version is 102.0.1245.39 64-bit on Win 8.1. It says it's up to date.
There was an upgrade earlier this week (it resulted in one of those splash screens that tell you about all the wonderful new features, so it was more than just bug fixes), so it might have been that that brought the change.
Has anyone else had a similar problem using Edge?
Any thoughts on what the problem might be and whether there's anything I can do to get it back?
I'm posting this using Sea Monkey (based on Mozilla), which is fine with the editing so it doesn't stop me contributing, but it's more sluggish than Edge and I'd like to continue with using Edge if I could.