Hi,
Happy New Year! My first feature suggestion of 2024 : ) It's similar to suggestions in 2023 and 2022, but it's still worth bringing up again perhaps.
I was wondering, could there be some brainstorming between users and element14 to improve notifications-enabling, solely in ways that are not dependent on Verint? Because if it's dependent on Verint then it's unlikely to happen in a good timeframe.
If a user either comments or likes a discussion (or likes the comments), or likes a blog post or review, or likes any of the comments for them, then the suggestion is to either
(1) to automatically subscribe the user for for both discussion/blog/review notifications _and_ comment notifications (provided that's what the user wants in their profile) or
(2) to show a pop-up to allow the user to subscribe when they actively click 'Like', or
(3) replace "Like" with two buttons: "Like and Subscribe" and "Like Only", and replace the 'Reply" button during commenting, with "Reply and Subscribe" and "Reply Only".
Other ideas appreciated (since it's clear some brainstorming is needed, to find a non-Verint-dependent path).
This would not replace the need for "Latest Activity" by the way. If there was a "Latest Activity" that worked as well as Jive did, then notifications-enabling probably would not need to be improved.