Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog Arduino LightBox
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: feiticeir0
  • Date Created: 3 Feb 2021 4:32 PM Date Created
  • Views 3216 views
  • Likes 8 likes
  • Comments 6 comments
  • lightbox
  • arduino light box
  • ambient light
  • arduino ambient light
  • arduino projects for beginners
  • arduino
Related
Recommended

Arduino LightBox

feiticeir0
feiticeir0
3 Feb 2021

Hi all

This is a project that I've build a time ago to have some ambient light in photos I've taken of some projects that I did to display in Arduino day in my town.

Using 4 potentiometers you can change the LED color and brightness .

 

imageimage

 

Materials needed

  • Arduino - I've used a Micro Pro
  • 4x 10k potentiometer
  • 1x Adafruit Neopixel stick - or compatible
  • 1x 18650 battery
  • 1x 18650 battery holder
  • Toggle Switch ON-OFF
  • DC-DC Mini Step Up Power Module 1-5v to 5v boost converter
  • image

 

image

3D printed case

image

 

Assembly

 

Following the schematics, the assembly is very simple.

Wire the toggle switch to the battery and to the step-up .

image

Insert the battery holder next to the wall - there is a separator to keep the holder in place.

image

Wire all the potentiometers and the Neopixel strip

image

image

Everything wired

imageimage

 

Let it be light

image

 

Use 4 M2.5x7 screws to close the LID

image

image

image

imageimage

 

Code

Here's the Arduino code for it. It's very straightforward and it uses the FastLed library.

 

#include <FastLED.h>


#define NUM_LEDS 8

#define DATA_PIN 9

CRGB leds[NUM_LEDS];

const int redPin = A3;
const int greenPin = A2;
const int bluePin = A1;
const int brightPin = A0;

// variable for storing the potentiometer value
int redValue = 0;
int greenValue = 0;
int blueValue = 0;
int brightValue = 255; //1.0 ???

//store old values
int oldRedValue = 0;
int oldGreenValue = 0;
int oldBlueValue = 0;

void setup() {
  // put your setup code here, to run once:
  Serial.begin(115200);
  Serial.println();
  
  //LEDS
  FastLED.addLeds<NEOPIXEL, DATA_PIN>(leds, NUM_LEDS);
  
  //show leds
  fill_solid (leds, NUM_LEDS, CRGB(0, 0, 0));
  FastLED.show();
}


void loop() {
  // put your main code here, to run repeatedly:
  //Read colors to send
  redValue = map(analogRead (redPin),0, 1023, 0, 255);
  greenValue = map(analogRead (greenPin), 0, 1023, 0, 255);
  blueValue = map(analogRead (bluePin), 0, 1023, 0, 255); 
  brightValue = map(analogRead (brightPin), 0, 4095, 0, 255);
  /*Serial.print("R: ");
  Serial.println(redValue);
  Serial.print("G: ");
  Serial.println(greenValue);
  Serial.print("B: ");
  Serial.println(blueValue); */
  FastLED.setBrightness(brightValue);
  fill_solid (leds, NUM_LEDS, CRGB(redValue, greenValue, blueValue));
  FastLED.show();   
}

 

Hope you like it !

Files are attached

Thingiverse thing

Attachments:
Arduino_lightbox.zip
  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +2
    Nice project. It was fun seeing you use analog inputs, they are clearly an under used feature of an Arduino application. DAB
  • neilk
    neilk over 5 years ago +2
    Very nice project neil
  • genebren
    genebren over 5 years ago +1
    Nice project! Always fun and rewarding to build something that works.
Parents
  • DAB
    DAB over 5 years ago

    Nice project.

     

    It was fun seeing you use analog inputs, they are clearly an under used feature of an Arduino application.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 5 years ago

    Nice project.

     

    It was fun seeing you use analog inputs, they are clearly an under used feature of an Arduino application.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • feiticeir0
    feiticeir0 over 5 years ago in reply to DAB

    Thank you.

    Yes they are.

    • Cancel
    • Vote Up +1 Vote Down