Hi all
This is a project that I've build a time ago to have some ambient light in photos I've taken of some projects that I did to display in Arduino day in my town.
Using 4 potentiometers you can change the LED color and brightness .
Materials needed
- Arduino - I've used a Micro Pro
- 4x 10k potentiometer
- 1x Adafruit Neopixel stick - or compatible
- 1x 18650 battery
- 1x 18650 battery holder
- Toggle Switch ON-OFF
- DC-DC Mini Step Up Power Module 1-5v to 5v boost converter

3D printed case
Assembly
Following the schematics, the assembly is very simple.
Wire the toggle switch to the battery and to the step-up .
Insert the battery holder next to the wall - there is a separator to keep the holder in place.
Wire all the potentiometers and the Neopixel strip
Everything wired
Let it be light
Use 4 M2.5x7 screws to close the LID
Code
Here's the Arduino code for it. It's very straightforward and it uses the FastLed library.
#include <FastLED.h>
#define NUM_LEDS 8
#define DATA_PIN 9
CRGB leds[NUM_LEDS];
const int redPin = A3;
const int greenPin = A2;
const int bluePin = A1;
const int brightPin = A0;
// variable for storing the potentiometer value
int redValue = 0;
int greenValue = 0;
int blueValue = 0;
int brightValue = 255; //1.0 ???
//store old values
int oldRedValue = 0;
int oldGreenValue = 0;
int oldBlueValue = 0;
void setup() {
// put your setup code here, to run once:
Serial.begin(115200);
Serial.println();
//LEDS
FastLED.addLeds<NEOPIXEL, DATA_PIN>(leds, NUM_LEDS);
//show leds
fill_solid (leds, NUM_LEDS, CRGB(0, 0, 0));
FastLED.show();
}
void loop() {
// put your main code here, to run repeatedly:
//Read colors to send
redValue = map(analogRead (redPin),0, 1023, 0, 255);
greenValue = map(analogRead (greenPin), 0, 1023, 0, 255);
blueValue = map(analogRead (bluePin), 0, 1023, 0, 255);
brightValue = map(analogRead (brightPin), 0, 4095, 0, 255);
/*Serial.print("R: ");
Serial.println(redValue);
Serial.print("G: ");
Serial.println(greenValue);
Serial.print("B: ");
Serial.println(blueValue); */
FastLED.setBrightness(brightValue);
fill_solid (leds, NUM_LEDS, CRGB(redValue, greenValue, blueValue));
FastLED.show();
}
Hope you like it !
Files are attached
















Top Comments
-
neilk
-
Cancel
-
Vote Up
+2
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
neilk
-
Cancel
-
Vote Up
+2
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children