This video demonstrates how to wirelessly control two DC motors using two Arduino Unos. One Arduino acts as a controller with a joystick and XBee module, while the other acts as a receiver with a motor shield and XBee module. The video shows the connections and provides a basic overview of the code used to read joystick input and control the motors wirelessly.
Project#1
DualVNH5019MotorShield library
2 x Arduino Uno
2 x xbee series 1
1 x tumb joystick
1 x 9 Volt power pack
1 x Pololu VNH5019 Motor Shield
2 x 12 Volt dc motors
1 x power supply 12V
GitHub:
https://github.com/Fabiolus2020/ArduinoUno_1Joystick_2Motors_2Xbees_DualVNH5019MotorShield
EasyTrasnfer library:
https://github.com/madsci1016/Arduino-EasyTransfer
Example Sketch:
Pololu VNH5019 user guide
https://www.pololu.com/docs/0J49/all
How to program Xbees
https://learn.sparkfun.com/tutorials/exploring-xbees-and-xctu/all
Demo Video
controller sketch
//created by Fabiolus 2021/01/08
#include <EasyTransfer.h>
//create two objects
EasyTransfer ETout;
const int potpin1 = A0;
const int potpin2 = A1;
struct SEND_DATA_STRUCTURE {
//put your variable definitions here for the data you want to receive
//THIS MUST BE EXACTLY THE SAME ON THE OTHER ARDUINO
int valX;
int valY;
};
SEND_DATA_STRUCTURE txdata;
void setup() {
Serial.begin(9600);
//start the library, pass in the data details and the name of the serial port. Can be Serial, Serial1, Serial2, etc.
ETout.begin(details(txdata), &Serial);
}
void loop() {
txdata.valY = analogRead(potpin1);
txdata.valX = analogRead(potpin2);
ETout.sendData();
}
receiver sketch
//created by Fabiolus 2021/01/08
#include <DualVNH5019MotorShield.h>
#include <EasyTransfer.h>
DualVNH5019MotorShield md;
void stopIfFault()
{
if (md.getM1Fault())
{
Serial.println("M1 fault");
while (1);
}
if (md.getM2Fault())
{
Serial.println("M2 fault");
while (1);
}
}
EasyTransfer ETin;
struct RECEIVE_DATA_STRUCTURE {
//put your variable definitions here for the data you want to receive
//THIS MUST BE EXACTLY THE SAME ON THE OTHER ARDUINO
int valX;
int valY;
};
RECEIVE_DATA_STRUCTURE rxdata;
void setup() {
Serial.begin(9600);
md.init(); //initiates default pololu shield pins
ETin.begin(details(rxdata), &Serial);
}
void loop() {
for (int i = 0; i < 5; i++) {
if (ETin.receiveData()) {
rxdata.valY = map(rxdata.valY, 0, 1023, -255, 255);
rxdata.valX = map(rxdata.valX, 0, 1023, -255, 255);
if (rxdata.valX >= 10)
{
md.setM1Speed(rxdata.valX);
md.setM2Speed(rxdata.valX);
stopIfFault();
}
else if (rxdata.valX <= -10)
{
md.setM1Speed(rxdata.valX);
md.setM2Speed(rxdata.valX);
stopIfFault();
}
else if (rxdata.valY <= -10)
{
md.setM1Speed(rxdata.valY);
md.setM2Speed(-rxdata.valY);
stopIfFault();
}
else if (rxdata.valY >= 10)
{
md.setM1Speed(-rxdata.valY);
md.setM2Speed(rxdata.valY);
stopIfFault();
}
else {
md.setM1Speed(0);
md.setM2Speed(0);
}
}
delay(10);
}
}
-
DAB
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
-
fabiolus
in reply to DAB
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
-
cstanton
in reply to fabiolus
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
cstanton
in reply to fabiolus
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children