Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog RS422 / RS485 Shield for Arduino
  • Blog
  • Forum
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Arduino Projects requires membership for participation - click to join
Blog Post Actions
  • Subscribe by email
  • More
  • Cancel
  • Share
  • Subscribe by email
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
Author: hwhardsoft
Date Created: 14 Aug 2018 9:35 AM
Views: 1178
Likes: 9
Comments: 5
  • modbus rs485 arduino
  • rs422/485
  • arduino shield
  • rs485
  • dmx
  • useful arduino projects
  • rs422
  • arduino
Related
Recommended

RS422 / RS485 Shield for Arduino

hwhardsoft
hwhardsoft
14 Aug 2018

I'm working currently on a professional RS422/RS485 shield for the Arduino UNO (and compatible boards) and other SBC with Arduino style headers (like STM Nucleo) . I wasn't satisfied with the shields on the market. They are very simple and have some disadvantages. My shield comes with the following features:

 

  - RS485 mode (half duplex)

  - RS422 mode (full duplex)

  - galvanic isolation between Arduino and connected RS485 bus

  - free choice of TX-pin between pins 0-5

  - free choice of RX-pin between pins 0-5

  - enhanced ESD protection

  - adjustable automatic transceiver switching for RS485 mode

  - adjustable control of transceiver/receiver via pin 6 or 7

  - adjustable Pull-Up, Pull-Down und terminating resistors

  - indicator LEDs for RX and TX

  - removable block terminal for bus connection

  - many options adjustable via DIP switches

  - stackable headers

  - can be configured for 3.3V and 5V logic

 

You don't have permission to edit metadata of this video.
Edit media
x
Upload Preview

 

Anonymous

Top Comments

  • hwhardsoft
    hwhardsoft over 3 years ago +3

    We got the first batch of Arduino RS485 shields - fresh from the factory:

     

  • hwhardsoft
    hwhardsoft over 3 years ago +3

    Test run of a RS485 connection of a Raspberry Pi (left position), Arduino 101 and Arduino UNO (right).... This setting can be extended to up to 255 devices and a distance over 1km

    https://www.hwhardsoft…

Parents
  • hwhardsoft
    hwhardsoft over 3 years ago

    Test run of a RS485 connection of a Raspberry Pi (left position), Arduino 101 and Arduino UNO (right).... This setting can be extended to up to 255 devices and a distance over 1km

    https://www.hwhardsoft.de/english/projects/rs485-arduino/

    • Cancel
    • Up +3 Down
    • Reply
    • More
    • Cancel
Comment
  • hwhardsoft
    hwhardsoft over 3 years ago

    Test run of a RS485 connection of a Raspberry Pi (left position), Arduino 101 and Arduino UNO (right).... This setting can be extended to up to 255 devices and a distance over 1km

    https://www.hwhardsoft.de/english/projects/rs485-arduino/

    • Cancel
    • Up +3 Down
    • Reply
    • More
    • Cancel
Children
  • hwhardsoft
    hwhardsoft over 3 years ago in reply to hwhardsoft

    its possible to stack up to 3 RS485 shields to an Arduino (or compatible) board. You can connect the Arduino to  3 independet RS485 busses in this case

     

    • Cancel
    • Up 0 Down
    • Reply