Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog Simple thermometer using Arduino Micro and OLED display
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 4 Jul 2015 11:27 AM Date Created
  • Views 3134 views
  • Likes 9 likes
  • Comments 14 comments
  • oled
  • micro
  • tmp36
  • adafruit
  • arduino
Related
Recommended

Simple thermometer using Arduino Micro and OLED display

fvan
fvan
4 Jul 2015

A colleague recently made an Arduino-based thermometer to measure how hot it gets in the office. I thought I'd recreate and document the project with the components I have at hand image

 

Circuit

 

The circuit is based around the TMP36 temperature sensor. It's cheap, easy to use and doesn't require any external calibration. The voltage output is linearly proportional to temperature in degrees Celsius, making the conversion easy to calculate.

Any Arduino or microcontroller having at least one analog input pin can be used to make the reading. Finally, some form of display is required. This could be a 7-segment display, a character LCD or even an OLED display.

 

I'll be using an Arduino Micro combined with a small OLED display.

 

The resulting circuit is the following:

image

 

Code

 

The temperature sensor can be used without any additional libraries, the analogRead() function and some math will do the trick.

 

The OLED display however, requires two libraries:

  • Adafruit GFX: core graphics library
  • Adafruit SSD1306: library for monochrome OLED displays based on SSD1306 drivers

 

The completed code looks as follows (comments in the code for explanation):

 

 

Result

 

Now I finally know how hot it is in my room ... Outside temperature is not bad either image

imageimage

 

Extra

 

As requested in the comments, I have made an updated version of the above project. It includes a button to toggle between degrees C, F and K.

 

All temperatures are calculated, and a button connected to an interrupt pin is used to toggle the displayed value.

 

The updated code:

 

 

Some pics:

 

imageimage

  • Sign in to reply

Top Comments

  • fvan
    fvan over 10 years ago +3
    Added a button linked to an interrupt to toggle the displayed value between degrees C, F and K. Updated the post above
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    Its all in the software so you can have it show in any unuit you prefer, Kelvin anyone
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to clem57 +2
    ... and for doing that in these harsh hot conditions!
Parents
  • fvan
    fvan over 10 years ago

    Added a button linked to an interrupt to toggle the displayed value between degrees C, F and K. Updated the post above image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to fvan

    Thank you for the updated version.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to clem57

    ... and for doing that in these harsh hot conditions!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to clem57

    ... and for doing that in these harsh hot conditions!

    • Cancel
    • Vote Up +2 Vote Down
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.